<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックRe: Can you program PCA9632 with non-default settings?</title>
    <link>https://community.nxp.com/t5/Power-Management/Can-you-program-PCA9632-with-non-default-settings/m-p/1692027#M2832</link>
    <description>&lt;P&gt;Oh wait, one more question: Do you know if NXP has any similar product in the same family that does allow this?&lt;/P&gt;</description>
    <pubDate>Tue, 25 Jul 2023 08:00:04 GMT</pubDate>
    <dc:creator>CoryP</dc:creator>
    <dc:date>2023-07-25T08:00:04Z</dc:date>
    <item>
      <title>Can you program PCA9632 with non-default settings?</title>
      <link>https://community.nxp.com/t5/Power-Management/Can-you-program-PCA9632-with-non-default-settings/m-p/1691947#M2829</link>
      <description>&lt;P&gt;Hi, I need a PWM controller to control the brightness of a set of LEDs and I'm considering using the PCA9632. This is perfect for my needs except for one thing.&lt;/P&gt;&lt;P&gt;The power-on configuration appears to be SLEEP with 0% duty cycle on all outputs. I'd prefer if it could power on directly into OSC on, with 50% duty cycle on one of the pins. From my understanding of the datasheet, this must be programmed on every power-on.&lt;/P&gt;&lt;P&gt;Is there a way to configure the power-on defaults so that I don't have to create a script to send 3-4 of the same I2C commands on every power-up? This would complicate things because I would need my microcontroller to do this while it powers up at the same time as this chip.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Cory&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jul 2023 06:44:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Can-you-program-PCA9632-with-non-default-settings/m-p/1691947#M2829</guid>
      <dc:creator>CoryP</dc:creator>
      <dc:date>2023-07-25T06:44:42Z</dc:date>
    </item>
    <item>
      <title>Re: Can you program PCA9632 with non-default settings?</title>
      <link>https://community.nxp.com/t5/Power-Management/Can-you-program-PCA9632-with-non-default-settings/m-p/1692012#M2830</link>
      <description>&lt;P&gt;Hello Cory,&lt;/P&gt;
&lt;P&gt;Thank you for considering the PCA9632 for your application.&lt;/P&gt;
&lt;P&gt;As you correctly stated, the oscillator is off (low power mode) and duty cycles in PWMx registers set to 0% by default.&lt;/P&gt;
&lt;P&gt;Unfortunately, the PCA9632 does not allow to pre-configure the default settings in OTP or similar, it needs to be set every time the power is turned on.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Tomas&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jul 2023 07:46:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Can-you-program-PCA9632-with-non-default-settings/m-p/1692012#M2830</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2023-07-25T07:46:59Z</dc:date>
    </item>
    <item>
      <title>Re: Can you program PCA9632 with non-default settings?</title>
      <link>https://community.nxp.com/t5/Power-Management/Can-you-program-PCA9632-with-non-default-settings/m-p/1692026#M2831</link>
      <description>&lt;P&gt;Ah I see, thank you for clarifying.&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jul 2023 07:59:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Can-you-program-PCA9632-with-non-default-settings/m-p/1692026#M2831</guid>
      <dc:creator>CoryP</dc:creator>
      <dc:date>2023-07-25T07:59:20Z</dc:date>
    </item>
    <item>
      <title>Re: Can you program PCA9632 with non-default settings?</title>
      <link>https://community.nxp.com/t5/Power-Management/Can-you-program-PCA9632-with-non-default-settings/m-p/1692027#M2832</link>
      <description>&lt;P&gt;Oh wait, one more question: Do you know if NXP has any similar product in the same family that does allow this?&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jul 2023 08:00:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Can-you-program-PCA9632-with-non-default-settings/m-p/1692027#M2832</guid>
      <dc:creator>CoryP</dc:creator>
      <dc:date>2023-07-25T08:00:04Z</dc:date>
    </item>
    <item>
      <title>Re: Can you program PCA9632 with non-default settings?</title>
      <link>https://community.nxp.com/t5/Power-Management/Can-you-program-PCA9632-with-non-default-settings/m-p/1692034#M2833</link>
      <description>&lt;P&gt;Unfortunately, currently not.&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jul 2023 08:07:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Can-you-program-PCA9632-with-non-default-settings/m-p/1692034#M2833</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2023-07-25T08:07:13Z</dc:date>
    </item>
    <item>
      <title>Re: Can you program PCA9632 with non-default settings?</title>
      <link>https://community.nxp.com/t5/Power-Management/Can-you-program-PCA9632-with-non-default-settings/m-p/1692107#M2834</link>
      <description>&lt;P&gt;Ok I see. Thank you again for the information!&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jul 2023 08:48:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Can-you-program-PCA9632-with-non-default-settings/m-p/1692107#M2834</guid>
      <dc:creator>CoryP</dc:creator>
      <dc:date>2023-07-25T08:48:22Z</dc:date>
    </item>
  </channel>
</rss>