<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Troubleshooting FRDM33771B FRDM33664BEVB setup in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/Troubleshooting-FRDM33771B-FRDM33664BEVB-setup/m-p/1671406#M2728</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are attempting to use the FRDM33771B via TPL and FRDM33664BEVB from an STM32 microcontroller.&lt;BR /&gt;We are unable to get the device properly communicating and would like some help resolving the problem.&lt;/P&gt;&lt;P&gt;The software being used is from &lt;A href="https://www.nxp.com/products/power-management/battery-management/battery-cell-controllers/14-channel-li-ion-battery-cell-controller-ic:MC33771B" target="_blank"&gt;https://www.nxp.com/products/power-management/battery-management/battery-cell-controllers/14-channel-li-ion-battery-cell-controller-ic:MC33771B&lt;/A&gt; (BCC_SDK_SW/S32DS_Examples/BCC_S32K144_Monitoring_Diagnostics). The bcc_peripheries.c functions have been ported to STM32.&lt;/P&gt;&lt;P&gt;At startup, the software calls:&lt;/P&gt;&lt;P&gt;- BCC_SoftwareReset()&lt;BR /&gt;- BCC_Reg_WriteGlobal(drvConfig, BCC_REG_SYS_CFG1_ADDR, BCC_W_SOFT_RST_MASK);&lt;/P&gt;&lt;P&gt;The following bytes are sent over SPI to the transceiver (SPI master), 00 10 03 03 37&lt;BR /&gt;The same data (but each byte shifted by a bit) is received (SPI slave), 00 20 06 06 6e&lt;/P&gt;&lt;P&gt;Next, the software attempts to:&lt;/P&gt;&lt;P&gt;- BCC_AssignCid()&lt;BR /&gt;- BCC_Reg_Read(drvConfig, BCC_CID_UNASSIG, BCC_REG_INIT_ADDR, 1U, &amp;amp;readVal);&lt;/P&gt;&lt;P&gt;It sends the following bytes, 00 01 01 01 7a&lt;BR /&gt;However, it instructs the SPI slave that it expects to receive two blocks in response.&lt;BR /&gt;As with the previous call, we only observe one block being echoed back, which then causes a receive timeout.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Looking at the TPL RDTX_IN, RDTX_OUT pads on the FRDM33771B, we do see pulses - suggesting that data is being sent across TPL.&lt;BR /&gt;We also observe that the LED on the transceiver board stays on, suggesting that communications are active.&lt;/P&gt;&lt;P&gt;Can you please suggest how to debug further.&lt;/P&gt;</description>
    <pubDate>Sat, 17 Jun 2023 09:46:29 GMT</pubDate>
    <dc:creator>tobyjaffey</dc:creator>
    <dc:date>2023-06-17T09:46:29Z</dc:date>
    <item>
      <title>Troubleshooting FRDM33771B FRDM33664BEVB setup</title>
      <link>https://community.nxp.com/t5/Power-Management/Troubleshooting-FRDM33771B-FRDM33664BEVB-setup/m-p/1671406#M2728</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are attempting to use the FRDM33771B via TPL and FRDM33664BEVB from an STM32 microcontroller.&lt;BR /&gt;We are unable to get the device properly communicating and would like some help resolving the problem.&lt;/P&gt;&lt;P&gt;The software being used is from &lt;A href="https://www.nxp.com/products/power-management/battery-management/battery-cell-controllers/14-channel-li-ion-battery-cell-controller-ic:MC33771B" target="_blank"&gt;https://www.nxp.com/products/power-management/battery-management/battery-cell-controllers/14-channel-li-ion-battery-cell-controller-ic:MC33771B&lt;/A&gt; (BCC_SDK_SW/S32DS_Examples/BCC_S32K144_Monitoring_Diagnostics). The bcc_peripheries.c functions have been ported to STM32.&lt;/P&gt;&lt;P&gt;At startup, the software calls:&lt;/P&gt;&lt;P&gt;- BCC_SoftwareReset()&lt;BR /&gt;- BCC_Reg_WriteGlobal(drvConfig, BCC_REG_SYS_CFG1_ADDR, BCC_W_SOFT_RST_MASK);&lt;/P&gt;&lt;P&gt;The following bytes are sent over SPI to the transceiver (SPI master), 00 10 03 03 37&lt;BR /&gt;The same data (but each byte shifted by a bit) is received (SPI slave), 00 20 06 06 6e&lt;/P&gt;&lt;P&gt;Next, the software attempts to:&lt;/P&gt;&lt;P&gt;- BCC_AssignCid()&lt;BR /&gt;- BCC_Reg_Read(drvConfig, BCC_CID_UNASSIG, BCC_REG_INIT_ADDR, 1U, &amp;amp;readVal);&lt;/P&gt;&lt;P&gt;It sends the following bytes, 00 01 01 01 7a&lt;BR /&gt;However, it instructs the SPI slave that it expects to receive two blocks in response.&lt;BR /&gt;As with the previous call, we only observe one block being echoed back, which then causes a receive timeout.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Looking at the TPL RDTX_IN, RDTX_OUT pads on the FRDM33771B, we do see pulses - suggesting that data is being sent across TPL.&lt;BR /&gt;We also observe that the LED on the transceiver board stays on, suggesting that communications are active.&lt;/P&gt;&lt;P&gt;Can you please suggest how to debug further.&lt;/P&gt;</description>
      <pubDate>Sat, 17 Jun 2023 09:46:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Troubleshooting-FRDM33771B-FRDM33664BEVB-setup/m-p/1671406#M2728</guid>
      <dc:creator>tobyjaffey</dc:creator>
      <dc:date>2023-06-17T09:46:29Z</dc:date>
    </item>
    <item>
      <title>Re: Troubleshooting FRDM33771B FRDM33664BEVB setup</title>
      <link>https://community.nxp.com/t5/Power-Management/Troubleshooting-FRDM33771B-FRDM33664BEVB-setup/m-p/1671880#M2732</link>
      <description>&lt;P&gt;Hello Toby,&lt;/P&gt;
&lt;P&gt;we have an&amp;nbsp;AN12084 "MC33771B/MC33772B programming guide", which can be downloaded from the &lt;A href="https://www.nxp.com/products/power-management/battery-management/battery-cell-controllers/14-channel-li-ion-battery-cell-controller-ic:MC33771B?fpsp=1&amp;amp;#documentation" target="_self"&gt;MC33771B product page&lt;/A&gt;, under the Secure Files.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_0-1687168318922.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/228305i85ED2F857B14D824/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_0-1687168318922.png" alt="JozefKozon_0-1687168318922.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_1-1687168345261.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/228306i95B49A2B46FEDA39/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_1-1687168345261.png" alt="JozefKozon_1-1687168345261.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_2-1687168368616.png" style="width: 219px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/228307i408796A314D7146B/image-dimensions/219x34?v=v2" width="219" height="34" role="button" title="JozefKozon_2-1687168368616.png" alt="JozefKozon_2-1687168368616.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_3-1687168386153.png" style="width: 378px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/228308iBACAA203B5FB501A/image-dimensions/378x34?v=v2" width="378" height="34" role="button" title="JozefKozon_3-1687168386153.png" alt="JozefKozon_3-1687168386153.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_4-1687168406126.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/228309iADBD6CD341454387/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_4-1687168406126.png" alt="JozefKozon_4-1687168406126.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_5-1687168496499.png" style="width: 216px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/228310iF7419EE61D5CF22A/image-dimensions/216x19?v=v2" width="216" height="19" role="button" title="JozefKozon_5-1687168496499.png" alt="JozefKozon_5-1687168496499.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;There is a complete guideline for the MC3377xB BCCs (Battery Cell Controllers) initialization. To be able to download the confidential documents, you need to have a valid NDA (Non Disclosure Agreement) with NXP. I have checked our NDA database and I couldn't find your company (&lt;SPAN&gt;RINGTAIL SOFTWARE&lt;/SPAN&gt;) in there. If you want to sign the NDA with NXP, please create a ticket &lt;A href="https://www.nxp.com/support/support:SUPPORTHOME?tid=sbmenu" target="_self"&gt;here&lt;/A&gt; and an NXP representative for NDA matters will support you.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_6-1687168818011.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/228316i24FE9DE843A7580F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_6-1687168818011.png" alt="JozefKozon_6-1687168818011.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Mon, 19 Jun 2023 10:00:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Troubleshooting-FRDM33771B-FRDM33664BEVB-setup/m-p/1671880#M2732</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2023-06-19T10:00:47Z</dc:date>
    </item>
  </channel>
</rss>