<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FS8530&amp;amp;8430 in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/FS8530-amp-8430/m-p/1665838#M2701</link>
    <description>&lt;P&gt;VMONx是不一样的，你查看下VMONx的电路配置&lt;/P&gt;</description>
    <pubDate>Thu, 08 Jun 2023 05:24:52 GMT</pubDate>
    <dc:creator>guoweisun</dc:creator>
    <dc:date>2023-06-08T05:24:52Z</dc:date>
    <item>
      <title>FS8530&amp;8430</title>
      <link>https://community.nxp.com/t5/Power-Management/FS8530-amp-8430/m-p/1665056#M2697</link>
      <description>&lt;P&gt;这是FS8530完成ABSIT1的条件&lt;FONT&gt;(Vxx_uv=0 and Vxx_ov=0) or !Vxx_ABIST1_OTP&amp;nbsp; 。&lt;BR /&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT&gt;我在8530A1ES上成功完成调试，但是PIN TO PIN 换上8430A0ES的时候，却卡在了ABSIT1，导致我无法进入INT_FS，我已经确定了DEBUG=0V, WAKE=1，然后VMON1=VMON2=0.8V，8430A0ES应该是没有FCCU的所以，这个脚应该是可以忽略的，但是我通过读取寄存器，返回没有VMON的OV和UV报错。我想问问，这个PIN TO PIN的替换后，还有那些引脚的电压问题，导致无法通过ABIST1吗&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 07 Jun 2023 09:30:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS8530-amp-8430/m-p/1665056#M2697</guid>
      <dc:creator>Oliver2</dc:creator>
      <dc:date>2023-06-07T09:30:14Z</dc:date>
    </item>
    <item>
      <title>Re: FS8530&amp;8430</title>
      <link>https://community.nxp.com/t5/Power-Management/FS8530-amp-8430/m-p/1665838#M2701</link>
      <description>&lt;P&gt;VMONx是不一样的，你查看下VMONx的电路配置&lt;/P&gt;</description>
      <pubDate>Thu, 08 Jun 2023 05:24:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS8530-amp-8430/m-p/1665838#M2701</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2023-06-08T05:24:52Z</dc:date>
    </item>
  </channel>
</rss>