<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power Management中的主题 Re: Reserve Power Circuit for LS1012A Design</title>
    <link>https://community.nxp.com/t5/Power-Management/Reserve-Power-Circuit-for-LS1012A-Design/m-p/869914#M258</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Joe,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is a reference design board for the QorIQ LS1012A using the VR5100 as the power management IC I charge of powering the system according to the LS1012A requirements, you can find details of the reference design in the reference manual that you can download from the following link: &lt;A href="https://www.nxp.com/support/developer-resources/software-development-tools/qoriq-developer-resources/qoriq-ls1012a-reference-design-board:LS1012A-RDB?tab=Documentation_Tab"&gt;https://www.nxp.com/support/developer-resources/software-development-tools/qoriq-developer-resources/qoriq-ls1012a-reference-design-board:LS1012A-RDB?tab=Documentation_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Plus, you can find the schematic and board design files by downloading the LS1012ARDB-PB Design files (REV D) on the following link: &lt;A href="https://www.nxp.com/support/developer-resources/software-development-tools/qoriq-developer-resources/qoriq-ls1012a-reference-design-board:LS1012A-RDB?tab=Design_Tools_Tab"&gt;https://www.nxp.com/support/developer-resources/software-development-tools/qoriq-developer-resources/qoriq-ls1012a-reference-design-board:LS1012A-RDB?tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The VR5100 have an integrated circuit used as battery backup:&lt;/P&gt;&lt;P&gt;From the On mode, when the voltage at VIN drops below the undervoltage falling threshold, UVDET, the state machine transitions to the Coin Cell mode.&lt;/P&gt;&lt;P&gt;The LICELL pin provides for a connection of a coin cell backup battery or a “super” capacitor. If the voltage at VIN goes below the VIN threshold (VTL1), contact-bounced, or removed, the coin cell maintained logic is powered by the voltage applied to LICELL.&lt;/P&gt;&lt;P&gt;Check the VR5100 datasheet for more details: &lt;A href="https://www.nxp.com/docs/en/data-sheet/VR5100.pdf"&gt;https://www.nxp.com/docs/en/data-sheet/VR5100.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 Mar 2019 19:46:57 GMT</pubDate>
    <dc:creator>reyes</dc:creator>
    <dc:date>2019-03-05T19:46:57Z</dc:date>
    <item>
      <title>Reserve Power Circuit for LS1012A Design</title>
      <link>https://community.nxp.com/t5/Power-Management/Reserve-Power-Circuit-for-LS1012A-Design/m-p/869913#M257</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I am designing a small board with the LS1012A ARM Processor. The board will likely consume about 16W of power. I will need to design a reserve power circuit to supply power to the board for a short amount of time. Does NXP have any devices that I could use to monitor the input power and switch over to some supercaps to provide a short time of power to the board, say 2 seconds or so, enough time for the Processor to finish what it was doing and go through the power down sequence of the Linux OS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Joe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Mar 2019 17:07:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Reserve-Power-Circuit-for-LS1012A-Design/m-p/869913#M257</guid>
      <dc:creator>joe1652</dc:creator>
      <dc:date>2019-03-05T17:07:54Z</dc:date>
    </item>
    <item>
      <title>Re: Reserve Power Circuit for LS1012A Design</title>
      <link>https://community.nxp.com/t5/Power-Management/Reserve-Power-Circuit-for-LS1012A-Design/m-p/869914#M258</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Joe,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is a reference design board for the QorIQ LS1012A using the VR5100 as the power management IC I charge of powering the system according to the LS1012A requirements, you can find details of the reference design in the reference manual that you can download from the following link: &lt;A href="https://www.nxp.com/support/developer-resources/software-development-tools/qoriq-developer-resources/qoriq-ls1012a-reference-design-board:LS1012A-RDB?tab=Documentation_Tab"&gt;https://www.nxp.com/support/developer-resources/software-development-tools/qoriq-developer-resources/qoriq-ls1012a-reference-design-board:LS1012A-RDB?tab=Documentation_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Plus, you can find the schematic and board design files by downloading the LS1012ARDB-PB Design files (REV D) on the following link: &lt;A href="https://www.nxp.com/support/developer-resources/software-development-tools/qoriq-developer-resources/qoriq-ls1012a-reference-design-board:LS1012A-RDB?tab=Design_Tools_Tab"&gt;https://www.nxp.com/support/developer-resources/software-development-tools/qoriq-developer-resources/qoriq-ls1012a-reference-design-board:LS1012A-RDB?tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The VR5100 have an integrated circuit used as battery backup:&lt;/P&gt;&lt;P&gt;From the On mode, when the voltage at VIN drops below the undervoltage falling threshold, UVDET, the state machine transitions to the Coin Cell mode.&lt;/P&gt;&lt;P&gt;The LICELL pin provides for a connection of a coin cell backup battery or a “super” capacitor. If the voltage at VIN goes below the VIN threshold (VTL1), contact-bounced, or removed, the coin cell maintained logic is powered by the voltage applied to LICELL.&lt;/P&gt;&lt;P&gt;Check the VR5100 datasheet for more details: &lt;A href="https://www.nxp.com/docs/en/data-sheet/VR5100.pdf"&gt;https://www.nxp.com/docs/en/data-sheet/VR5100.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Mar 2019 19:46:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Reserve-Power-Circuit-for-LS1012A-Design/m-p/869914#M258</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2019-03-05T19:46:57Z</dc:date>
    </item>
    <item>
      <title>Re: Reserve Power Circuit for LS1012A Design</title>
      <link>https://community.nxp.com/t5/Power-Management/Reserve-Power-Circuit-for-LS1012A-Design/m-p/869915#M259</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;Jose,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hello, thank you very much for responding to my post. This is very helpful.&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Joe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Mar 2019 20:13:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Reserve-Power-Circuit-for-LS1012A-Design/m-p/869915#M259</guid>
      <dc:creator>joe1652</dc:creator>
      <dc:date>2019-03-05T20:13:04Z</dc:date>
    </item>
    <item>
      <title>Re: Reserve Power Circuit for LS1012A Design</title>
      <link>https://community.nxp.com/t5/Power-Management/Reserve-Power-Circuit-for-LS1012A-Design/m-p/869916#M260</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, do you know the power consumption for the&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;LS1012ARDB-PB Development board? I find it very exciting that it use Power Over Ethernet.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Joe&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Mar 2019 04:44:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Reserve-Power-Circuit-for-LS1012A-Design/m-p/869916#M260</guid>
      <dc:creator>joe1652</dc:creator>
      <dc:date>2019-03-06T04:44:21Z</dc:date>
    </item>
    <item>
      <title>Re: Reserve Power Circuit for LS1012A Design</title>
      <link>https://community.nxp.com/t5/Power-Management/Reserve-Power-Circuit-for-LS1012A-Design/m-p/869917#M261</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Joe,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The LS1012A&amp;nbsp;by itself have a 1W typical power dissipation, unfortunately I do not have access to the total power consumption of the LS1012ARDB-PB Development board, but you can enter a new community thread in the QorIQ community to ask this question, you can find this community in the following link: &lt;A _jive_internal="true" href="https://community.nxp.com/community/qoriq?tid=community"&gt;https://community.nxp.com/community/qoriq?tid=community&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Mar 2019 16:27:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Reserve-Power-Circuit-for-LS1012A-Design/m-p/869917#M261</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2019-03-06T16:27:06Z</dc:date>
    </item>
  </channel>
</rss>