<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックFRDM-K82F Mounted But Won't Connect toNXP GUI</title>
    <link>https://community.nxp.com/t5/Power-Management/FRDM-K82F-Mounted-But-Won-t-Connect-toNXP-GUI/m-p/1640690#M2566</link>
    <description>&lt;P&gt;I have a KITVR5510DA0EVM, which is the VR5510 eval board. It utilizes the FRDM-K82F to faciliate communication between the PC running the NXP GUI and actually configuring the VR5510.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I followed the guide below (Section 5) to get the K82F updated.&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/user-guide/UM11586.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/user-guide/UM11586.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was able to update the bootloader and application on the K82F, but I am having problems starting a session with the device through the NXP GUI. I can see the device is mounted through the file explorer on Windows 10, and right after I connect the device I do see the start session become "clickable", but then it immediately goes away and the light right next to J5 turns off on the K82F. This symptoms are repeatable by hot-plugging the USB cable. I have tried reflashing the K82F multiple times, no luck.&lt;/P&gt;&lt;P&gt;What should I try next?&lt;/P&gt;</description>
    <pubDate>Wed, 26 Apr 2023 14:59:35 GMT</pubDate>
    <dc:creator>swhite39</dc:creator>
    <dc:date>2023-04-26T14:59:35Z</dc:date>
    <item>
      <title>FRDM-K82F Mounted But Won't Connect toNXP GUI</title>
      <link>https://community.nxp.com/t5/Power-Management/FRDM-K82F-Mounted-But-Won-t-Connect-toNXP-GUI/m-p/1640690#M2566</link>
      <description>&lt;P&gt;I have a KITVR5510DA0EVM, which is the VR5510 eval board. It utilizes the FRDM-K82F to faciliate communication between the PC running the NXP GUI and actually configuring the VR5510.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I followed the guide below (Section 5) to get the K82F updated.&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/user-guide/UM11586.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/user-guide/UM11586.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was able to update the bootloader and application on the K82F, but I am having problems starting a session with the device through the NXP GUI. I can see the device is mounted through the file explorer on Windows 10, and right after I connect the device I do see the start session become "clickable", but then it immediately goes away and the light right next to J5 turns off on the K82F. This symptoms are repeatable by hot-plugging the USB cable. I have tried reflashing the K82F multiple times, no luck.&lt;/P&gt;&lt;P&gt;What should I try next?&lt;/P&gt;</description>
      <pubDate>Wed, 26 Apr 2023 14:59:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FRDM-K82F-Mounted-But-Won-t-Connect-toNXP-GUI/m-p/1640690#M2566</guid>
      <dc:creator>swhite39</dc:creator>
      <dc:date>2023-04-26T14:59:35Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K82F Mounted But Won't Connect toNXP GUI</title>
      <link>https://community.nxp.com/t5/Power-Management/FRDM-K82F-Mounted-But-Won-t-Connect-toNXP-GUI/m-p/1641019#M2568</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I hope all is great with you. Thank you for using the NXP communities.&lt;/P&gt;
&lt;P&gt;Could you please share a short video of the procedure that you followed?&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;David&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 26 Apr 2023 23:37:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FRDM-K82F-Mounted-But-Won-t-Connect-toNXP-GUI/m-p/1641019#M2568</guid>
      <dc:creator>diazmarin09</dc:creator>
      <dc:date>2023-04-26T23:37:46Z</dc:date>
    </item>
  </channel>
</rss>