<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックRe: FS4503 FS0B released only during debug</title>
    <link>https://community.nxp.com/t5/Power-Management/FS4503-FS0B-released-only-during-debug/m-p/1588799#M2363</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;SPAN&gt;Jozef,&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you for the advise.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;It is a reset due to watchdog. What I observe currently is, after the INIT_FS state, when I try to clear the FLT_ERR counter through multiple watchdog triggers, the reset is seen.&lt;/P&gt;&lt;P&gt;Clearing of FLT_ERR counter is required to release the FS0B pin.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also if I try to set the WD_WINDOW value to 0, similar reset is observed while accessing the register itself. Currently the WD_WINDOW is set to 12.&amp;nbsp;&lt;/P&gt;&lt;P&gt;However if I monitor the FS0B_SNS sense every time the watchdog is triggered correctly (through a timed event) there is no issue observed but it takes time to release the FS0B pin.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please advise me on the same.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Aditya&lt;/P&gt;</description>
    <pubDate>Fri, 27 Jan 2023 10:59:00 GMT</pubDate>
    <dc:creator>aditya_barve</dc:creator>
    <dc:date>2023-01-27T10:59:00Z</dc:date>
    <item>
      <title>FS4503 FS0B released only during debug</title>
      <link>https://community.nxp.com/t5/Power-Management/FS4503-FS0B-released-only-during-debug/m-p/1587646#M2360</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are using FS4503 power management IC in one of our projects.&amp;nbsp;&lt;/P&gt;&lt;P&gt;On trying to release the FS0B after the ABIST and LBIST tests are run, the FS0B is released only when the debug connector is attached.&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I disconnect the debugger and perform a power on reset, I observe a reset every 50ms, and the execution is stuck. And the FS0B is not released.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you please help with the same?&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Aditya&lt;/P&gt;</description>
      <pubDate>Wed, 25 Jan 2023 12:57:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS4503-FS0B-released-only-during-debug/m-p/1587646#M2360</guid>
      <dc:creator>aditya_barve</dc:creator>
      <dc:date>2023-01-25T12:57:42Z</dc:date>
    </item>
    <item>
      <title>Re: FS4503 FS0B released only during debug</title>
      <link>https://community.nxp.com/t5/Power-Management/FS4503-FS0B-released-only-during-debug/m-p/1588164#M2362</link>
      <description>&lt;P&gt;Hello&amp;nbsp;Aditya,&lt;/P&gt;
&lt;P&gt;this looks like the watchdog is resetting the SBC. In debug mode watchdog refresh is not required, but in normal mode a periodic watchdog refresh from an MCU is required. Please refer to the section 12.5.2 in the FS6500-FS4500 datasheet for Watchdog operation.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_0-1674715313086.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/208404i959F28866402DBE0/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_0-1674715313086.png" alt="JozefKozon_0-1674715313086.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Please confirm if the SBC is in the Debug or Normal mode by measuring voltage on the DEBUG pin.&amp;nbsp; I guess when you connect the debugger to the SBC, the DEBUG pin is connected to the Vpre pin and the voltage is within the&amp;nbsp;VDEBUG_IL and&amp;nbsp;VDEBUG_IH.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot_3.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/208407i8D3123746DB1BF3C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Screenshot_3.png" alt="Screenshot_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot_4.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/208408i4833749C8F45C74E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Screenshot_4.png" alt="Screenshot_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Disconnecting the debugger, the DEBUG pin should be connected to GND through a pull-down resistor. Have you used a pull-down, pull-up resistor and a capacitor on the DEBUG pin?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot_3.png" style="width: 140px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/208405iC8D93C5580B14639/image-dimensions/140x157?v=v2" width="140" height="157" role="button" title="Screenshot_3.png" alt="Screenshot_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;You can refer to the&amp;nbsp;FRDMFS6523CAEVM-B-SCH-Schematic attached for recommended values.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot_2.png" style="width: 166px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/208406i9FF0F0A18420EECB/image-dimensions/166x245?v=v2" width="166" height="245" role="button" title="Screenshot_2.png" alt="Screenshot_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt; &lt;/P&gt;
&lt;P&gt; &lt;/P&gt;</description>
      <pubDate>Thu, 26 Jan 2023 06:53:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS4503-FS0B-released-only-during-debug/m-p/1588164#M2362</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2023-01-26T06:53:52Z</dc:date>
    </item>
    <item>
      <title>Re: FS4503 FS0B released only during debug</title>
      <link>https://community.nxp.com/t5/Power-Management/FS4503-FS0B-released-only-during-debug/m-p/1588799#M2363</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;SPAN&gt;Jozef,&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you for the advise.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;It is a reset due to watchdog. What I observe currently is, after the INIT_FS state, when I try to clear the FLT_ERR counter through multiple watchdog triggers, the reset is seen.&lt;/P&gt;&lt;P&gt;Clearing of FLT_ERR counter is required to release the FS0B pin.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also if I try to set the WD_WINDOW value to 0, similar reset is observed while accessing the register itself. Currently the WD_WINDOW is set to 12.&amp;nbsp;&lt;/P&gt;&lt;P&gt;However if I monitor the FS0B_SNS sense every time the watchdog is triggered correctly (through a timed event) there is no issue observed but it takes time to release the FS0B pin.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please advise me on the same.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Aditya&lt;/P&gt;</description>
      <pubDate>Fri, 27 Jan 2023 10:59:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS4503-FS0B-released-only-during-debug/m-p/1588799#M2363</guid>
      <dc:creator>aditya_barve</dc:creator>
      <dc:date>2023-01-27T10:59:00Z</dc:date>
    </item>
    <item>
      <title>Re: FS4503 FS0B released only during debug</title>
      <link>https://community.nxp.com/t5/Power-Management/FS4503-FS0B-released-only-during-debug/m-p/1589734#M2364</link>
      <description>There was an issue during a function call to set the wd_window value. Its functional now and FS0B is released.&lt;BR /&gt;I have one following querry,&lt;BR /&gt;If watch dog is turned off and the wd_window value is set to 0, will the SBC go back into the INIT_FS state ?&lt;BR /&gt;&lt;BR /&gt;Thank you,&lt;BR /&gt;Aditya</description>
      <pubDate>Mon, 30 Jan 2023 10:27:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS4503-FS0B-released-only-during-debug/m-p/1589734#M2364</guid>
      <dc:creator>aditya_barve</dc:creator>
      <dc:date>2023-01-30T10:27:21Z</dc:date>
    </item>
    <item>
      <title>Re: FS4503 FS0B released only during debug</title>
      <link>https://community.nxp.com/t5/Power-Management/FS4503-FS0B-released-only-during-debug/m-p/1593705#M2384</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello&amp;nbsp;Aditya,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;If watch dog is turned off and the wd_window value is set to 0, will the SBC go back into the INIT_FS state?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;[A] Do you mean, that you have properly refreshed the watchdog during the INIT_FS state and entered NORMAL_WD state? If yes, than you need to send a periodic watchdog refresh. It you have set the WD_WINDOW to&amp;nbsp;0000, this value will be valid only during the INIT phase. In the NORMAL_WD state will be the WD_WINDOW set to default value 3.0ms.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_0-1675666757113.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/209669iB2355DE1DAD6D4F1/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_0-1675666757113.png" alt="JozefKozon_0-1675666757113.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_1-1675666817567.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/209670iB5EE72D17A09F8AA/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_1-1675666817567.png" alt="JozefKozon_1-1675666817567.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_2-1675667493763.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/209671i051938E0EF67F2E8/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_2-1675667493763.png" alt="JozefKozon_2-1675667493763.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_3-1675667586548.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/209672iB28FF01649C5338C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_3-1675667586548.png" alt="JozefKozon_3-1675667586548.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;After each incorrect watchdog refresh, the Watchdog error counter is incremented.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_4-1675667817265.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/209673i7F4747030A646CF7/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_4-1675667817265.png" alt="JozefKozon_4-1675667817265.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_5-1675667933149.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/209674iA926CFD0ACE61E79/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_5-1675667933149.png" alt="JozefKozon_5-1675667933149.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;From INIT_FS or from NORMAL_WD state, if the&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 06 Feb 2023 07:19:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS4503-FS0B-released-only-during-debug/m-p/1593705#M2384</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2023-02-06T07:19:14Z</dc:date>
    </item>
    <item>
      <title>Re: FS4503 FS0B released only during debug</title>
      <link>https://community.nxp.com/t5/Power-Management/FS4503-FS0B-released-only-during-debug/m-p/1634599#M2544</link>
      <description>Hello,&lt;BR /&gt;It appears that on a sbc where FS1B is enabled/ available, for FS0B to be released the test fs1b has to executed atleast once through a spi command.&lt;BR /&gt;It is observed that after running and releasing FS1B, the FS0B is released.&lt;BR /&gt;Let me know if this behaviour is acceptable.&lt;BR /&gt;&lt;BR /&gt;Thank you,&lt;BR /&gt;Aditya</description>
      <pubDate>Mon, 17 Apr 2023 10:26:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS4503-FS0B-released-only-during-debug/m-p/1634599#M2544</guid>
      <dc:creator>aditya_barve</dc:creator>
      <dc:date>2023-04-17T10:26:20Z</dc:date>
    </item>
  </channel>
</rss>