<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックSet FS26 To Normal Mode</title>
    <link>https://community.nxp.com/t5/Power-Management/Set-FS26-To-Normal-Mode/m-p/1585618#M2349</link>
    <description>&lt;P&gt;Hello Community,&lt;BR /&gt;I want to set the FS26 sbc in the normal mode, currently it is in the "Safety Output not released" state.&lt;/P&gt;&lt;P&gt;I did the procedure according to the datasheet:&lt;BR /&gt;got the&amp;nbsp;FLT_ERR_CNT To 0 (read the FS_I_FSSM register to verify it), and followed the procedure to write&amp;nbsp;RELEASE_FS0B_FS1B[15:0].&lt;/P&gt;&lt;P&gt;But still, the SBC is in the&amp;nbsp;"Safety Output not released" state.&lt;/P&gt;&lt;P&gt;Did I forget a step here? Is there anything I can check?&lt;/P&gt;&lt;P&gt;BR&lt;BR /&gt;Youssef&lt;/P&gt;</description>
    <pubDate>Thu, 19 Jan 2023 16:42:55 GMT</pubDate>
    <dc:creator>YBoughallad</dc:creator>
    <dc:date>2023-01-19T16:42:55Z</dc:date>
    <item>
      <title>Set FS26 To Normal Mode</title>
      <link>https://community.nxp.com/t5/Power-Management/Set-FS26-To-Normal-Mode/m-p/1585618#M2349</link>
      <description>&lt;P&gt;Hello Community,&lt;BR /&gt;I want to set the FS26 sbc in the normal mode, currently it is in the "Safety Output not released" state.&lt;/P&gt;&lt;P&gt;I did the procedure according to the datasheet:&lt;BR /&gt;got the&amp;nbsp;FLT_ERR_CNT To 0 (read the FS_I_FSSM register to verify it), and followed the procedure to write&amp;nbsp;RELEASE_FS0B_FS1B[15:0].&lt;/P&gt;&lt;P&gt;But still, the SBC is in the&amp;nbsp;"Safety Output not released" state.&lt;/P&gt;&lt;P&gt;Did I forget a step here? Is there anything I can check?&lt;/P&gt;&lt;P&gt;BR&lt;BR /&gt;Youssef&lt;/P&gt;</description>
      <pubDate>Thu, 19 Jan 2023 16:42:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Set-FS26-To-Normal-Mode/m-p/1585618#M2349</guid>
      <dc:creator>YBoughallad</dc:creator>
      <dc:date>2023-01-19T16:42:55Z</dc:date>
    </item>
    <item>
      <title>Re: Set FS26 To Normal Mode</title>
      <link>https://community.nxp.com/t5/Power-Management/Set-FS26-To-Normal-Mode/m-p/1585770#M2350</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I hope all is great with you. Thank you for using the NXP communities.&lt;/P&gt;
&lt;P&gt;Could you please confirm that you have done the procedures below?&lt;/P&gt;
&lt;OL&gt;
&lt;LI&gt;Write all INIT_FS registers To configure Safety outputs reaction and configure Watchdog&lt;/LI&gt;
&lt;LI&gt;Close INIT FS with x1 good Watchdog refresh&lt;/LI&gt;
&lt;LI&gt;Are ABIST = OK and LBIST = OK?&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;I hope this information helps.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;David&lt;/P&gt;</description>
      <pubDate>Thu, 19 Jan 2023 23:45:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Set-FS26-To-Normal-Mode/m-p/1585770#M2350</guid>
      <dc:creator>diazmarin09</dc:creator>
      <dc:date>2023-01-19T23:45:42Z</dc:date>
    </item>
    <item>
      <title>Re: Set FS26 To Normal Mode</title>
      <link>https://community.nxp.com/t5/Power-Management/Set-FS26-To-Normal-Mode/m-p/1585946#M2351</link>
      <description>&lt;P&gt;Hi David,&lt;BR /&gt;Step1 is OK&lt;BR /&gt;Step2 also OK&lt;BR /&gt;Step3 also OK&lt;/P&gt;&lt;P&gt;Is there any timing requirements, that I have to wait a certain amount of time before I write a register or something like that ? because it looks all the steps are done correctly but still the output is not released?&lt;BR /&gt;Could it be because i m still in debug mode?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 20 Jan 2023 16:42:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Set-FS26-To-Normal-Mode/m-p/1585946#M2351</guid>
      <dc:creator>YBoughallad</dc:creator>
      <dc:date>2023-01-20T16:42:38Z</dc:date>
    </item>
    <item>
      <title>Re: Set FS26 To Normal Mode</title>
      <link>https://community.nxp.com/t5/Power-Management/Set-FS26-To-Normal-Mode/m-p/1586232#M2354</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The below diagram provides high level flow chart to enter Normal mode in the application.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="diazmarin09_0-1674243591945.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/208075iFB55AE3DE88821AF/image-size/medium?v=v2&amp;amp;px=400" role="button" title="diazmarin09_0-1674243591945.png" alt="diazmarin09_0-1674243591945.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;diazmarin09_0-1674243591945.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please note that INT_FS windows is 256ms and after that, a WD refresh is required.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;David&lt;/P&gt;</description>
      <pubDate>Fri, 20 Jan 2023 19:40:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Set-FS26-To-Normal-Mode/m-p/1586232#M2354</guid>
      <dc:creator>diazmarin09</dc:creator>
      <dc:date>2023-01-20T19:40:04Z</dc:date>
    </item>
    <item>
      <title>Re: Set FS26 To Normal Mode</title>
      <link>https://community.nxp.com/t5/Power-Management/Set-FS26-To-Normal-Mode/m-p/1587112#M2358</link>
      <description>Hello,&lt;BR /&gt;I noticed that the Debug mode is set, and I have to exit the Debug mode to get to the normal mode.&lt;BR /&gt;I have to test that and see if it will work, meanwhile, is there a command to put the SBC in Init state again ? or only a reset will do that ?&lt;BR /&gt;YBoughallad</description>
      <pubDate>Tue, 24 Jan 2023 12:58:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Set-FS26-To-Normal-Mode/m-p/1587112#M2358</guid>
      <dc:creator>YBoughallad</dc:creator>
      <dc:date>2023-01-24T12:58:47Z</dc:date>
    </item>
    <item>
      <title>Re: Set FS26 To Normal Mode</title>
      <link>https://community.nxp.com/t5/Power-Management/Set-FS26-To-Normal-Mode/m-p/1587277#M2359</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I am pleased to know that your device is in Normal mode as requested.&lt;/P&gt;
&lt;P&gt;Do you mean going to INIT_FS from normal mode?&lt;/P&gt;
&lt;P&gt;The below diagram provides high level flow chart to enter normal mode in the application.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="diazmarin09_0-1674582435298.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/208263iE21B79087E626AEF/image-size/medium?v=v2&amp;amp;px=400" role="button" title="diazmarin09_0-1674582435298.png" alt="diazmarin09_0-1674582435298.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;diazmarin09_0-1674582435298.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Based on the diagram above, you are correct, a reset is needed.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;David&lt;/P&gt;</description>
      <pubDate>Tue, 24 Jan 2023 17:47:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Set-FS26-To-Normal-Mode/m-p/1587277#M2359</guid>
      <dc:creator>diazmarin09</dc:creator>
      <dc:date>2023-01-24T17:47:23Z</dc:date>
    </item>
  </channel>
</rss>