<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power Management中的主题 Re: PF5020 Open Drain Outputs</title>
    <link>https://community.nxp.com/t5/Power-Management/PF5020-Open-Drain-Outputs/m-p/1577481#M2331</link>
    <description>&lt;P&gt;Hello Thor,&lt;/P&gt;
&lt;P&gt;Thank you for using the NXP community.&lt;/P&gt;
&lt;P&gt;I personally do not think this is going to be an issue. Anyway, I do recommend using the &lt;A href="https://www.nxp.com/downloads/en/schematics/KITPF5020FRDMEVM-SCH.pdf" target="_blank"&gt;KITPF5020FRDMEVM Schematics&lt;/A&gt; as a reference for your design:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="diazmarin09_0-1672870750041.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/206117iFC628712C7D6AF19/image-size/medium?v=v2&amp;amp;px=400" role="button" title="diazmarin09_0-1672870750041.png" alt="diazmarin09_0-1672870750041.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;I hope this information helps.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;David&lt;/P&gt;</description>
    <pubDate>Wed, 04 Jan 2023 22:19:31 GMT</pubDate>
    <dc:creator>diazmarin09</dc:creator>
    <dc:date>2023-01-04T22:19:31Z</dc:date>
    <item>
      <title>PF5020 Open Drain Outputs</title>
      <link>https://community.nxp.com/t5/Power-Management/PF5020-Open-Drain-Outputs/m-p/1577370#M2328</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I just want to know if the PF5020 is safe to pull up the OD outputs (PGOOD, PGOODx, INTB) to a 5V source with 100k. I checked the datasheet and it says it can be pulled up to the VDDIO and the VDDIO is a voltage rail of either 1.8V or 3.3V.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The datasheet mentioned that these OD outputs have max 6V so &lt;/SPAN&gt;I think it should be OK since it is open drain but I am just wondering if there is any internal weak pull ups connected to VDDIO that wasn't mentioned in the datasheet&lt;SPAN&gt;.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Wed, 04 Jan 2023 18:47:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PF5020-Open-Drain-Outputs/m-p/1577370#M2328</guid>
      <dc:creator>ThorVic</dc:creator>
      <dc:date>2023-01-04T18:47:54Z</dc:date>
    </item>
    <item>
      <title>Re: PF5020 Open Drain Outputs</title>
      <link>https://community.nxp.com/t5/Power-Management/PF5020-Open-Drain-Outputs/m-p/1577419#M2329</link>
      <description>&lt;P&gt;Hello Thor,&lt;/P&gt;
&lt;P&gt;I hope all is great with you. Thank you for using the NXP communities.&lt;/P&gt;
&lt;P&gt;Will you supply the device with 5V as well? I mean, the main input supply will be 5V?&lt;/P&gt;
&lt;P&gt;I hope this information helps.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;David&lt;/P&gt;</description>
      <pubDate>Wed, 04 Jan 2023 20:06:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PF5020-Open-Drain-Outputs/m-p/1577419#M2329</guid>
      <dc:creator>diazmarin09</dc:creator>
      <dc:date>2023-01-04T20:06:41Z</dc:date>
    </item>
    <item>
      <title>Re: PF5020 Open Drain Outputs</title>
      <link>https://community.nxp.com/t5/Power-Management/PF5020-Open-Drain-Outputs/m-p/1577420#M2330</link>
      <description>&lt;P&gt;Thanks David.&lt;/P&gt;&lt;P&gt;Yes VIN will be 5V but VDDIO will be 3.3V.&lt;/P&gt;&lt;P&gt;Thor&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 04 Jan 2023 20:08:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PF5020-Open-Drain-Outputs/m-p/1577420#M2330</guid>
      <dc:creator>ThorVic</dc:creator>
      <dc:date>2023-01-04T20:08:26Z</dc:date>
    </item>
    <item>
      <title>Re: PF5020 Open Drain Outputs</title>
      <link>https://community.nxp.com/t5/Power-Management/PF5020-Open-Drain-Outputs/m-p/1577481#M2331</link>
      <description>&lt;P&gt;Hello Thor,&lt;/P&gt;
&lt;P&gt;Thank you for using the NXP community.&lt;/P&gt;
&lt;P&gt;I personally do not think this is going to be an issue. Anyway, I do recommend using the &lt;A href="https://www.nxp.com/downloads/en/schematics/KITPF5020FRDMEVM-SCH.pdf" target="_blank"&gt;KITPF5020FRDMEVM Schematics&lt;/A&gt; as a reference for your design:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="diazmarin09_0-1672870750041.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/206117iFC628712C7D6AF19/image-size/medium?v=v2&amp;amp;px=400" role="button" title="diazmarin09_0-1672870750041.png" alt="diazmarin09_0-1672870750041.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;I hope this information helps.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;David&lt;/P&gt;</description>
      <pubDate>Wed, 04 Jan 2023 22:19:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PF5020-Open-Drain-Outputs/m-p/1577481#M2331</guid>
      <dc:creator>diazmarin09</dc:creator>
      <dc:date>2023-01-04T22:19:31Z</dc:date>
    </item>
    <item>
      <title>Re: PF5020 Open Drain Outputs</title>
      <link>https://community.nxp.com/t5/Power-Management/PF5020-Open-Drain-Outputs/m-p/1577493#M2332</link>
      <description>&lt;P&gt;Hi David,&lt;BR /&gt;Yes I am using that and the SCH-50735 S32K3-T-Box EVM as a references. But both of them are using 3.3V MCUs and in our application, we are using S32K324 MCU which has 5V and 3.3V IO Domains. I am running out of 3.3V IOs from the S32K324 so I have to use the 5V IOs to read the OD outputs of the PF5020.&lt;/P&gt;</description>
      <pubDate>Wed, 04 Jan 2023 22:55:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PF5020-Open-Drain-Outputs/m-p/1577493#M2332</guid>
      <dc:creator>ThorVic</dc:creator>
      <dc:date>2023-01-04T22:55:28Z</dc:date>
    </item>
    <item>
      <title>Re: PF5020 Open Drain Outputs</title>
      <link>https://community.nxp.com/t5/Power-Management/PF5020-Open-Drain-Outputs/m-p/1578119#M2334</link>
      <description>&lt;P&gt;Hello Thor,&lt;/P&gt;
&lt;P&gt;If your main supply voltage is 5V, then, you can pull-up the INTB and PGOOD outputs to such level using a 100kΩ resistor.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;David&lt;/P&gt;</description>
      <pubDate>Thu, 05 Jan 2023 17:08:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PF5020-Open-Drain-Outputs/m-p/1578119#M2334</guid>
      <dc:creator>diazmarin09</dc:creator>
      <dc:date>2023-01-05T17:08:26Z</dc:date>
    </item>
  </channel>
</rss>