<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックRe: RDVCU5775EVM SBC problems</title>
    <link>https://community.nxp.com/t5/Power-Management/RDVCU5775EVM-SBC-problems/m-p/1562969#M2299</link>
    <description>&lt;P&gt;I have an issue with my VCU board ( RDVCU5775EVM) , I uploaded a BL into the Chip , there might be some error during the upload process, the board reset itself , and ever since the load, there is only one LED stay on( D55),&amp;nbsp; For D56,D57,D58,D59 will stay on for first second or so then turn off , I powered the VBAT , and GND , whenever power is supplied to SBC_WAKE , it is doing the same thing, it is doing the same thing regardless J1 jumper being open or closed. My question is for the SBC , is there anyways I can keep the power on so I can reload the BL ? during that split second, PE software able to recognize the chips, so I think it is SBC is doing something and shut the power to provide to the MCU.&lt;/P&gt;</description>
    <pubDate>Thu, 01 Dec 2022 18:50:32 GMT</pubDate>
    <dc:creator>Ckh091020</dc:creator>
    <dc:date>2022-12-01T18:50:32Z</dc:date>
    <item>
      <title>RDVCU5775EVM SBC problems</title>
      <link>https://community.nxp.com/t5/Power-Management/RDVCU5775EVM-SBC-problems/m-p/1154771#M1167</link>
      <description>&lt;P&gt;Hi, I'm using the RDVCU5775EVM board for BMS development, the board is connect the 12V power supply on connector J8's A11 and A21, when I power up with the jumper J1(SBC debug pin) attached, the board can power-up correctly(I have download the demo BMS program inside the MCU), and the promgramming is running, because the LED GPIO1&amp;amp;2&amp;nbsp; blink. But, when I remove the jumper J1, and power up board again, I can see the led D54(reset) blink several times and the board power down. I guess the KL15_WAKE is using for wake up the SBC and I try to connect the KL15_wake to +12V, the board just powered like 2 seconds and shut down as well.&lt;/P&gt;&lt;P&gt;So, my question is:&lt;/P&gt;&lt;P&gt;1, My connection correct or not?&lt;/P&gt;&lt;P&gt;2, Does LED D54 blink during reset term is correct?&amp;nbsp;&lt;/P&gt;&lt;P&gt;3, How to set up the SBC during reset term?&lt;/P&gt;&lt;P&gt;Thanks for helping!&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;</description>
      <pubDate>Thu, 17 Sep 2020 11:40:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/RDVCU5775EVM-SBC-problems/m-p/1154771#M1167</guid>
      <dc:creator>mayao999</dc:creator>
      <dc:date>2020-09-17T11:40:00Z</dc:date>
    </item>
    <item>
      <title>Re: RDVCU5775EVM SBC problems</title>
      <link>https://community.nxp.com/t5/Power-Management/RDVCU5775EVM-SBC-problems/m-p/1165213#M1192</link>
      <description>&lt;P&gt;I have forwarded these question to RDVCU5775EVM project owner and here there are the answers:&lt;/P&gt;
&lt;P&gt;1, My connection correct or not?&lt;BR /&gt;&lt;STRONG&gt;&lt;FONT color="#00FF00"&gt;Correct.&lt;/FONT&gt;&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;2, Does LED D54 blink during reset term is correct?&lt;BR /&gt;&lt;FONT color="#00FF00"&gt;&lt;STRONG&gt;It shouldn’t blink several times. That indicates the MCU failed to refresh the SBC watchdog during the 256ms from power-up in the non-debug mode.&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;3, How to set up the SBC during reset term?&lt;BR /&gt;&lt;FONT color="#00FF00"&gt;&lt;STRONG&gt;Make sure that MCU refreshes the SBC watchdog during the 256ms from power-up.&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#00FF00"&gt;&lt;STRONG&gt;Now the SDK-based project we provided has an issue that can’t refresh SBC watchdog first time under the O0 optimization level for GCC, I’m working on fixing this issue, suggest the user change the GCC optimization level to at least O1, that is ok I tested.&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 09 Oct 2020 13:06:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/RDVCU5775EVM-SBC-problems/m-p/1165213#M1192</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2020-10-09T13:06:33Z</dc:date>
    </item>
    <item>
      <title>Re: RDVCU5775EVM SBC problems</title>
      <link>https://community.nxp.com/t5/Power-Management/RDVCU5775EVM-SBC-problems/m-p/1165216#M1193</link>
      <description>&lt;P&gt;And also forwarding another his comment:&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#339966"&gt;&lt;STRONG&gt;I have reproduced this problem in SDK-based projects at the O0 level of GCC optimization, but it works at the O1, O2, and O3 levels.&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#339966"&gt;&lt;STRONG&gt;At the O0 level, it exceeds the maximum time 256ms of SBC first watchdog refresh, I'm working on fixing the issue.&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#339966"&gt;&lt;STRONG&gt;Current workaround: Change the GCC optimization level to at least O1.&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 09 Oct 2020 13:08:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/RDVCU5775EVM-SBC-problems/m-p/1165216#M1193</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2020-10-09T13:08:31Z</dc:date>
    </item>
    <item>
      <title>Re: RDVCU5775EVM SBC problems</title>
      <link>https://community.nxp.com/t5/Power-Management/RDVCU5775EVM-SBC-problems/m-p/1171767#M1211</link>
      <description>&lt;P&gt;Thanks David!&lt;/P&gt;</description>
      <pubDate>Thu, 22 Oct 2020 10:19:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/RDVCU5775EVM-SBC-problems/m-p/1171767#M1211</guid>
      <dc:creator>mayao999</dc:creator>
      <dc:date>2020-10-22T10:19:57Z</dc:date>
    </item>
    <item>
      <title>Re: RDVCU5775EVM SBC problems</title>
      <link>https://community.nxp.com/t5/Power-Management/RDVCU5775EVM-SBC-problems/m-p/1562969#M2299</link>
      <description>&lt;P&gt;I have an issue with my VCU board ( RDVCU5775EVM) , I uploaded a BL into the Chip , there might be some error during the upload process, the board reset itself , and ever since the load, there is only one LED stay on( D55),&amp;nbsp; For D56,D57,D58,D59 will stay on for first second or so then turn off , I powered the VBAT , and GND , whenever power is supplied to SBC_WAKE , it is doing the same thing, it is doing the same thing regardless J1 jumper being open or closed. My question is for the SBC , is there anyways I can keep the power on so I can reload the BL ? during that split second, PE software able to recognize the chips, so I think it is SBC is doing something and shut the power to provide to the MCU.&lt;/P&gt;</description>
      <pubDate>Thu, 01 Dec 2022 18:50:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/RDVCU5775EVM-SBC-problems/m-p/1562969#M2299</guid>
      <dc:creator>Ckh091020</dc:creator>
      <dc:date>2022-12-01T18:50:32Z</dc:date>
    </item>
  </channel>
</rss>