<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックFS86 Debug mode</title>
    <link>https://community.nxp.com/t5/Power-Management/FS86-Debug-mode/m-p/1537014#M2209</link>
    <description>&lt;P&gt;hi，&lt;/P&gt;&lt;P&gt;When the FS86 enters DEBUG mode through the DBG pin, can it skip the FS_INIT state without refreshing the watchdog?&lt;BR /&gt;At this time, the state of the FS0B pin and the RSTB pin is high or low.&lt;/P&gt;&lt;P&gt;thank you.&lt;/P&gt;</description>
    <pubDate>Thu, 13 Oct 2022 09:28:30 GMT</pubDate>
    <dc:creator>libra_z</dc:creator>
    <dc:date>2022-10-13T09:28:30Z</dc:date>
    <item>
      <title>FS86 Debug mode</title>
      <link>https://community.nxp.com/t5/Power-Management/FS86-Debug-mode/m-p/1537014#M2209</link>
      <description>&lt;P&gt;hi，&lt;/P&gt;&lt;P&gt;When the FS86 enters DEBUG mode through the DBG pin, can it skip the FS_INIT state without refreshing the watchdog?&lt;BR /&gt;At this time, the state of the FS0B pin and the RSTB pin is high or low.&lt;/P&gt;&lt;P&gt;thank you.&lt;/P&gt;</description>
      <pubDate>Thu, 13 Oct 2022 09:28:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS86-Debug-mode/m-p/1537014#M2209</guid>
      <dc:creator>libra_z</dc:creator>
      <dc:date>2022-10-13T09:28:30Z</dc:date>
    </item>
    <item>
      <title>Re: FS86 Debug mode</title>
      <link>https://community.nxp.com/t5/Power-Management/FS86-Debug-mode/m-p/1537377#M2211</link>
      <description>&lt;P&gt;No you can't do that,FS_INIT state can't be skipped.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 13 Oct 2022 23:14:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS86-Debug-mode/m-p/1537377#M2211</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2022-10-13T23:14:42Z</dc:date>
    </item>
    <item>
      <title>Re: FS86 Debug mode</title>
      <link>https://community.nxp.com/t5/Power-Management/FS86-Debug-mode/m-p/1538194#M2214</link>
      <description>&lt;P&gt;thank you for your reply.&lt;/P&gt;&lt;P&gt;According to the connection method in the figure, connect the DBG pin to VBOS through a diode to enter the debug mode. Can FS86 work normally at this time? Does the watchdog need to be refreshed in this mode to skip the INIT_FS state machine?&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="屏幕截图 2022-10-17 100722.png" style="width: 685px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/196871iF55EFD432A82DA66/image-size/large?v=v2&amp;amp;px=999" role="button" title="屏幕截图 2022-10-17 100722.png" alt="屏幕截图 2022-10-17 100722.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 17 Oct 2022 02:09:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS86-Debug-mode/m-p/1538194#M2214</guid>
      <dc:creator>libra_z</dc:creator>
      <dc:date>2022-10-17T02:09:50Z</dc:date>
    </item>
    <item>
      <title>Re: FS86 Debug mode</title>
      <link>https://community.nxp.com/t5/Power-Management/FS86-Debug-mode/m-p/1621521#M2526</link>
      <description>&lt;P&gt;Hello&lt;BR /&gt;A little bit support&lt;BR /&gt;&lt;SPAN class=""&gt;(V&lt;/SPAN&gt;&lt;SPAN class=""&gt;DBG &lt;/SPAN&gt;&lt;SPAN class=""&gt;= VBOS – Vd ≈ 4.5V) Entry the debug mode.&lt;BR /&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;SPAN class=""&gt;The DEBUG mode disables the Watchdog, lock FS0B low.&lt;BR /&gt;&lt;/SPAN&gt;In the InitFSstate, you cannot use the watchdog, and release the safety path pin FS0b.&lt;BR /&gt;If you want to use the device, you should switch it to NORMAL_FS where you need to refresh watchdog, exit debug mode, and release FS0b pin&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;Cuong&lt;/P&gt;</description>
      <pubDate>Fri, 24 Mar 2023 08:43:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS86-Debug-mode/m-p/1621521#M2526</guid>
      <dc:creator>cuongnguyenvan</dc:creator>
      <dc:date>2023-03-24T08:43:19Z</dc:date>
    </item>
  </channel>
</rss>