<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power Management中的主题 Re: FS26 Configuration Without Boost</title>
    <link>https://community.nxp.com/t5/Power-Management/FS26-Configuration-Without-Boost/m-p/1535062#M2190</link>
    <description>&lt;P&gt;Hi David!&lt;/P&gt;&lt;P&gt;Correct - I do not want to use the BOOST regulator.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Currently we have several samples of the FS26 that have OTP configuration factory set&amp;nbsp;&lt;SPAN&gt;VBST_CFG_OTP = 0. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is there any way we can use these samples without the boost?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 10 Oct 2022 18:37:40 GMT</pubDate>
    <dc:creator>michael86</dc:creator>
    <dc:date>2022-10-10T18:37:40Z</dc:date>
    <item>
      <title>FS26 Configuration Without Boost</title>
      <link>https://community.nxp.com/t5/Power-Management/FS26-Configuration-Without-Boost/m-p/1534069#M2184</link>
      <description>&lt;P&gt;Hello, The datasheet and application notes for the FS26 discuss using the boost in front end and back end mode.&lt;/P&gt;&lt;P&gt;1. There is an OTP setting&amp;nbsp;VBST_CFG_OTP with option to set to front-end or back-end. What should this setting be set to for no boost?&lt;/P&gt;&lt;P&gt;2.&amp;nbsp;We have part number FS2613 AMDA3AD. The datasheet says VBST_CFG_OTP is set to front-end. Does this mean if we remove the boost circuitry it will not work?&lt;/P&gt;&lt;P&gt;3. If VBST_CFG_OTP is set to front-end, can we&amp;nbsp;set VBSTDIS to 1 to disable the boost and not have the boost circuitry?&lt;/P&gt;&lt;P&gt;4. Is there other OTP or MCU configuration that needs to be done when not using the boost converter?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 07 Oct 2022 20:17:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS26-Configuration-Without-Boost/m-p/1534069#M2184</guid>
      <dc:creator>michael86</dc:creator>
      <dc:date>2022-10-07T20:17:24Z</dc:date>
    </item>
    <item>
      <title>Re: FS26 Configuration Without Boost</title>
      <link>https://community.nxp.com/t5/Power-Management/FS26-Configuration-Without-Boost/m-p/1535052#M2189</link>
      <description>&lt;P&gt;Hello Michael,&lt;/P&gt;
&lt;P&gt;I hope everything is great with you.&lt;/P&gt;
&lt;P&gt;Do you mean that, you do not want to use the BOOST regulator in your design? If that is the case, you may follow the recommendation below:&lt;/P&gt;
&lt;P&gt;Connection if not used:&lt;STRONG&gt; open when BOOST is used in back-end&lt;/STRONG&gt;.&lt;/P&gt;
&lt;P&gt;Please make sure VBST_CFG_OTP = 1 (back-end mode).&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope this information helps.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;David&lt;/P&gt;</description>
      <pubDate>Mon, 10 Oct 2022 17:44:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS26-Configuration-Without-Boost/m-p/1535052#M2189</guid>
      <dc:creator>diazmarin09</dc:creator>
      <dc:date>2022-10-10T17:44:58Z</dc:date>
    </item>
    <item>
      <title>Re: FS26 Configuration Without Boost</title>
      <link>https://community.nxp.com/t5/Power-Management/FS26-Configuration-Without-Boost/m-p/1535062#M2190</link>
      <description>&lt;P&gt;Hi David!&lt;/P&gt;&lt;P&gt;Correct - I do not want to use the BOOST regulator.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Currently we have several samples of the FS26 that have OTP configuration factory set&amp;nbsp;&lt;SPAN&gt;VBST_CFG_OTP = 0. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is there any way we can use these samples without the boost?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 10 Oct 2022 18:37:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS26-Configuration-Without-Boost/m-p/1535062#M2190</guid>
      <dc:creator>michael86</dc:creator>
      <dc:date>2022-10-10T18:37:40Z</dc:date>
    </item>
    <item>
      <title>Re: FS26 Configuration Without Boost</title>
      <link>https://community.nxp.com/t5/Power-Management/FS26-Configuration-Without-Boost/m-p/1536336#M2199</link>
      <description>&lt;P&gt;Hello Michael,&lt;/P&gt;
&lt;P&gt;Do you mean that your devices are already programmed?&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;David&lt;/P&gt;</description>
      <pubDate>Wed, 12 Oct 2022 14:47:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS26-Configuration-Without-Boost/m-p/1536336#M2199</guid>
      <dc:creator>diazmarin09</dc:creator>
      <dc:date>2022-10-12T14:47:21Z</dc:date>
    </item>
    <item>
      <title>Re: FS26 Configuration Without Boost</title>
      <link>https://community.nxp.com/t5/Power-Management/FS26-Configuration-Without-Boost/m-p/1545106#M2241</link>
      <description>&lt;P&gt;From NXP Apps:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;There is an OTP setting VBST_CFG_OTP with option to set to front-end or back-end. What should this setting be set to for no boost?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;STRONG&gt;WS: This should be configured as back-end mode.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;We have part number FS2613 AMDA3AD. The datasheet says VBST_CFG_OTP is set to front-end. Does this mean if we remove the boost circuitry it will not work?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;STRONG&gt;WS: Customer will anyway not be able to start up the device (see datasheet p.23, the state machine when VBST_CFG_OTP = 0). Do you know why did they choose this OTP if they don’t want to use the Boost controller ?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;If VBST_CFG_OTP is set to front-end, can we set VBSTDIS to 1 to disable the boost and not have the boost circuitry?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;STRONG&gt;WS: In order to do so, they would need to start up the device, have the RSTB released to allow the MCU to write in M_REG_CTRL2 register.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Unfortunately, as I explained in the previous bullet, the device will be stuck with no possibility to reach this point.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Is there other OTP or MCU configuration that needs to be done when not using the boost converter?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;STRONG&gt;WS: When the boost is not used, the OTP configuration needed is only to set VBST_CFG_OTP = 1 and VSUP_UVTH_OTP = 1. Of course, the unused pins must be handled as described in the datasheet p. 13, but the MCU has no action to take.&lt;/STRONG&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 27 Oct 2022 14:57:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS26-Configuration-Without-Boost/m-p/1545106#M2241</guid>
      <dc:creator>jbirchy</dc:creator>
      <dc:date>2022-10-27T14:57:40Z</dc:date>
    </item>
  </channel>
</rss>