<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PCA9420 Battery detection in-progress ? in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/PCA9420-Battery-detection-in-progress/m-p/1531596#M2177</link>
    <description>&lt;P&gt;Vbat should be clear DC voltage, don't understand why it has the frequency in your side.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 03 Oct 2022 11:33:37 GMT</pubDate>
    <dc:creator>guoweisun</dc:creator>
    <dc:date>2022-10-03T11:33:37Z</dc:date>
    <item>
      <title>PCA9420 Battery detection in-progress ?</title>
      <link>https://community.nxp.com/t5/Power-Management/PCA9420-Battery-detection-in-progress/m-p/1526486#M2166</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Our device adopts PCA9420UKZ to be pmic,&lt;BR /&gt;and charging source is Qi wireless charging,&lt;/P&gt;&lt;P&gt;When we charging battery by Qi wlc charger,&lt;BR /&gt;if antennas aren't aligned very accurately,&lt;BR /&gt;even charger feels everhthing is right and keep power output,&lt;/P&gt;&lt;P&gt;the pca9420 would stop charging because it falled into a state "Battery detection in-progress",&lt;BR /&gt;(CHG_STATUS_2(1Ah) = 0x10, "Battery detection in-progress", "Charger in Idle State")&lt;/P&gt;&lt;P&gt;but at the sametime, register reveals pca9420 has detected battery,&lt;BR /&gt;(CHG_STATUS_0(18h) = 0xf0, "VBAT_DET_OK = 1", "VBAT_OK = 1")&lt;/P&gt;&lt;P&gt;Detailed register values:&lt;/P&gt;&lt;PRE&gt;0x01=0x00, 0x02=0x00, 0x03=0x3f, 0x04=0x00,
0x05=0x7f, 0x06=0x00, 0x07=0xff, 0x08=0xff,
0x09=0x41, 0x0a=0x81, 0x0b=0xce, 0x0c=0x01,
0x0d=0x00, 0x10=0xaf, 0x11=0x14, 0x12=0x02,
0x13=0x13, 0x14=0x0a, 0x15=0x25, 0x16=0x95,
0x17=0x24, 0x18=0xf0, 0x19=0xc0, 0x1a=0x10,
0x1b=0x00, 0x20=0x10, 0x21=0x00, 0x22=0x14,
0x23=0x2c, 0x24=0x41, 0x25=0x2c, 0x26=0x1c,
0x27=0x4c, 0x28=0x4f, 0x29=0x0c, 0x2a=0x1c,
0x2b=0x4c, 0x2c=0x4f, 0x2d=0x0c, 0x2e=0x1c,
0x2f=0x4c, 0x30=0x4f, 0x31=0x0c&lt;/PRE&gt;&lt;P&gt;datasheet of pca9420 mentioned the battery detection sqquence at "Figure 10. Charger state diagram",&amp;nbsp;&lt;BR /&gt;but we still have no idea how pca9420 to have suceh state,&lt;BR /&gt;because seems the voltage we measured doesn't match the conditions of document description,&lt;/P&gt;&lt;P&gt;So we do like to consult more detailed of the "Battery detection in-progress",&lt;BR /&gt;How it happened?&lt;BR /&gt;Do we have way to know the truly VBAT voltage what pca9420 detected?&lt;BR /&gt;Any suggestion to investigate more forward?&lt;/P&gt;&lt;P&gt;2022-09-30:&lt;BR /&gt;Try to measure VBAT voltage by o&lt;SPAN&gt;scilloscope,&lt;BR /&gt;the voltage has ~0.1V gap between 2 case,&lt;BR /&gt;but when wlc charger isn't aligned perfectly, the frquency is ~37Hz only,&lt;BR /&gt;compare to aligned perfectly case, the frequency is very low,&lt;BR /&gt;is't caused pca9420 can't detect battery?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thanks~&lt;/P&gt;</description>
      <pubDate>Fri, 30 Sep 2022 03:08:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PCA9420-Battery-detection-in-progress/m-p/1526486#M2166</guid>
      <dc:creator>akckwang</dc:creator>
      <dc:date>2022-09-30T03:08:09Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9420 Battery detection in-progress ?</title>
      <link>https://community.nxp.com/t5/Power-Management/PCA9420-Battery-detection-in-progress/m-p/1527880#M2168</link>
      <description>&lt;P&gt;The device has a unique battery detection scheme with two comparators, 1.9V and 3.4V.&lt;BR /&gt;when the detection scheme is executed, a 5mA current sink is activated to determine&lt;BR /&gt;battery presence by detection the fall threshold, VBAT_DET_LOW, 1.9V typ. In addition,&lt;BR /&gt;a 5mA current source is used to detect battery voltage whether it stays above the&lt;BR /&gt;threshold, VBAT_DET_UP, 3.4V. if both conditions are met, absence of battery is declared.&lt;/P&gt;</description>
      <pubDate>Mon, 26 Sep 2022 06:33:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PCA9420-Battery-detection-in-progress/m-p/1527880#M2168</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2022-09-26T06:33:13Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9420 Battery detection in-progress ?</title>
      <link>https://community.nxp.com/t5/Power-Management/PCA9420-Battery-detection-in-progress/m-p/1528026#M2169</link>
      <description>&lt;P&gt;Hi Guoweisun,&lt;BR /&gt;Your reply is exactly what pca9420 document Figured 10 mentioned,&lt;BR /&gt;and that can't explain why our pca9420 can't detect battery event VBAT is stable ~3.9V...&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 26 Sep 2022 09:09:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PCA9420-Battery-detection-in-progress/m-p/1528026#M2169</guid>
      <dc:creator>akckwang</dc:creator>
      <dc:date>2022-09-26T09:09:49Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9420 Battery detection in-progress ?</title>
      <link>https://community.nxp.com/t5/Power-Management/PCA9420-Battery-detection-in-progress/m-p/1530829#M2172</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/138749"&gt;@guoweisun&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;If VBAT freuency drop to ~37Hz, can pca9420 still detect battery normally?&lt;/P&gt;&lt;P&gt;We measured VBAT by&amp;nbsp;oscilloscope,&lt;BR /&gt;and noticed that when wlc charger isn't aligned perfectly,&lt;BR /&gt;the VBAT voltage has ~0.1V drop compare to normal case,&lt;BR /&gt;but frequency is droped to ~37Hz.&lt;/P&gt;&lt;P&gt;Thanks~&lt;/P&gt;</description>
      <pubDate>Fri, 30 Sep 2022 03:18:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PCA9420-Battery-detection-in-progress/m-p/1530829#M2172</guid>
      <dc:creator>akckwang</dc:creator>
      <dc:date>2022-09-30T03:18:16Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9420 Battery detection in-progress ?</title>
      <link>https://community.nxp.com/t5/Power-Management/PCA9420-Battery-detection-in-progress/m-p/1531596#M2177</link>
      <description>&lt;P&gt;Vbat should be clear DC voltage, don't understand why it has the frequency in your side.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 03 Oct 2022 11:33:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PCA9420-Battery-detection-in-progress/m-p/1531596#M2177</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2022-10-03T11:33:37Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9420 Battery detection in-progress ?</title>
      <link>https://community.nxp.com/t5/Power-Management/PCA9420-Battery-detection-in-progress/m-p/1531878#M2178</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/138749"&gt;@guoweisun&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Can pca9420 battery detection work with the "strange frequency" dc voltage?&lt;/P&gt;&lt;P&gt;Thanks~&lt;/P&gt;</description>
      <pubDate>Tue, 04 Oct 2022 02:41:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PCA9420-Battery-detection-in-progress/m-p/1531878#M2178</guid>
      <dc:creator>akckwang</dc:creator>
      <dc:date>2022-10-04T02:41:21Z</dc:date>
    </item>
  </channel>
</rss>