<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックRe: PCA9420 - general questions</title>
    <link>https://community.nxp.com/t5/Power-Management/PCA9420-general-questions/m-p/1525187#M2161</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/35448"&gt;@reyes&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using PCA9849 i2c MUX to connect the 2 camera modules to IMX8MP&lt;/P&gt;&lt;P&gt;It automatically detects the channel ID when the device is connected.(say if module is connected to channel 1, control register status returns 0x04 and if module is connected to channel 2, control register status returns 0x05).&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Charles3_0-1663692983294.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/194341iF32C8AF1D6302B74/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Charles3_0-1663692983294.png" alt="Charles3_0-1663692983294.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here I'm able to control the channel 1 device by default. But if I have to point the MUX to channel 2, what I have to do?&lt;/P&gt;&lt;P&gt;I have tried to set the control status register to 0x05 using i2c-tools (i2cset -f -y 2 0x71 0x0000 0x05).&lt;/P&gt;&lt;P&gt;But still it is not pointed to channel 2.&lt;BR /&gt;Is there anyways to handle it from the mux driver?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Charles&lt;/P&gt;</description>
    <pubDate>Tue, 20 Sep 2022 16:58:44 GMT</pubDate>
    <dc:creator>Amal_Antony3331</dc:creator>
    <dc:date>2022-09-20T16:58:44Z</dc:date>
    <item>
      <title>PCA9420 - general questions</title>
      <link>https://community.nxp.com/t5/Power-Management/PCA9420-general-questions/m-p/1074281#M1030</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HelloTeam,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My customer has the following inquiries, could you please comment them see below, Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. There is any way to receive different&amp;nbsp;default settings (from the factory) such as Buck1 to be 1.2V?&lt;/P&gt;&lt;P&gt;2. There is a way to use a&amp;nbsp;selective i2c address to cascade multiple pca9420 devices on one bus?&lt;/P&gt;&lt;P&gt;3. Could you please confirm that LDO1&amp;nbsp;is&amp;nbsp;only 1mA?&lt;/P&gt;&lt;P&gt;4. on page 3 at the datasheet&amp;nbsp;@&lt;A class="link-titled" href="https://www.nxp.com/docs/en/data-sheet/PCA9420DS.pdf" title="https://www.nxp.com/docs/en/data-sheet/PCA9420DS.pdf"&gt;https://www.nxp.com/docs/en/data-sheet/PCA9420DS.pdf&lt;/A&gt;&amp;nbsp;, the AGND1/2/3 connected to the GND, could you please explain why there is need for an analog ground and for shorting between them?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;waiting for your kind response, Thanks in advance.&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Shai&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Aug 2020 12:37:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PCA9420-general-questions/m-p/1074281#M1030</guid>
      <dc:creator>shai_b</dc:creator>
      <dc:date>2020-08-07T12:37:43Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9420 - general questions</title>
      <link>https://community.nxp.com/t5/Power-Management/PCA9420-general-questions/m-p/1074282#M1031</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Shai,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please find my answer to your questions below:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;[A1] The default value for SW1 _OUT_0[5:0] is set at 1.00V, but it should be MTP programmable, this means that you can change it via I2C.&lt;/P&gt;&lt;P&gt;I understand that your customer wants a different default preprogrammed version of the PMIC, maybe this can be arranged depending on the opportunity, for this task I recommend you to contact your local NXP Sales representative directly for a discussion about this topic.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;[A2] There are only two option for i2c address on the PCA9420 device, the slave address is set as in table 6 of the datasheet, where Bit7 is fixed to ‘1’, Bit6 is fixed to ‘1’, Bit5 is fixed to ‘0’, Bit4 is configurable, Bit3 is fixed to ‘0’, Bit2 is fixed to ‘0’, Bit1 is fixed to ‘1’, and Bit0 is read/write bit.&lt;/P&gt;&lt;P&gt;Bit 4 should be reserved as MTP option, with its default value set as “0” but can be trimmed to “1” when needed.&lt;/P&gt;&lt;P&gt;If more than two are needed, maybe an I2C MUX device placed between the MPU and the PMICs can be an option.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;[A3] Correct, LDO1 max output current is up to 1mA.&lt;/P&gt;&lt;P&gt;Take in mind that LDO1 is an Always-on LDO, so it is typically used to supply the VDD_AO1V8 pin of the i.MXRT600, which need a 1.8V supply for “always on” features (RTC, RESETN, LDO_ENABLE, PMIC_IRQ_N, PMIC_MODE0, and PMIC_MODE1).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;[A4] Analog Grounds and Power Grounds, should not be connected on the top PCB layer. We recommend to separate the grounds so the PGND of the Switching regulators are short and the return pad/loop of the switching regulators are closed to the output components this way you avoid noise caused by the power switching all around the board.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;AGNDs and PGND should be connected/shorted in PCB inner GND layer.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Jose&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Aug 2020 18:34:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PCA9420-general-questions/m-p/1074282#M1031</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2020-08-07T18:34:24Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9420 - general questions</title>
      <link>https://community.nxp.com/t5/Power-Management/PCA9420-general-questions/m-p/1179692#M1234</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/35448"&gt;@reyes&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Could you please advise the following questions below:&lt;/P&gt;&lt;P&gt;1.&amp;nbsp; Please advise if the customer latch always-on at the ON pin, could this lead to reset the device, or may it cause other phenomena?&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. About the BIT4 for changing the I2C address to able to run two devices in parallel, please advise how to configure/trim BIT4 to “1”?.&lt;/P&gt;&lt;P&gt;Waiting for your kind response, Thanks a lot.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Shai&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 07 Nov 2020 10:28:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PCA9420-general-questions/m-p/1179692#M1234</guid>
      <dc:creator>shai_b</dc:creator>
      <dc:date>2020-11-07T10:28:16Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9420 - general questions</title>
      <link>https://community.nxp.com/t5/Power-Management/PCA9420-general-questions/m-p/1183120#M1237</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/35448" target="_blank"&gt;@reyes&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Could you please advise the following questions below:&lt;/P&gt;&lt;P&gt;1.&amp;nbsp; Please advise if the customer latch always-on at the ON pin, could this lead to reset the device, or may it cause other phenomena?&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. About the BIT4 for changing the I2C address to able to run two devices in parallel, please advise how to configure/trim BIT4 to “1”?.&lt;/P&gt;&lt;P&gt;Waiting for your kind response, Thanks a lot.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Shai&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 13 Nov 2020 11:51:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PCA9420-general-questions/m-p/1183120#M1237</guid>
      <dc:creator>shai_b</dc:creator>
      <dc:date>2020-11-13T11:51:13Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9420 - general questions</title>
      <link>https://community.nxp.com/t5/Power-Management/PCA9420-general-questions/m-p/1525187#M2161</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/35448"&gt;@reyes&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using PCA9849 i2c MUX to connect the 2 camera modules to IMX8MP&lt;/P&gt;&lt;P&gt;It automatically detects the channel ID when the device is connected.(say if module is connected to channel 1, control register status returns 0x04 and if module is connected to channel 2, control register status returns 0x05).&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Charles3_0-1663692983294.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/194341iF32C8AF1D6302B74/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Charles3_0-1663692983294.png" alt="Charles3_0-1663692983294.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here I'm able to control the channel 1 device by default. But if I have to point the MUX to channel 2, what I have to do?&lt;/P&gt;&lt;P&gt;I have tried to set the control status register to 0x05 using i2c-tools (i2cset -f -y 2 0x71 0x0000 0x05).&lt;/P&gt;&lt;P&gt;But still it is not pointed to channel 2.&lt;BR /&gt;Is there anyways to handle it from the mux driver?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Charles&lt;/P&gt;</description>
      <pubDate>Tue, 20 Sep 2022 16:58:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PCA9420-general-questions/m-p/1525187#M2161</guid>
      <dc:creator>Amal_Antony3331</dc:creator>
      <dc:date>2022-09-20T16:58:44Z</dc:date>
    </item>
  </channel>
</rss>