<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: High Voltage Motor Control Platform - Javascript error in the FreeMASTER  ACIM demo app in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/High-Voltage-Motor-Control-Platform-Javascript-error-in-the/m-p/1520204#M2144</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;yes, I am using &lt;A href="https://mcuxpresso.nxp.com/en/builder?hw=HVP-KV46F150M&amp;amp;rel=366" target="_blank" rel="noopener nofollow noreferrer"&gt;HVP-KV46F (2.8.0)&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and I reloaded it again, remembering to tick the&amp;nbsp; freemaster&amp;nbsp; tickbox, and now found acim.pmp.&lt;/P&gt;&lt;P&gt;However, when I run it, I still see this message:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="johnwood101_1-1662796712579.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/193202i237AC972F38D4EBB/image-size/medium?v=v2&amp;amp;px=400" role="button" title="johnwood101_1-1662796712579.png" alt="johnwood101_1-1662796712579.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;johnwood101_1-1662796712579.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It looks like the error is to do with Javascript.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;( The&amp;nbsp; old&amp;nbsp; 2017&amp;nbsp;&amp;nbsp; acim_ref_sol.pmp&amp;nbsp; which came with&lt;/P&gt;&lt;P&gt;High Voltage Motor Control Platform&amp;nbsp;&amp;nbsp; software&lt;/P&gt;&lt;P&gt;does not show this error,&amp;nbsp; so it must me something introduced&lt;/P&gt;&lt;P&gt;between the two version of the&amp;nbsp; .pmp file. )&lt;/P&gt;&lt;P&gt;Please could you tell me which version of Windows is it that&lt;/P&gt;&lt;P&gt;the acim.pmp &amp;nbsp; is running on for you?&amp;nbsp;&lt;/P&gt;&lt;P&gt;( the acim.pmp&amp;nbsp; which comes with &lt;A href="https://mcuxpresso.nxp.com/en/builder?hw=HVP-KV46F150M&amp;amp;rel=366" target="_blank" rel="noopener nofollow noreferrer"&gt;HVP-KV46F (2.8.0))&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I will go and buy a bare metal Windows machine to check if it works.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sat, 10 Sep 2022 08:01:53 GMT</pubDate>
    <dc:creator>johnwood101</dc:creator>
    <dc:date>2022-09-10T08:01:53Z</dc:date>
    <item>
      <title>High Voltage Motor Control Platform - Javascript error in the FreeMASTER  ACIM demo app</title>
      <link>https://community.nxp.com/t5/Power-Management/High-Voltage-Motor-Control-Platform-Javascript-error-in-the/m-p/1513616#M2124</link>
      <description>&lt;P&gt;I bought the High Voltage Motor Control Platform with the&lt;/P&gt;&lt;P&gt;HVPKV46F150MUG_high_voltage_processor_module.&lt;/P&gt;&lt;P&gt;The firmware compiled and uploaded OK with latest Linux&amp;nbsp; MCUxpresso ide&lt;/P&gt;&lt;P&gt;and installing&amp;nbsp; the&lt;/P&gt;&lt;P&gt;SDK_2.x_HVP-K46F150M&lt;/P&gt;&lt;P&gt;into the ide and then importing&amp;nbsp;&amp;nbsp; acim&amp;nbsp; example via&amp;nbsp; "Import SDK examples" option.&lt;/P&gt;&lt;P&gt;No problems with the compile / firmware upload.&lt;/P&gt;&lt;P&gt;Tried to power up the motor with FreeMASTER 3.2 - running under Virtualbox Windows VM&lt;/P&gt;&lt;P&gt;using an old (2017) copy of&lt;/P&gt;&lt;P&gt;acim_ref_sol.pmp.&amp;nbsp; It connected correctly at 19,200 baud&amp;nbsp; but with a lot of non-javascript 'missing freemaster variables errors',&lt;/P&gt;&lt;P&gt;but it would spin the motor.&amp;nbsp; I couldn't complete the motor tests because of the missing variables. It would just report crazy negative estimated speeds.&lt;/P&gt;&lt;P&gt;Now, I tried instead the&amp;nbsp; same&amp;nbsp; acim.pmp&amp;nbsp; which came with the above SDK.&lt;/P&gt;&lt;P&gt;Even though it does connect over UART at 19200, it doesnt run at all because&lt;/P&gt;&lt;P&gt;I just get the following error, and the GUI is not operational&lt;/P&gt;&lt;P&gt;--- See attachment for image of error&lt;/P&gt;&lt;P&gt;Is there a newer version of ACIM or anything else I can try.&lt;/P&gt;&lt;P&gt;Strangely,&amp;nbsp; even the old&amp;nbsp;&amp;nbsp; acim_ref_sol.pmp&amp;nbsp;&amp;nbsp; which used to&amp;nbsp; kind-of run,&lt;/P&gt;&lt;P&gt;now reports these same javascript errors as in the attachment.&lt;/P&gt;&lt;P&gt;thanks for looking at this.&lt;/P&gt;&lt;P&gt;I can't really get past this error.&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;</description>
      <pubDate>Tue, 30 Aug 2022 06:14:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/High-Voltage-Motor-Control-Platform-Javascript-error-in-the/m-p/1513616#M2124</guid>
      <dc:creator>johnwood101</dc:creator>
      <dc:date>2022-08-30T06:14:46Z</dc:date>
    </item>
    <item>
      <title>Re: High Voltage Motor Control Platform - Javascript error in the FreeMASTER  ACIM demo app</title>
      <link>https://community.nxp.com/t5/Power-Management/High-Voltage-Motor-Control-Platform-Javascript-error-in-the/m-p/1517103#M2132</link>
      <description>&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;Just to clarify, I'm assuming you're using the &lt;A href="https://www.nxp.com/docs/en/user-guide/ACIMKV46DEMOUG.pdf" target="_blank" rel="noopener"&gt;ACIMKV46DEMOUG&lt;/A&gt; User's Guide as a reference.&lt;/P&gt;
&lt;P&gt;On the other hand, I recommend you to use FreeMASTER tool 3.1 – Linux installer instead of using Virtualbox Window, you can download it from &lt;A href="https://www.nxp.com/design/software/development-software/freemaster-run-time-debugging-tool:FREEMASTER" target="_blank" rel="noopener"&gt;FreeMASTER Run-Time Debugging Tool&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Hope it helps you. Please let me know if you have more questions about it.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 05 Sep 2022 13:52:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/High-Voltage-Motor-Control-Platform-Javascript-error-in-the/m-p/1517103#M2132</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2022-09-05T13:52:47Z</dc:date>
    </item>
    <item>
      <title>Re: High Voltage Motor Control Platform - Javascript error in the FreeMASTER  ACIM demo app</title>
      <link>https://community.nxp.com/t5/Power-Management/High-Voltage-Motor-Control-Platform-Javascript-error-in-the/m-p/1517573#M2135</link>
      <description>&lt;P&gt;Yes, I am working from instructions in &lt;A href="https://www.nxp.com/docs/en/user-guide/ACIMKV46DEMOUG.pdf" target="_blank" rel="noopener nofollow noreferrer"&gt;ACIMKV46DEMOUG&lt;/A&gt;&amp;nbsp; which seems to date from 2020.&lt;/P&gt;&lt;P&gt;but I cannot find a recent&amp;nbsp;&amp;nbsp;acim_ref_sol.pmp&amp;nbsp; file&amp;nbsp; to operate the the demo.&lt;/P&gt;&lt;P&gt;The only one I can find is from 2017 as comes as part of MCRSP_ACIM_V1.2.0&lt;/P&gt;&lt;P&gt;This 2017 software expects to be installed on Kinetis Design Studio 3.2.0.&lt;/P&gt;&lt;P&gt;When I compile under KDS, the firmware doesnt run --- communication cannot be established with Freemaster.&lt;/P&gt;&lt;P&gt;If I build the more recent&amp;nbsp; MCUexpressoIDE&amp;nbsp;&amp;nbsp; ACIM project,&amp;nbsp; the&amp;nbsp; firmware does run, but I believe that now the&amp;nbsp; old&amp;nbsp; 2017&amp;nbsp; acim_ref_sol.pmp&amp;nbsp;&amp;nbsp; is&amp;nbsp; not properly compatible with this firmware - and hence the warning messages about unknown&amp;nbsp; FreeMASTER variables.&lt;/P&gt;&lt;P&gt;When I try to setup a motor, the sensorless mode doesnt run correctly (it only works about 400rpm).&lt;/P&gt;&lt;P&gt;I tried FreeMASTER3.1 but on Linux, it only installed the&amp;nbsp; LITE version, not the full version.&lt;/P&gt;&lt;P&gt;I think if I had an &amp;nbsp; acim_ref_sol.pmp&amp;nbsp;&amp;nbsp;&amp;nbsp; which is more up to date then my problems would be over.&lt;/P&gt;&lt;P&gt;( The latest SDK for MCUexpressoIDE to match for the&amp;nbsp; hvpkv46f&amp;nbsp; does not include a new&amp;nbsp; pmp file.)&lt;/P&gt;&lt;P&gt;I found one called&amp;nbsp;&amp;nbsp; acim.pmp&amp;nbsp; somewhere on the internet but this does not work.&lt;/P&gt;&lt;P&gt;I think if you had an newer&amp;nbsp;&amp;nbsp; acim_ref_sol.pmp&amp;nbsp;&amp;nbsp; to match the&amp;nbsp; MCUexpressoIDE ACIM demo, then my problems would be over.&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 06 Sep 2022 09:06:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/High-Voltage-Motor-Control-Platform-Javascript-error-in-the/m-p/1517573#M2135</guid>
      <dc:creator>johnwood101</dc:creator>
      <dc:date>2022-09-06T09:06:12Z</dc:date>
    </item>
    <item>
      <title>Re: High Voltage Motor Control Platform - Javascript error in the FreeMASTER  ACIM demo app</title>
      <link>https://community.nxp.com/t5/Power-Management/High-Voltage-Motor-Control-Platform-Javascript-error-in-the/m-p/1520178#M2143</link>
      <description>&lt;P&gt;Sorry, what version of SDK are you using? Since the SDK for &lt;A href="https://mcuxpresso.nxp.com/en/builder?hw=HVP-KV46F150M&amp;amp;rel=366" target="_blank" rel="noopener"&gt;HVP-KV46F (2.8.0)&lt;/A&gt; does have the .pmp file in the following path:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="nxf86756_0-1662771050414.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/193200iE84F3B3B1C7BC44B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="nxf86756_0-1662771050414.png" alt="nxf86756_0-1662771050414.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;nxf86756_0-1662771050414.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;On the other hand, I must admit that I am working on Windows and we have not tested anything about this on virtual machines on Linux.&lt;/P&gt;
&lt;P&gt;If you still have questions regarding FreeMASTER, I recommend you ask in the &lt;A href="https://community.nxp.com/community/freemaster?_gl=1*139bpkw*_ga*MTMzOTkyMzkxNS4xNjYyNzcxMzUx*_ga_WM5LE0KMSH*MTY2Mjc3MTM1MS4xLjEuMTY2Mjc3MTQ5My4wLjAuMA.." target="_blank" rel="noopener"&gt;FreeMASTER Community&lt;/A&gt; where our experts in this tool can help you in more detail.&lt;/P&gt;</description>
      <pubDate>Sat, 10 Sep 2022 01:01:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/High-Voltage-Motor-Control-Platform-Javascript-error-in-the/m-p/1520178#M2143</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2022-09-10T01:01:31Z</dc:date>
    </item>
    <item>
      <title>Re: High Voltage Motor Control Platform - Javascript error in the FreeMASTER  ACIM demo app</title>
      <link>https://community.nxp.com/t5/Power-Management/High-Voltage-Motor-Control-Platform-Javascript-error-in-the/m-p/1520204#M2144</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;yes, I am using &lt;A href="https://mcuxpresso.nxp.com/en/builder?hw=HVP-KV46F150M&amp;amp;rel=366" target="_blank" rel="noopener nofollow noreferrer"&gt;HVP-KV46F (2.8.0)&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and I reloaded it again, remembering to tick the&amp;nbsp; freemaster&amp;nbsp; tickbox, and now found acim.pmp.&lt;/P&gt;&lt;P&gt;However, when I run it, I still see this message:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="johnwood101_1-1662796712579.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/193202i237AC972F38D4EBB/image-size/medium?v=v2&amp;amp;px=400" role="button" title="johnwood101_1-1662796712579.png" alt="johnwood101_1-1662796712579.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;johnwood101_1-1662796712579.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It looks like the error is to do with Javascript.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;( The&amp;nbsp; old&amp;nbsp; 2017&amp;nbsp;&amp;nbsp; acim_ref_sol.pmp&amp;nbsp; which came with&lt;/P&gt;&lt;P&gt;High Voltage Motor Control Platform&amp;nbsp;&amp;nbsp; software&lt;/P&gt;&lt;P&gt;does not show this error,&amp;nbsp; so it must me something introduced&lt;/P&gt;&lt;P&gt;between the two version of the&amp;nbsp; .pmp file. )&lt;/P&gt;&lt;P&gt;Please could you tell me which version of Windows is it that&lt;/P&gt;&lt;P&gt;the acim.pmp &amp;nbsp; is running on for you?&amp;nbsp;&lt;/P&gt;&lt;P&gt;( the acim.pmp&amp;nbsp; which comes with &lt;A href="https://mcuxpresso.nxp.com/en/builder?hw=HVP-KV46F150M&amp;amp;rel=366" target="_blank" rel="noopener nofollow noreferrer"&gt;HVP-KV46F (2.8.0))&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I will go and buy a bare metal Windows machine to check if it works.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 10 Sep 2022 08:01:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/High-Voltage-Motor-Control-Platform-Javascript-error-in-the/m-p/1520204#M2144</guid>
      <dc:creator>johnwood101</dc:creator>
      <dc:date>2022-09-10T08:01:53Z</dc:date>
    </item>
    <item>
      <title>Re: High Voltage Motor Control Platform - Javascript error in the FreeMASTER  ACIM demo app</title>
      <link>https://community.nxp.com/t5/Power-Management/High-Voltage-Motor-Control-Platform-Javascript-error-in-the/m-p/1520629#M2149</link>
      <description>&lt;P&gt;Windows 10&lt;/P&gt;</description>
      <pubDate>Mon, 12 Sep 2022 15:35:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/High-Voltage-Motor-Control-Platform-Javascript-error-in-the/m-p/1520629#M2149</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2022-09-12T15:35:24Z</dc:date>
    </item>
    <item>
      <title>Re: High Voltage Motor Control Platform - Javascript error in the FreeMASTER  ACIM demo app</title>
      <link>https://community.nxp.com/t5/Power-Management/High-Voltage-Motor-Control-Platform-Javascript-error-in-the/m-p/1525581#M2164</link>
      <description>&lt;P&gt;thanks for your help.&amp;nbsp; I have it running correctly now on the Windows machine,&amp;nbsp; but after motor identification,&amp;nbsp; the control is not stable below 300rpm on a 1500rpm 0.55kW ACIM in sensorless FOC .&lt;/P&gt;&lt;P&gt;I had previously tried ST's motion control development system X-Cube-MCSDK and had the same problem with it's FOC algorithm, so this is not unique to NXP&amp;nbsp; / Freescale&amp;nbsp; code.&lt;/P&gt;&lt;P&gt;I've also tried a commerical Invertek inverter&amp;nbsp; which works correctly, and just now I tested the TI&amp;nbsp; InstaSPIN HV development kit on Windows, and it will run the same motor stably down to 20rpm,&amp;nbsp; so&amp;nbsp; I think I'll be using the&amp;nbsp; TMDSCNCD280049C&amp;nbsp; processor for this project.&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;</description>
      <pubDate>Wed, 21 Sep 2022 06:45:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/High-Voltage-Motor-Control-Platform-Javascript-error-in-the/m-p/1525581#M2164</guid>
      <dc:creator>johnwood101</dc:creator>
      <dc:date>2022-09-21T06:45:24Z</dc:date>
    </item>
  </channel>
</rss>