<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Having a problem initializing the MC33771 in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/Having-a-problem-initializing-the-MC33771/m-p/861400#M214</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;I have written code to talk to the MC33771 part. After initialization of the INIT register I can read registers and get what appears to be good data with valid CRCs without fail for what appears to be exactly 1 second and then I begin getting invalid replies.&amp;nbsp; I'm using the SPI port. What I'm looking for is any ideas as to whether the 1 second timeout is normal or is a clue for what I am doing wrong.&amp;nbsp; Shouldn't the chip keep&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;responding&lt;/SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;indefinitely after proper initialization?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Investigating further I figured out a little bit more.&amp;nbsp; As mentioned above, I can do an initialization sequence and immediately follow that with good reads.&amp;nbsp; If I wait a second, subsequent reads are invalid. They are all 0's with what is probably a good crc on it, but useless as far as reading a register.&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;What I learned just now is that, after it starts failing, if I issue another read to the INIT register but using the CID-unassigned value of all 0's, it responds properly. The INIT register is a good place to experiment because it can be read using CID=0 when unassigned and CID=xx after assigning the address to it.&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;So, it's as if it has forgotten that I assigned the device with the CID address in the init sequence if I wait long enough.&amp;nbsp; Under what circumstances can the part forget it's CID address?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 08 Jan 2019 20:23:32 GMT</pubDate>
    <dc:creator>rogerdavis_mitr</dc:creator>
    <dc:date>2019-01-08T20:23:32Z</dc:date>
    <item>
      <title>Having a problem initializing the MC33771</title>
      <link>https://community.nxp.com/t5/Power-Management/Having-a-problem-initializing-the-MC33771/m-p/861400#M214</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;I have written code to talk to the MC33771 part. After initialization of the INIT register I can read registers and get what appears to be good data with valid CRCs without fail for what appears to be exactly 1 second and then I begin getting invalid replies.&amp;nbsp; I'm using the SPI port. What I'm looking for is any ideas as to whether the 1 second timeout is normal or is a clue for what I am doing wrong.&amp;nbsp; Shouldn't the chip keep&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;responding&lt;/SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;indefinitely after proper initialization?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Investigating further I figured out a little bit more.&amp;nbsp; As mentioned above, I can do an initialization sequence and immediately follow that with good reads.&amp;nbsp; If I wait a second, subsequent reads are invalid. They are all 0's with what is probably a good crc on it, but useless as far as reading a register.&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;What I learned just now is that, after it starts failing, if I issue another read to the INIT register but using the CID-unassigned value of all 0's, it responds properly. The INIT register is a good place to experiment because it can be read using CID=0 when unassigned and CID=xx after assigning the address to it.&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;So, it's as if it has forgotten that I assigned the device with the CID address in the init sequence if I wait long enough.&amp;nbsp; Under what circumstances can the part forget it's CID address?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Jan 2019 20:23:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Having-a-problem-initializing-the-MC33771/m-p/861400#M214</guid>
      <dc:creator>rogerdavis_mitr</dc:creator>
      <dc:date>2019-01-08T20:23:32Z</dc:date>
    </item>
    <item>
      <title>Re: Having a problem initializing the MC33771</title>
      <link>https://community.nxp.com/t5/Power-Management/Having-a-problem-initializing-the-MC33771/m-p/861401#M215</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Roger,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It sounds like COM timeout reset which is enabled by default:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/74098i2E539FB3BB17FCF5/image-size/large?v=v2&amp;amp;px=999" title="COM timeout.png" alt="COM timeout.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/74208iEC3212E3E816ED33/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jan 2019 09:34:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Having-a-problem-initializing-the-MC33771/m-p/861401#M215</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2019-01-09T09:34:17Z</dc:date>
    </item>
    <item>
      <title>Re: Having a problem initializing the MC33771</title>
      <link>https://community.nxp.com/t5/Power-Management/Having-a-problem-initializing-the-MC33771/m-p/861402#M216</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi，Tomas,&lt;/P&gt;&lt;P&gt;we have some problems about MC33771 initializing, it always failed with a return&amp;nbsp; value CRC_STATUS.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The second question is about SPI communication, we use the driver software from&amp;nbsp;BCC_S32K144_Monitoring&amp;nbsp; NXP official website, we can detect the signal of CSB , CLK , but none of&amp;nbsp; DATA_OUT, so we are looking foward for your suggestion.&lt;/P&gt;&lt;P&gt;At last , we don't&amp;nbsp; have the datasheet above you use, hope you can provide&amp;nbsp; a download address~&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;appreciate for your reply~&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Nov 2019 03:55:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Having-a-problem-initializing-the-MC33771/m-p/861402#M216</guid>
      <dc:creator>climbhuang</dc:creator>
      <dc:date>2019-11-25T03:55:33Z</dc:date>
    </item>
    <item>
      <title>Re: Having a problem initializing the MC33771</title>
      <link>https://community.nxp.com/t5/Power-Management/Having-a-problem-initializing-the-MC33771/m-p/861403#M217</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi sir,&lt;/P&gt;&lt;P&gt;I have one issue regarding in daisy chain connection of MC33771. How to read voltage reading from particular AFE (out of 2 AFE). How to differentiate between two AFE is there any criteria to enable AFE one after the other continuously.&lt;/P&gt;&lt;P&gt;In daisy chain connection if we remove battery of one AFE then next to that AFE will work or not.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Veeraju V Hallikeri&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jan 2020 07:56:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Having-a-problem-initializing-the-MC33771/m-p/861403#M217</guid>
      <dc:creator>veerajuvh619</dc:creator>
      <dc:date>2020-01-08T07:56:06Z</dc:date>
    </item>
  </channel>
</rss>