<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power Management中的主题 Re: PF1510 driver</title>
    <link>https://community.nxp.com/t5/Power-Management/PF1510-driver/m-p/861141#M213</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Norman,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;PF1550 and PF1510 are similar to each other with some specific features of difference:&lt;/P&gt;&lt;P&gt;PF1510 specific features: 1.5 A front-end LDO&lt;/P&gt;&lt;P&gt;PF1550 specific features: Linear 1 A Li+ Battery Charger&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The PF1510 is same as PF1550 except for the charger function, we removed the charging function for the PF1510.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you are not planning to use these specific features, then the PF1550 driver should be compatible for the PF1510.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;These PMICs share the same address and register map (except for the special features), so, PF1550 driver can be used for PF1510, just ignore charger related operations.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 01 Mar 2019 14:45:26 GMT</pubDate>
    <dc:creator>reyes</dc:creator>
    <dc:date>2019-03-01T14:45:26Z</dc:date>
    <item>
      <title>PF1510 driver</title>
      <link>https://community.nxp.com/t5/Power-Management/PF1510-driver/m-p/861140#M212</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is the pf1550 driver from the &lt;EM&gt;imx_4.9.88_2.0.0_ga&lt;/EM&gt;&amp;nbsp; kernel compatible with the pf1510?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also checked&amp;nbsp;&lt;EM&gt;imx_4.14.78_1.0.0_ga&lt;/EM&gt;, which doesn't have a driver for pf1510 either.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My processor is a IMX6ULL (MCIMX6Y2CVM08AB)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Norman&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Mar 2019 12:10:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PF1510-driver/m-p/861140#M212</guid>
      <dc:creator>norman_stetter</dc:creator>
      <dc:date>2019-03-01T12:10:05Z</dc:date>
    </item>
    <item>
      <title>Re: PF1510 driver</title>
      <link>https://community.nxp.com/t5/Power-Management/PF1510-driver/m-p/861141#M213</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Norman,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;PF1550 and PF1510 are similar to each other with some specific features of difference:&lt;/P&gt;&lt;P&gt;PF1510 specific features: 1.5 A front-end LDO&lt;/P&gt;&lt;P&gt;PF1550 specific features: Linear 1 A Li+ Battery Charger&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The PF1510 is same as PF1550 except for the charger function, we removed the charging function for the PF1510.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you are not planning to use these specific features, then the PF1550 driver should be compatible for the PF1510.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;These PMICs share the same address and register map (except for the special features), so, PF1550 driver can be used for PF1510, just ignore charger related operations.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Mar 2019 14:45:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PF1510-driver/m-p/861141#M213</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2019-03-01T14:45:26Z</dc:date>
    </item>
  </channel>
</rss>