<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックVR5510 test mode also at pre-programmed devices</title>
    <link>https://community.nxp.com/t5/Power-Management/VR5510-test-mode-also-at-pre-programmed-devices/m-p/1513176#M2122</link>
    <description>&lt;P&gt;The documentation of the VR5510 is not clear at this point:&lt;/P&gt;&lt;P&gt;Is it possible to continue entering test mode or debug mode with an already programmed device in order to continue testing of parameter sets like it is possible with an un-programmed (empty) device?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp; Klaus&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;PS: I know that I can program the device only once, but I want to know if I can continue to use an already programmed device for further optimizing the parameter set during development testing.&lt;/P&gt;</description>
    <pubDate>Mon, 29 Aug 2022 12:25:55 GMT</pubDate>
    <dc:creator>K_Steinhammer</dc:creator>
    <dc:date>2022-08-29T12:25:55Z</dc:date>
    <item>
      <title>VR5510 test mode also at pre-programmed devices</title>
      <link>https://community.nxp.com/t5/Power-Management/VR5510-test-mode-also-at-pre-programmed-devices/m-p/1513176#M2122</link>
      <description>&lt;P&gt;The documentation of the VR5510 is not clear at this point:&lt;/P&gt;&lt;P&gt;Is it possible to continue entering test mode or debug mode with an already programmed device in order to continue testing of parameter sets like it is possible with an un-programmed (empty) device?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp; Klaus&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;PS: I know that I can program the device only once, but I want to know if I can continue to use an already programmed device for further optimizing the parameter set during development testing.&lt;/P&gt;</description>
      <pubDate>Mon, 29 Aug 2022 12:25:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/VR5510-test-mode-also-at-pre-programmed-devices/m-p/1513176#M2122</guid>
      <dc:creator>K_Steinhammer</dc:creator>
      <dc:date>2022-08-29T12:25:55Z</dc:date>
    </item>
    <item>
      <title>Re: VR5510 test mode also at pre-programmed devices</title>
      <link>https://community.nxp.com/t5/Power-Management/VR5510-test-mode-also-at-pre-programmed-devices/m-p/1513391#M2123</link>
      <description>&lt;P&gt;Hello Klaus,&lt;/P&gt;
&lt;P&gt;I hope all is great with you.&lt;/P&gt;
&lt;P&gt;You are correct, you will be able to enter in Debug mode even with a programmed device. You may follow the procedure mentioned on &lt;A href="https://www.nxp.com/docs/en/data-sheet/VR5510.pdf" target="_blank"&gt;datasheet&lt;/A&gt;, &lt;STRONG&gt;chapter 8.12&lt;/STRONG&gt;.&lt;/P&gt;
&lt;P&gt;I hope this information helps.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;David&lt;/P&gt;</description>
      <pubDate>Mon, 29 Aug 2022 20:47:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/VR5510-test-mode-also-at-pre-programmed-devices/m-p/1513391#M2123</guid>
      <dc:creator>diazmarin09</dc:creator>
      <dc:date>2022-08-29T20:47:15Z</dc:date>
    </item>
  </channel>
</rss>