<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power Management中的主题 JN5189 Power down</title>
    <link>https://community.nxp.com/t5/Power-Management/JN5189-Power-down/m-p/1488144#M2079</link>
    <description>&lt;P&gt;Good afternoon,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have had a PCB board made with the JN5189 MCU on it. I have the board setup to read a sensor through an ADC channel. I have had another PCB board that attaches to the other board which as an op amp on for the sensor attached and aso the capability to run off a 3.7v rechargable battery. What i am struggling with is making the PCB board with the JN5189 on go to sleep so that i can save battery life. I want to be able to send my device to sleep at least 4 times throughout a 24Hr period. I have looked at the powerdown demo that comes with the SDK. I am running SDK 2.6.2.&lt;/P&gt;&lt;P&gt;Any help would be much apprieciated.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Matt&lt;/P&gt;</description>
    <pubDate>Tue, 12 Jul 2022 12:53:14 GMT</pubDate>
    <dc:creator>matthew3</dc:creator>
    <dc:date>2022-07-12T12:53:14Z</dc:date>
    <item>
      <title>JN5189 Power down</title>
      <link>https://community.nxp.com/t5/Power-Management/JN5189-Power-down/m-p/1488144#M2079</link>
      <description>&lt;P&gt;Good afternoon,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have had a PCB board made with the JN5189 MCU on it. I have the board setup to read a sensor through an ADC channel. I have had another PCB board that attaches to the other board which as an op amp on for the sensor attached and aso the capability to run off a 3.7v rechargable battery. What i am struggling with is making the PCB board with the JN5189 on go to sleep so that i can save battery life. I want to be able to send my device to sleep at least 4 times throughout a 24Hr period. I have looked at the powerdown demo that comes with the SDK. I am running SDK 2.6.2.&lt;/P&gt;&lt;P&gt;Any help would be much apprieciated.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Matt&lt;/P&gt;</description>
      <pubDate>Tue, 12 Jul 2022 12:53:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/JN5189-Power-down/m-p/1488144#M2079</guid>
      <dc:creator>matthew3</dc:creator>
      <dc:date>2022-07-12T12:53:14Z</dc:date>
    </item>
    <item>
      <title>Re: JN5189 Power down</title>
      <link>https://community.nxp.com/t5/Power-Management/JN5189-Power-down/m-p/1488355#M2080</link>
      <description>&lt;P&gt;Hi Matthew,&lt;/P&gt;
&lt;P lang="es-MX"&gt;Just to confirm, you are using a custom board, is this correct? If so, could you please confirm that you followed these guides for your hardware design?&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12898.pdf" target="_blank"&gt;JN5189-Power Consumption&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/user-guide/JN-RM-2078.pdf" target="_blank"&gt;JN5189 modules development reference manual&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Could you please help us providing more details about the problem you are facing?&lt;/P&gt;
&lt;P&gt;As you mentioned, you can take a look at the powerdown_demo project, inside the J5189 SDK, and use it as a base to develop your application. More information on power management can be found in the JN5189 User Manual (UM11138), Chapter 5: Power Management.&lt;/P&gt;
&lt;P&gt;Also, we recommend to update your SDK version. A newer version is available in the &lt;A href="https://mcuxpresso.nxp.com/en/select" target="_blank"&gt;MCUXpresso SDK Builder&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Tue, 12 Jul 2022 22:55:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/JN5189-Power-down/m-p/1488355#M2080</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2022-07-12T22:55:24Z</dc:date>
    </item>
  </channel>
</rss>