<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックSome problems with UJA1078</title>
    <link>https://community.nxp.com/t5/Power-Management/Some-problems-with-UJA1078/m-p/1486712#M2060</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Dear Support,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;UJA1078 High-speed CAN transceiver, inter-operable and downward compatible with CAN transceiver TJA1042, and compatible with the ISO 11898-2 and ISO 11898-5 standards.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1.&amp;nbsp;UJA1078 supports ISO 16845 standard?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2.Confirm contains filtering to detect valid remote wake up event?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;3.Confirm the CAN transceiver voltage reference pins are open circuit?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 08 Jul 2022 08:41:53 GMT</pubDate>
    <dc:creator>ZhaozhangChen</dc:creator>
    <dc:date>2022-07-08T08:41:53Z</dc:date>
    <item>
      <title>Some problems with UJA1078</title>
      <link>https://community.nxp.com/t5/Power-Management/Some-problems-with-UJA1078/m-p/1486712#M2060</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Dear Support,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;UJA1078 High-speed CAN transceiver, inter-operable and downward compatible with CAN transceiver TJA1042, and compatible with the ISO 11898-2 and ISO 11898-5 standards.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1.&amp;nbsp;UJA1078 supports ISO 16845 standard?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2.Confirm contains filtering to detect valid remote wake up event?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;3.Confirm the CAN transceiver voltage reference pins are open circuit?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 08 Jul 2022 08:41:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Some-problems-with-UJA1078/m-p/1486712#M2060</guid>
      <dc:creator>ZhaozhangChen</dc:creator>
      <dc:date>2022-07-08T08:41:53Z</dc:date>
    </item>
    <item>
      <title>Re: Some problems with UJA1078</title>
      <link>https://community.nxp.com/t5/Power-Management/Some-problems-with-UJA1078/m-p/1486798#M2061</link>
      <description>&lt;P data-unlink="true"&gt;Dear&amp;nbsp;&lt;SPAN data-proxy-id="aura-pos-lib-7"&gt;Zhaozhang,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P data-unlink="true"&gt;1. The integrated HS-CAN transceiver is ISO 11898-2 and 11898-5 compliant.&lt;/P&gt;
&lt;P data-unlink="true"&gt;2. There is a filter at the receiver input that prevents unwanted wake-up events occurring due to automotive transients or EMI.&lt;/P&gt;
&lt;P&gt;The wake-up sequence consists of a recessive, dominant, recessive, dominant signal on the CAN-bus within the specified time:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Fig. 9.JPG" style="width: 536px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/186080iEEC11453B25CF86C/image-size/large?v=v2&amp;amp;px=999" role="button" title="Fig. 9.JPG" alt="Fig. 9.JPG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Fig. 9.JPG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Wake-up frame (WUF) detection is not supported.&lt;/P&gt;
&lt;P&gt;3. I do not fully understand this question. Can you please rephrase it or provide more details?&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Tomas&lt;/P&gt;</description>
      <pubDate>Fri, 08 Jul 2022 11:00:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Some-problems-with-UJA1078/m-p/1486798#M2061</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2022-07-08T11:00:18Z</dc:date>
    </item>
    <item>
      <title>Re: Some problems with UJA1078</title>
      <link>https://community.nxp.com/t5/Power-Management/Some-problems-with-UJA1078/m-p/1487151#M2066</link>
      <description>&lt;P&gt;&lt;SPAN&gt;What is the tolerance of CAN transmission rate at 500 Kbps?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 11 Jul 2022 03:03:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Some-problems-with-UJA1078/m-p/1487151#M2066</guid>
      <dc:creator>ZhaozhangChen</dc:creator>
      <dc:date>2022-07-11T03:03:37Z</dc:date>
    </item>
  </channel>
</rss>