<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックRe: Regarding  USBPHYLDO of PF1510</title>
    <link>https://community.nxp.com/t5/Power-Management/Regarding-USBPHYLDO-of-PF1510/m-p/851636#M190</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tomohisa,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;[Answer 1]&lt;/P&gt;&lt;P&gt;This is a typo, USBPHYLDO = ‘0’ is for Disabled and &amp;nbsp;USBPHYLDO = ‘1’ should be for Enabled.&lt;/P&gt;&lt;P&gt;I reported this typo to the Apps team, I’ll be fixed for the next revision of the datasheet.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;[Answer 2]&lt;/P&gt;&lt;P&gt;Correct, USBPHY LDO regulator can be 0V if USBPHYLDO bit is disabled (‘0’).&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Feb 2019 21:38:20 GMT</pubDate>
    <dc:creator>reyes</dc:creator>
    <dc:date>2019-02-26T21:38:20Z</dc:date>
    <item>
      <title>Regarding  USBPHYLDO of PF1510</title>
      <link>https://community.nxp.com/t5/Power-Management/Regarding-USBPHYLDO-of-PF1510/m-p/851635#M189</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Support-team,&lt;/P&gt;&lt;P&gt;We have below questions about USBPHYLDO of PF1510.&lt;BR /&gt;Please support us.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;Question 1&amp;gt;&lt;BR /&gt;USBPHY (default 3.3 V output) seems to be described as being enable / disable with USBPHYLDO bit,&lt;BR /&gt;In the datasheet, USBPHYLDO = '0' for both Enable and Disable.&lt;BR /&gt;*The datasheet&amp;nbsp; of PF 1550 is also the same description.&lt;/P&gt;&lt;P&gt;Is Enable / Disable control possible? (Is it a typo)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;Question 2&amp;gt;&lt;BR /&gt;If it is set to Disable, will the USBPHY output become 0 V?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;&lt;A href="mailto:T.Sakamoto@Ryosan"&gt;T.Sakamoto@Ryosan&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Feb 2019 07:01:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Regarding-USBPHYLDO-of-PF1510/m-p/851635#M189</guid>
      <dc:creator>tomohisa_sakamo</dc:creator>
      <dc:date>2019-02-26T07:01:38Z</dc:date>
    </item>
    <item>
      <title>Re: Regarding  USBPHYLDO of PF1510</title>
      <link>https://community.nxp.com/t5/Power-Management/Regarding-USBPHYLDO-of-PF1510/m-p/851636#M190</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tomohisa,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;[Answer 1]&lt;/P&gt;&lt;P&gt;This is a typo, USBPHYLDO = ‘0’ is for Disabled and &amp;nbsp;USBPHYLDO = ‘1’ should be for Enabled.&lt;/P&gt;&lt;P&gt;I reported this typo to the Apps team, I’ll be fixed for the next revision of the datasheet.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;[Answer 2]&lt;/P&gt;&lt;P&gt;Correct, USBPHY LDO regulator can be 0V if USBPHYLDO bit is disabled (‘0’).&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Feb 2019 21:38:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Regarding-USBPHYLDO-of-PF1510/m-p/851636#M190</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2019-02-26T21:38:20Z</dc:date>
    </item>
    <item>
      <title>Re: Regarding  USBPHYLDO of PF1510</title>
      <link>https://community.nxp.com/t5/Power-Management/Regarding-USBPHYLDO-of-PF1510/m-p/851637#M191</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Jose-san,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;We understood your answers.&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;&lt;A href="mailto:T.Sakamoto@Ryosan"&gt;T.Sakamoto@Ryosan&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Feb 2019 00:04:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Regarding-USBPHYLDO-of-PF1510/m-p/851637#M191</guid>
      <dc:creator>tomohisa_sakamo</dc:creator>
      <dc:date>2019-02-27T00:04:51Z</dc:date>
    </item>
  </channel>
</rss>