<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックRe: PCA9420 - &amp;quot;ON&amp;quot; push without effect</title>
    <link>https://community.nxp.com/t5/Power-Management/PCA9420-quot-ON-quot-push-without-effect/m-p/1426908#M1826</link>
    <description>&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;I found the solution. In my application it was necessary to disable SW1 which is not used. SW1 voltage output was not at the good value so SYSRSTn was pulled-down by the PCA9420. He looks like if the SYSRSTn is low the ON input algorithm is not working.&lt;/P&gt;&lt;P&gt;What was strange is, the ON mechanism didn't work but my LDO2/SW2 was enable and at my expected values.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Fri, 11 Mar 2022 13:46:41 GMT</pubDate>
    <dc:creator>Gautier_Electronic</dc:creator>
    <dc:date>2022-03-11T13:46:41Z</dc:date>
    <item>
      <title>PCA9420 - "ON" push without effect</title>
      <link>https://community.nxp.com/t5/Power-Management/PCA9420-quot-ON-quot-push-without-effect/m-p/1426181#M1824</link>
      <description>&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;I would like to have fresh ideas about my current problem.&lt;/P&gt;&lt;P&gt;I use a PCA9420 on my design and I would like to use the feature which is doing an hard reset to the output rails when "ON" pin is turned '0' for a certain time.&lt;/P&gt;&lt;P&gt;I see that the "ON" is well turned '0', my PMIC is doing all goods output voltages but I can stay pressed for &amp;gt;16s no rails are going down. I have no idea about what could be bad in my design.&lt;/P&gt;&lt;P&gt;If anybody has an idea it will be well appreciated.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 10 Mar 2022 13:34:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PCA9420-quot-ON-quot-push-without-effect/m-p/1426181#M1824</guid>
      <dc:creator>Gautier_Electronic</dc:creator>
      <dc:date>2022-03-10T13:34:56Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9420 - "ON" push without effect</title>
      <link>https://community.nxp.com/t5/Power-Management/PCA9420-quot-ON-quot-push-without-effect/m-p/1426908#M1826</link>
      <description>&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;I found the solution. In my application it was necessary to disable SW1 which is not used. SW1 voltage output was not at the good value so SYSRSTn was pulled-down by the PCA9420. He looks like if the SYSRSTn is low the ON input algorithm is not working.&lt;/P&gt;&lt;P&gt;What was strange is, the ON mechanism didn't work but my LDO2/SW2 was enable and at my expected values.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Fri, 11 Mar 2022 13:46:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PCA9420-quot-ON-quot-push-without-effect/m-p/1426908#M1826</guid>
      <dc:creator>Gautier_Electronic</dc:creator>
      <dc:date>2022-03-11T13:46:41Z</dc:date>
    </item>
  </channel>
</rss>