<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックRe: Establishing SPI communication between Two MC33771 and Master Controller Unit.</title>
    <link>https://community.nxp.com/t5/Power-Management/Establishing-SPI-communication-between-Two-MC33771-and-Master/m-p/1408217#M1763</link>
    <description>&lt;P&gt;Hello Autoven,&lt;/P&gt;
&lt;P&gt;Have you considered using two parallel MC33771 devices with the same SPI bus but with different chip selects?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;David&lt;/P&gt;</description>
    <pubDate>Wed, 02 Feb 2022 18:00:37 GMT</pubDate>
    <dc:creator>diazmarin09</dc:creator>
    <dc:date>2022-02-02T18:00:37Z</dc:date>
    <item>
      <title>Establishing SPI communication between Two MC33771 and Master Controller Unit.</title>
      <link>https://community.nxp.com/t5/Power-Management/Establishing-SPI-communication-between-Two-MC33771-and-Master/m-p/1406872#M1756</link>
      <description>&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;I am using MC33771 for BMS development, for 16 cell battery.&lt;BR /&gt;MC33771 is 14 channel cell controller. Thus using two of them, eight channel from each MC33771 cell controller.&amp;nbsp;&lt;/P&gt;&lt;P&gt;These two MC33771 cell controller will be communicating through SPI with the Master Controller.&lt;BR /&gt;Master Controller has two SPI Modules say, SPI A and SPI B,&lt;/P&gt;&lt;P&gt;The question is, is it OK to connect the SPI A of MCU with MC33771 Cell Controller and SPI B of MCU with other MC33771 cell controller.&lt;BR /&gt;If it is connected will the battery get shorted in the MCU, because it will be having a common ground for both SPI lines.&lt;/P&gt;</description>
      <pubDate>Sun, 30 Jan 2022 06:39:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Establishing-SPI-communication-between-Two-MC33771-and-Master/m-p/1406872#M1756</guid>
      <dc:creator>Autoven</dc:creator>
      <dc:date>2022-01-30T06:39:13Z</dc:date>
    </item>
    <item>
      <title>Re: Establishing SPI communication between Two MC33771 and Master Controller Unit.</title>
      <link>https://community.nxp.com/t5/Power-Management/Establishing-SPI-communication-between-Two-MC33771-and-Master/m-p/1408217#M1763</link>
      <description>&lt;P&gt;Hello Autoven,&lt;/P&gt;
&lt;P&gt;Have you considered using two parallel MC33771 devices with the same SPI bus but with different chip selects?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;David&lt;/P&gt;</description>
      <pubDate>Wed, 02 Feb 2022 18:00:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Establishing-SPI-communication-between-Two-MC33771-and-Master/m-p/1408217#M1763</guid>
      <dc:creator>diazmarin09</dc:creator>
      <dc:date>2022-02-02T18:00:37Z</dc:date>
    </item>
  </channel>
</rss>