<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックVR5510 VCOREMON</title>
    <link>https://community.nxp.com/t5/Power-Management/VR5510-VCOREMON/m-p/1381000#M1705</link>
    <description>&lt;P&gt;I know that VCOREMON has to be connected directly to the core voltage supply of an S32G CPU. But there is no information how to connect this pin if a different CPU with a different core voltage level is used.&lt;/P&gt;&lt;P&gt;Does&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;the voltage monitor automatically adjust according to BUCK1 output voltage configuration so a direct connection between VCOREMON and BUCK1 output is mandatory&lt;/LI&gt;&lt;LI&gt;or do I have to insert an external voltage divider between VCOREMON and BUCK1 output?&lt;UL&gt;&lt;LI&gt;What would be the target voltage of this voltage divider (= nominal input voltage of the voltage monitor on VCOREMON pin)?&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;PS I need a static BUCK1 output voltage of 1.0V for my use case.&lt;/P&gt;</description>
    <pubDate>Fri, 03 Dec 2021 06:11:41 GMT</pubDate>
    <dc:creator>K_Steinhammer</dc:creator>
    <dc:date>2021-12-03T06:11:41Z</dc:date>
    <item>
      <title>VR5510 VCOREMON</title>
      <link>https://community.nxp.com/t5/Power-Management/VR5510-VCOREMON/m-p/1381000#M1705</link>
      <description>&lt;P&gt;I know that VCOREMON has to be connected directly to the core voltage supply of an S32G CPU. But there is no information how to connect this pin if a different CPU with a different core voltage level is used.&lt;/P&gt;&lt;P&gt;Does&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;the voltage monitor automatically adjust according to BUCK1 output voltage configuration so a direct connection between VCOREMON and BUCK1 output is mandatory&lt;/LI&gt;&lt;LI&gt;or do I have to insert an external voltage divider between VCOREMON and BUCK1 output?&lt;UL&gt;&lt;LI&gt;What would be the target voltage of this voltage divider (= nominal input voltage of the voltage monitor on VCOREMON pin)?&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;PS I need a static BUCK1 output voltage of 1.0V for my use case.&lt;/P&gt;</description>
      <pubDate>Fri, 03 Dec 2021 06:11:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/VR5510-VCOREMON/m-p/1381000#M1705</guid>
      <dc:creator>K_Steinhammer</dc:creator>
      <dc:date>2021-12-03T06:11:41Z</dc:date>
    </item>
    <item>
      <title>Re: VR5510 VCOREMON</title>
      <link>https://community.nxp.com/t5/Power-Management/VR5510-VCOREMON/m-p/1381117#M1706</link>
      <description>&lt;P&gt;Dear Klaus,&lt;/P&gt;
&lt;P&gt;the VCOREMON automatically sets to the BUCK1 or BUCK1/2 in dual phase output voltage. You just need to set the BUCK1 output voltage. The VCOREMON overvoltage and undervoltage thresholds are listed in Table 57. in the VR5510 datasheet.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_0-1638519984824.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/164012iAC3D628E338D7ECC/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_0-1638519984824.png" alt="JozefKozon_0-1638519984824.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;The output voltage is configurable by OTP through the BUCK1V_OTP [7:0] bit field (CFG_ BUCK1_1_OTPregister) or the BUCK2V_OTP [7:0] bit field (CFG_ BUCK2_ 1_OTP register) from 0.4 V&lt;BR /&gt;to 1.8 V.&lt;/P&gt;
&lt;P&gt;Please refer to section 23.6.2 in the VR5510 datasheet for the BUCK1/2 output voltage transition.&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Fri, 03 Dec 2021 08:30:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/VR5510-VCOREMON/m-p/1381117#M1706</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2021-12-03T08:30:41Z</dc:date>
    </item>
  </channel>
</rss>