<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックBAT54 - Inrush current capability</title>
    <link>https://community.nxp.com/t5/Power-Management/BAT54-Inrush-current-capability/m-p/1372791#M1690</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm designing an isolated DC/DC converter with a simple push-pull configuration and a central-tapped transformer. On the secondary side, there are two diodes and a 1uF capacitor to rectify the output. The operating frequency is 500kHz.&lt;/P&gt;&lt;P&gt;The nominal output current is around 100mA (abs max 150mA).&lt;/P&gt;&lt;P&gt;I'm planning to use BAT54 diodes, but I have a concern about their peak current capability, related to the inrush current of the circuit (charging the output capacitor at the startup). I'm assuming an ambient temperature &amp;lt; 60°C.&lt;/P&gt;&lt;P&gt;The NXP datasheet shows If=200mA at&amp;nbsp;25°C, and Ifsm=600mA at 25°C, square wave, tp&amp;lt;10ms; I guess this is related to the usage of the diode in a standard 50Hz / 60Hz rectifier. I would like to know if BAT54 can handle an higher forward current for a shorter time.&amp;nbsp;&lt;SPAN&gt;In my circuit, the peak current duration is &amp;lt; 10µs and the maximum value is 1.8A. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is there some documentation about "pulse power rating" of BAT54? I would like to understand if it can be used in my application.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Many thanks,&lt;/P&gt;&lt;P&gt;Alessio&lt;/P&gt;</description>
    <pubDate>Wed, 17 Nov 2021 13:27:03 GMT</pubDate>
    <dc:creator>AlessioCaligiuri</dc:creator>
    <dc:date>2021-11-17T13:27:03Z</dc:date>
    <item>
      <title>BAT54 - Inrush current capability</title>
      <link>https://community.nxp.com/t5/Power-Management/BAT54-Inrush-current-capability/m-p/1372791#M1690</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm designing an isolated DC/DC converter with a simple push-pull configuration and a central-tapped transformer. On the secondary side, there are two diodes and a 1uF capacitor to rectify the output. The operating frequency is 500kHz.&lt;/P&gt;&lt;P&gt;The nominal output current is around 100mA (abs max 150mA).&lt;/P&gt;&lt;P&gt;I'm planning to use BAT54 diodes, but I have a concern about their peak current capability, related to the inrush current of the circuit (charging the output capacitor at the startup). I'm assuming an ambient temperature &amp;lt; 60°C.&lt;/P&gt;&lt;P&gt;The NXP datasheet shows If=200mA at&amp;nbsp;25°C, and Ifsm=600mA at 25°C, square wave, tp&amp;lt;10ms; I guess this is related to the usage of the diode in a standard 50Hz / 60Hz rectifier. I would like to know if BAT54 can handle an higher forward current for a shorter time.&amp;nbsp;&lt;SPAN&gt;In my circuit, the peak current duration is &amp;lt; 10µs and the maximum value is 1.8A. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is there some documentation about "pulse power rating" of BAT54? I would like to understand if it can be used in my application.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Many thanks,&lt;/P&gt;&lt;P&gt;Alessio&lt;/P&gt;</description>
      <pubDate>Wed, 17 Nov 2021 13:27:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/BAT54-Inrush-current-capability/m-p/1372791#M1690</guid>
      <dc:creator>AlessioCaligiuri</dc:creator>
      <dc:date>2021-11-17T13:27:03Z</dc:date>
    </item>
    <item>
      <title>Re: BAT54 - Inrush current capability</title>
      <link>https://community.nxp.com/t5/Power-Management/BAT54-Inrush-current-capability/m-p/1373904#M1691</link>
      <description>&lt;P&gt;&lt;SPAN&gt;BAT54 had Transferred to&amp;nbsp;&lt;A href="http://www.nexperia.com/catcher/BAT54" target="_blank" rel="noopener"&gt;Nexperia&lt;/A&gt;&amp;nbsp;on 06-Feb-2017,please contact with them for your issue.&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 19 Nov 2021 00:22:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/BAT54-Inrush-current-capability/m-p/1373904#M1691</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2021-11-19T00:22:59Z</dc:date>
    </item>
    <item>
      <title>Re: BAT54 - Inrush current capability</title>
      <link>https://community.nxp.com/t5/Power-Management/BAT54-Inrush-current-capability/m-p/1374265#M1692</link>
      <description>&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Alessio&lt;/P&gt;</description>
      <pubDate>Fri, 19 Nov 2021 10:14:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/BAT54-Inrush-current-capability/m-p/1374265#M1692</guid>
      <dc:creator>AlessioCaligiuri</dc:creator>
      <dc:date>2021-11-19T10:14:12Z</dc:date>
    </item>
  </channel>
</rss>