<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックRe: 35FS6500 Reset Reason</title>
    <link>https://community.nxp.com/t5/Power-Management/35FS6500-Reset-Reason/m-p/841589#M169</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dennis,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using 33FS6513. Currently, checking in debug mode. So, can this be concluded that on POR, this bit(RSTB_EXT) won't be set?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The main problem that am facing is BAT_FAIL bit of INIT_VREG register is always 0. So MSM doesn't get initialized according to the SBC Init flowchart.&lt;/P&gt;&lt;P&gt;While debugging, I thought, can it be due to this RSTB_EXT bit setting?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 26 Apr 2019 05:26:34 GMT</pubDate>
    <dc:creator>vaibhav_sharma</dc:creator>
    <dc:date>2019-04-26T05:26:34Z</dc:date>
    <item>
      <title>35FS6500 Reset Reason</title>
      <link>https://community.nxp.com/t5/Power-Management/35FS6500-Reset-Reason/m-p/841587#M167</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I saw on product's datasheet that there are a lot of reasons which could cause an SBC reset via RSTB route. That's fine, but I need to know, most generically, if the reset was due to RSTB or POR. How could I do that?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Oct 2018 10:57:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/35FS6500-Reset-Reason/m-p/841587#M167</guid>
      <dc:creator>daniele_spinell</dc:creator>
      <dc:date>2018-10-10T10:57:30Z</dc:date>
    </item>
    <item>
      <title>Re: 35FS6500 Reset Reason</title>
      <link>https://community.nxp.com/t5/Power-Management/35FS6500-Reset-Reason/m-p/841588#M168</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Daniele&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If reset is caused by POR, it is normal power up sequence, MCU will run initialization for SBC.&lt;/P&gt;&lt;P&gt;If reset is caused by&amp;nbsp; low pulse&amp;nbsp;of external RSTB pin, because MCU reset pin is connected to RSTB, so both MCU and SBC would reset.&amp;nbsp; &amp;nbsp;Pls. check below register for external reset of SBC.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/66883i271D665F2ADE4372/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Br&lt;/P&gt;&lt;P&gt;Dennis Zeng&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Nov 2018 04:27:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/35FS6500-Reset-Reason/m-p/841588#M168</guid>
      <dc:creator>DennisZeng</dc:creator>
      <dc:date>2018-11-01T04:27:48Z</dc:date>
    </item>
    <item>
      <title>Re: 35FS6500 Reset Reason</title>
      <link>https://community.nxp.com/t5/Power-Management/35FS6500-Reset-Reason/m-p/841589#M169</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dennis,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using 33FS6513. Currently, checking in debug mode. So, can this be concluded that on POR, this bit(RSTB_EXT) won't be set?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The main problem that am facing is BAT_FAIL bit of INIT_VREG register is always 0. So MSM doesn't get initialized according to the SBC Init flowchart.&lt;/P&gt;&lt;P&gt;While debugging, I thought, can it be due to this RSTB_EXT bit setting?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Apr 2019 05:26:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/35FS6500-Reset-Reason/m-p/841589#M169</guid>
      <dc:creator>vaibhav_sharma</dc:creator>
      <dc:date>2019-04-26T05:26:34Z</dc:date>
    </item>
    <item>
      <title>Re: 35FS6500 Reset Reason</title>
      <link>https://community.nxp.com/t5/Power-Management/35FS6500-Reset-Reason/m-p/841590#M170</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Vaibhav&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;RSTB_EXT bit should not be set after PoR.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Pls. make&amp;nbsp; sure Vsup is 0V&amp;nbsp; before you apply power supply on FS65. Sometimes the residual charge on capacitor of Vsup may maintain register vaules&amp;nbsp; and BAT_FAIL is 0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Br&lt;/P&gt;&lt;P&gt;Dennis&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Apr 2019 07:41:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/35FS6500-Reset-Reason/m-p/841590#M170</guid>
      <dc:creator>DennisZeng</dc:creator>
      <dc:date>2019-04-26T07:41:51Z</dc:date>
    </item>
  </channel>
</rss>