<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FS6523 CAN Transceiver in LISTEN Mode in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/FS6523-CAN-Transceiver-in-LISTEN-Mode/m-p/1338989#M1593</link>
    <description>&lt;P&gt;Hi All&lt;/P&gt;&lt;P&gt;I am using FS6523C as power chip and set the CAN mode as NORMAL Mode during initialization. When am set CAN mode as Normal mode am able to Rx and TX data successfully on Canalyzer. But when am set the CAN mode as LISTEN mode, Tx is off but am unable to Rx any signal also. Is this correct ?&lt;/P&gt;&lt;P&gt;Or any other configuration is required for CAN LISTEN mode.?&lt;/P&gt;&lt;P&gt;what is the expected behavior when we set CAN Mode as LISTEN mode ?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 13 Sep 2021 08:30:46 GMT</pubDate>
    <dc:creator>Shailendrag</dc:creator>
    <dc:date>2021-09-13T08:30:46Z</dc:date>
    <item>
      <title>FS6523 CAN Transceiver in LISTEN Mode</title>
      <link>https://community.nxp.com/t5/Power-Management/FS6523-CAN-Transceiver-in-LISTEN-Mode/m-p/1338989#M1593</link>
      <description>&lt;P&gt;Hi All&lt;/P&gt;&lt;P&gt;I am using FS6523C as power chip and set the CAN mode as NORMAL Mode during initialization. When am set CAN mode as Normal mode am able to Rx and TX data successfully on Canalyzer. But when am set the CAN mode as LISTEN mode, Tx is off but am unable to Rx any signal also. Is this correct ?&lt;/P&gt;&lt;P&gt;Or any other configuration is required for CAN LISTEN mode.?&lt;/P&gt;&lt;P&gt;what is the expected behavior when we set CAN Mode as LISTEN mode ?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 13 Sep 2021 08:30:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS6523-CAN-Transceiver-in-LISTEN-Mode/m-p/1338989#M1593</guid>
      <dc:creator>Shailendrag</dc:creator>
      <dc:date>2021-09-13T08:30:46Z</dc:date>
    </item>
    <item>
      <title>Re: FS6523 CAN Transceiver in LISTEN Mode</title>
      <link>https://community.nxp.com/t5/Power-Management/FS6523-CAN-Transceiver-in-LISTEN-Mode/m-p/1339381#M1594</link>
      <description>&lt;P&gt;When the CAN mode bit configuration is ’01’ (CAN in listen only), the device is only&lt;BR /&gt;able to report the bus level to the RXD pin. The TXD driver is off and the device is not&lt;BR /&gt;able to transmit information from TXD to the bus. TXD is maintained high by an internal&lt;BR /&gt;pull-up resistor TXDPULL-UP connected to VDDIO&lt;/P&gt;</description>
      <pubDate>Tue, 14 Sep 2021 02:17:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS6523-CAN-Transceiver-in-LISTEN-Mode/m-p/1339381#M1594</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2021-09-14T02:17:40Z</dc:date>
    </item>
    <item>
      <title>Re: FS6523 CAN Transceiver in LISTEN Mode</title>
      <link>https://community.nxp.com/t5/Power-Management/FS6523-CAN-Transceiver-in-LISTEN-Mode/m-p/1339722#M1595</link>
      <description>&lt;P&gt;Means when we set the CAN to LISTEN Mode then we should only able to receive the RXD signal. Is this understanding correct ?&lt;/P&gt;</description>
      <pubDate>Tue, 14 Sep 2021 09:41:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS6523-CAN-Transceiver-in-LISTEN-Mode/m-p/1339722#M1595</guid>
      <dc:creator>Shailendrag</dc:creator>
      <dc:date>2021-09-14T09:41:54Z</dc:date>
    </item>
  </channel>
</rss>