<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックFS6510 Reading BIST Result needs a delay</title>
    <link>https://community.nxp.com/t5/Power-Management/FS6510-Reading-BIST-Result-needs-a-delay/m-p/1311197#M1555</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I read the BIST Register after power-on reset, the result is 0x0, it means all the 4 bits of BIST reault are NOTOK. But after a 8ms delay, I read this register again, it returns 0xD, it means ABIST2_VAUX is NOTOK, and other bits such as LBIST, ABIST1, ABIST2_FS1B are Normal. Why does it need a delay, what's the possible reason about it?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="BIST延时.png" style="width: 984px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/150465i9847D19C20B1D5D0/image-size/large?v=v2&amp;amp;px=999" role="button" title="BIST延时.png" alt="BIST延时.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Jamber&lt;/P&gt;</description>
    <pubDate>Wed, 21 Jul 2021 09:33:42 GMT</pubDate>
    <dc:creator>Jamber_H</dc:creator>
    <dc:date>2021-07-21T09:33:42Z</dc:date>
    <item>
      <title>FS6510 Reading BIST Result needs a delay</title>
      <link>https://community.nxp.com/t5/Power-Management/FS6510-Reading-BIST-Result-needs-a-delay/m-p/1311197#M1555</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I read the BIST Register after power-on reset, the result is 0x0, it means all the 4 bits of BIST reault are NOTOK. But after a 8ms delay, I read this register again, it returns 0xD, it means ABIST2_VAUX is NOTOK, and other bits such as LBIST, ABIST1, ABIST2_FS1B are Normal. Why does it need a delay, what's the possible reason about it?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="BIST延时.png" style="width: 984px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/150465i9847D19C20B1D5D0/image-size/large?v=v2&amp;amp;px=999" role="button" title="BIST延时.png" alt="BIST延时.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Jamber&lt;/P&gt;</description>
      <pubDate>Wed, 21 Jul 2021 09:33:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS6510-Reading-BIST-Result-needs-a-delay/m-p/1311197#M1555</guid>
      <dc:creator>Jamber_H</dc:creator>
      <dc:date>2021-07-21T09:33:42Z</dc:date>
    </item>
    <item>
      <title>Re: FS6510 Reading BIST Result needs a delay</title>
      <link>https://community.nxp.com/t5/Power-Management/FS6510-Reading-BIST-Result-needs-a-delay/m-p/1311305#M1557</link>
      <description>&lt;P&gt;Hi Jamber,&lt;/P&gt;
&lt;P&gt;the 8ms is actually quite short delay time. According to the datasheet, the&amp;nbsp;Reset delay time after a power on reset is typically 16.5ms, minimally 12.5ms. Please refer to the Table 6. in the datasheet attached.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_0-1626871580793.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/150479i72A839BEC18C08C5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_0-1626871580793.png" alt="JozefKozon_0-1626871580793.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Wed, 21 Jul 2021 12:48:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/FS6510-Reading-BIST-Result-needs-a-delay/m-p/1311305#M1557</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2021-07-21T12:48:37Z</dc:date>
    </item>
  </channel>
</rss>