<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power Management中的主题 PF3001 with IMX6 solo</title>
    <link>https://community.nxp.com/t5/Power-Management/PF3001-with-IMX6-solo/m-p/1301320#M1534</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am having some issue with a PF3001 powering an IMX6 solo. This problem is very rare but I would like to find the cause and fix it. Basically, sometime, the unit is not booting properly. I have read quite a bit of community question about the same problem but I haven't find a way to fix the issue I have.&amp;nbsp;&lt;/P&gt;&lt;P&gt;It seem that the RTC_CLK on the IMX6 is not up fast enough sometime and this cause the unit not to boot. I looked at the POR_B on the PF3001 (or RESETBMCU) and it does go up a bit too fast. I looked into the data sheet to see if we could assert that pin directly but it doesn't seem so. I also try to use a delay with a RC on the PWRON but it was not enough (1M + 0.1µF on PWRON using VSNVS).&amp;nbsp;&lt;/P&gt;&lt;P&gt;If someone could give a hint on where to look or how to delay the supplies, I would appreciate.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Fred&lt;/P&gt;</description>
    <pubDate>Thu, 01 Jul 2021 16:38:22 GMT</pubDate>
    <dc:creator>Fred_Jutras</dc:creator>
    <dc:date>2021-07-01T16:38:22Z</dc:date>
    <item>
      <title>PF3001 with IMX6 solo</title>
      <link>https://community.nxp.com/t5/Power-Management/PF3001-with-IMX6-solo/m-p/1301320#M1534</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am having some issue with a PF3001 powering an IMX6 solo. This problem is very rare but I would like to find the cause and fix it. Basically, sometime, the unit is not booting properly. I have read quite a bit of community question about the same problem but I haven't find a way to fix the issue I have.&amp;nbsp;&lt;/P&gt;&lt;P&gt;It seem that the RTC_CLK on the IMX6 is not up fast enough sometime and this cause the unit not to boot. I looked at the POR_B on the PF3001 (or RESETBMCU) and it does go up a bit too fast. I looked into the data sheet to see if we could assert that pin directly but it doesn't seem so. I also try to use a delay with a RC on the PWRON but it was not enough (1M + 0.1µF on PWRON using VSNVS).&amp;nbsp;&lt;/P&gt;&lt;P&gt;If someone could give a hint on where to look or how to delay the supplies, I would appreciate.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Fred&lt;/P&gt;</description>
      <pubDate>Thu, 01 Jul 2021 16:38:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PF3001-with-IMX6-solo/m-p/1301320#M1534</guid>
      <dc:creator>Fred_Jutras</dc:creator>
      <dc:date>2021-07-01T16:38:22Z</dc:date>
    </item>
    <item>
      <title>Re: PF3001 with IMX6 solo</title>
      <link>https://community.nxp.com/t5/Power-Management/PF3001-with-IMX6-solo/m-p/1302228#M1536</link>
      <description>&lt;P&gt;What's your desired rise up time of PRO_B pin?&lt;/P&gt;</description>
      <pubDate>Mon, 05 Jul 2021 05:56:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PF3001-with-IMX6-solo/m-p/1302228#M1536</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2021-07-05T05:56:45Z</dc:date>
    </item>
    <item>
      <title>Re: PF3001 with IMX6 solo</title>
      <link>https://community.nxp.com/t5/Power-Management/PF3001-with-IMX6-solo/m-p/1303162#M1539</link>
      <description>&lt;P&gt;Hi Guoweisun,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I don't particulary need a set time, at the moment, it seem that the unit goes up as soon as possible which from the time the 5V is up until the POR_B de-assert, is approximatively 16 msec. From the errata ERR009678:&amp;nbsp;&lt;/P&gt;&lt;P&gt;"3. Delay POR_B de-assertion until after the 32 kHz crystal is stable (approximately 300 ms to 500&lt;BR /&gt;ms from VDD_SNVS_IN ramp timing; this timing is dependent on the crystal start up timing&lt;BR /&gt;characteristics)."&lt;/P&gt;&lt;P&gt;I don't think I would need that long of a delay but anything might help. Maybe I would need to search for a different crystal too.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Fred&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jul 2021 12:52:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PF3001-with-IMX6-solo/m-p/1303162#M1539</guid>
      <dc:creator>Fred_Jutras</dc:creator>
      <dc:date>2021-07-06T12:52:45Z</dc:date>
    </item>
  </channel>
</rss>