<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SBC FS65 SPI COMMUNICATION ISSUE in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/SBC-FS65-SPI-COMMUNICATION-ISSUE/m-p/1291768#M1507</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Am trying to create a SPI Communication between SBC Evolution Board KITFS6523CAEEVM and AURIX Controller TC387. In loopback it's working fine. But when trying with SBC board am facing issue. Am trying to read SPI register using read command (0x1400). As per sheet am expecting response as 0x0FD2. But when am sending 10 read command am getting around two times correct response (Not always) and rest are incorrect. Response are fluctuating. Tried by reading other register also but facing same issue, response are not constant&lt;/P&gt;&lt;P&gt;Pls help me on this&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Shailendra&lt;/P&gt;</description>
    <pubDate>Mon, 14 Jun 2021 07:42:58 GMT</pubDate>
    <dc:creator>Shailendrag</dc:creator>
    <dc:date>2021-06-14T07:42:58Z</dc:date>
    <item>
      <title>SBC FS65 SPI COMMUNICATION ISSUE</title>
      <link>https://community.nxp.com/t5/Power-Management/SBC-FS65-SPI-COMMUNICATION-ISSUE/m-p/1291768#M1507</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Am trying to create a SPI Communication between SBC Evolution Board KITFS6523CAEEVM and AURIX Controller TC387. In loopback it's working fine. But when trying with SBC board am facing issue. Am trying to read SPI register using read command (0x1400). As per sheet am expecting response as 0x0FD2. But when am sending 10 read command am getting around two times correct response (Not always) and rest are incorrect. Response are fluctuating. Tried by reading other register also but facing same issue, response are not constant&lt;/P&gt;&lt;P&gt;Pls help me on this&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Shailendra&lt;/P&gt;</description>
      <pubDate>Mon, 14 Jun 2021 07:42:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/SBC-FS65-SPI-COMMUNICATION-ISSUE/m-p/1291768#M1507</guid>
      <dc:creator>Shailendrag</dc:creator>
      <dc:date>2021-06-14T07:42:58Z</dc:date>
    </item>
    <item>
      <title>Re: SBC FS65 SPI COMMUNICATION ISSUE</title>
      <link>https://community.nxp.com/t5/Power-Management/SBC-FS65-SPI-COMMUNICATION-ISSUE/m-p/1291808#M1508</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Shailendra,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Do you have a logic analyzer or an oscilloscope to see what is going on the bus and double check the proper format/timing?&lt;/P&gt;
&lt;P&gt;Note that the FS65 uses the ‘Mode 1′ SPI protocol, which means that the base value of the SCLK signal is zero (CPOL = 0), data are sampled on a falling edge and changed on a rising edge (CPHA = 1).&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="SPI.JPG" style="width: 716px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/146997iE66BB973CC4B4EE9/image-size/large?v=v2&amp;amp;px=999" role="button" title="SPI.JPG" alt="SPI.JPG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;SPI.JPG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Tomas&lt;/P&gt;</description>
      <pubDate>Mon, 14 Jun 2021 08:46:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/SBC-FS65-SPI-COMMUNICATION-ISSUE/m-p/1291808#M1508</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2021-06-14T08:46:56Z</dc:date>
    </item>
  </channel>
</rss>