<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PCA9420 Power Up and Operation in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/PCA9420-Power-Up-and-Operation/m-p/1281353#M1484</link>
    <description>&lt;P&gt;Both conditions must be met?&amp;nbsp; VIN must be supplied?&amp;nbsp; This seems odd for battery powered devices.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In testing we are able to power up with just VBAT and no voltage on VIN.&amp;nbsp; ASYS will be powered by VBAT.&lt;/P&gt;&lt;P&gt;What is the valid voltage on VIN need for if a battery (VBAT) is attached?&lt;/P&gt;</description>
    <pubDate>Mon, 24 May 2021 23:09:48 GMT</pubDate>
    <dc:creator>Kevin23</dc:creator>
    <dc:date>2021-05-24T23:09:48Z</dc:date>
    <item>
      <title>PCA9420 Power Up and Operation</title>
      <link>https://community.nxp.com/t5/Power-Management/PCA9420-Power-Up-and-Operation/m-p/1279745#M1480</link>
      <description>&lt;P&gt;I am using the PCA9420 PMIC with the RT685.&amp;nbsp; I need to be able to power up with only VBAT connected (no external voltage on VIN).&amp;nbsp; It appears a voltage on VIN is required for power up.&amp;nbsp; I am not using VIN directly because our input voltage was falling too close or hitting to the 3.1V UVLO on VIN and not powering up.&amp;nbsp; Is it acceptable to use the VBAT voltage with a diode connected to VIN for power up?&lt;/P&gt;&lt;P&gt;I will be inputting 3.3V on VBAT.&amp;nbsp; This will result with VIN being 3.0-3.1V with the diode drop.&amp;nbsp; In testing this appears to work as all regulator enable to the proper voltage and the SYSRST is released.&amp;nbsp; I know the VIN is close to the UVLO but does not seem to disable the regulator outputs if it falls below the default 3.1V VIN_UVLO.&amp;nbsp; The ASYS voltage should be valid and use the VBAT input as it is higher than VIN.&amp;nbsp; I plan on leaving the PMIC powered in the configuration (VIN powered by VBAT with diode).&lt;/P&gt;&lt;P&gt;Is this a valid power up and operational design?&lt;/P&gt;</description>
      <pubDate>Thu, 20 May 2021 12:35:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PCA9420-Power-Up-and-Operation/m-p/1279745#M1480</guid>
      <dc:creator>Kevin23</dc:creator>
      <dc:date>2021-05-20T12:35:26Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9420 Power Up and Operation</title>
      <link>https://community.nxp.com/t5/Power-Management/PCA9420-Power-Up-and-Operation/m-p/1280150#M1481</link>
      <description>&lt;P&gt;which kind type of battery do you use in your case?&lt;/P&gt;
&lt;P&gt;what's the voltage range of your battery?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 21 May 2021 06:44:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PCA9420-Power-Up-and-Operation/m-p/1280150#M1481</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2021-05-21T06:44:00Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9420 Power Up and Operation</title>
      <link>https://community.nxp.com/t5/Power-Management/PCA9420-Power-Up-and-Operation/m-p/1280391#M1482</link>
      <description>&lt;P&gt;Our VBAT input will be 3.0-3.6V.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We had some confusion on the power up in section 8.10.3 of the datasheet. In condition 1, we though a valid voltage on VIN was required for power up.&amp;nbsp; We think inputting a voltage on VBAT, with VIN floating, will satisfy "A voltage on ASYS higher than ASYS_UVLO, a 2.8V typical" and should start the power up sequence.&amp;nbsp; Is this correct?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 21 May 2021 12:27:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PCA9420-Power-Up-and-Operation/m-p/1280391#M1482</guid>
      <dc:creator>Kevin23</dc:creator>
      <dc:date>2021-05-21T12:27:54Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9420 Power Up and Operation</title>
      <link>https://community.nxp.com/t5/Power-Management/PCA9420-Power-Up-and-Operation/m-p/1280847#M1483</link>
      <description>&lt;P&gt;• A valid VIN supply on VIN pin&lt;BR /&gt;• A voltage on ASYS higher than ASYS_UVLO, a 2.8V typical&lt;/P&gt;
&lt;P&gt;Please meet above these two conditions.&lt;/P&gt;</description>
      <pubDate>Mon, 24 May 2021 05:25:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PCA9420-Power-Up-and-Operation/m-p/1280847#M1483</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2021-05-24T05:25:48Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9420 Power Up and Operation</title>
      <link>https://community.nxp.com/t5/Power-Management/PCA9420-Power-Up-and-Operation/m-p/1281353#M1484</link>
      <description>&lt;P&gt;Both conditions must be met?&amp;nbsp; VIN must be supplied?&amp;nbsp; This seems odd for battery powered devices.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In testing we are able to power up with just VBAT and no voltage on VIN.&amp;nbsp; ASYS will be powered by VBAT.&lt;/P&gt;&lt;P&gt;What is the valid voltage on VIN need for if a battery (VBAT) is attached?&lt;/P&gt;</description>
      <pubDate>Mon, 24 May 2021 23:09:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PCA9420-Power-Up-and-Operation/m-p/1281353#M1484</guid>
      <dc:creator>Kevin23</dc:creator>
      <dc:date>2021-05-24T23:09:48Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9420 Power Up and Operation</title>
      <link>https://community.nxp.com/t5/Power-Management/PCA9420-Power-Up-and-Operation/m-p/1880293#M3545</link>
      <description>&lt;P&gt;Hi,Kevin!&lt;/P&gt;&lt;P&gt;I‘ve&amp;nbsp;tested powering only the VBAT pin without powering the VIN. A battery(400mAh, 3.7-4.2V) was connected to VBAT.The PCA9420 worked properly in my case.This may be helpful to you.&lt;/P&gt;</description>
      <pubDate>Tue, 04 Jun 2024 04:47:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PCA9420-Power-Up-and-Operation/m-p/1880293#M3545</guid>
      <dc:creator>GeoZh</dc:creator>
      <dc:date>2024-06-04T04:47:20Z</dc:date>
    </item>
  </channel>
</rss>