<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Configure FS8530 using NXP Flex GUI and I2C interface in Power Management</title>
    <link>https://community.nxp.com/t5/Power-Management/Configure-FS8530-using-NXP-Flex-GUI-and-I2C-interface/m-p/1263020#M1440</link>
    <description>&lt;P&gt;We&amp;nbsp; have been working on configuring the KITFS85SKTEVM(With&amp;nbsp; PC33FS8430C0ES) using NXP flexGUI and I2C interface. On Configuring the PMIC in Test-mode we have error response "Error: Command Execution failed".&lt;BR /&gt;&lt;BR /&gt;Step followed:&lt;BR /&gt;1. Generate the PMIC config file&amp;nbsp; using spreadsheet&lt;BR /&gt;2. Connect the EVAL board to the system loaded with NXP Flex GUI&lt;BR /&gt;3. Launch the GUI and select&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; i) Interface as debug-i2c&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ii) MCU type as KL25Z (Embedded)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; iii) USB as usb-cdc&lt;BR /&gt;4. Search for the available ports and Select the correct port for EVAL board&lt;BR /&gt;5. Press start button (GUI read back some register values)&lt;BR /&gt;6. Load the file generated on step1&lt;BR /&gt;7. Press start option&lt;BR /&gt;8. On the results column it says "Error: Command Exectuion Failed"&lt;BR /&gt;9. Tried with different I2C speed and the result is same.&lt;BR /&gt;&lt;BR /&gt;But the setup works well with SPI interface.&lt;BR /&gt;Did I miss any sequence here for I2C??&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 15 Apr 2021 18:02:13 GMT</pubDate>
    <dc:creator>satheesh_mb</dc:creator>
    <dc:date>2021-04-15T18:02:13Z</dc:date>
    <item>
      <title>Configure FS8530 using NXP Flex GUI and I2C interface</title>
      <link>https://community.nxp.com/t5/Power-Management/Configure-FS8530-using-NXP-Flex-GUI-and-I2C-interface/m-p/1263020#M1440</link>
      <description>&lt;P&gt;We&amp;nbsp; have been working on configuring the KITFS85SKTEVM(With&amp;nbsp; PC33FS8430C0ES) using NXP flexGUI and I2C interface. On Configuring the PMIC in Test-mode we have error response "Error: Command Execution failed".&lt;BR /&gt;&lt;BR /&gt;Step followed:&lt;BR /&gt;1. Generate the PMIC config file&amp;nbsp; using spreadsheet&lt;BR /&gt;2. Connect the EVAL board to the system loaded with NXP Flex GUI&lt;BR /&gt;3. Launch the GUI and select&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; i) Interface as debug-i2c&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ii) MCU type as KL25Z (Embedded)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; iii) USB as usb-cdc&lt;BR /&gt;4. Search for the available ports and Select the correct port for EVAL board&lt;BR /&gt;5. Press start button (GUI read back some register values)&lt;BR /&gt;6. Load the file generated on step1&lt;BR /&gt;7. Press start option&lt;BR /&gt;8. On the results column it says "Error: Command Exectuion Failed"&lt;BR /&gt;9. Tried with different I2C speed and the result is same.&lt;BR /&gt;&lt;BR /&gt;But the setup works well with SPI interface.&lt;BR /&gt;Did I miss any sequence here for I2C??&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 15 Apr 2021 18:02:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Configure-FS8530-using-NXP-Flex-GUI-and-I2C-interface/m-p/1263020#M1440</guid>
      <dc:creator>satheesh_mb</dc:creator>
      <dc:date>2021-04-15T18:02:13Z</dc:date>
    </item>
    <item>
      <title>Re: Configure FS8530 using NXP Flex GUI and I2C interface</title>
      <link>https://community.nxp.com/t5/Power-Management/Configure-FS8530-using-NXP-Flex-GUI-and-I2C-interface/m-p/1264320#M1442</link>
      <description>&lt;P&gt;Hello Satheesh,&lt;/P&gt;
&lt;P&gt;Based on the report, the&amp;nbsp;FS84 does not respond to the I2C bus. Please make sure that the DBG pin is connected to 5V and the FS84 is in debug mode, then the default I2C addresses 0x20 (main), 0x21 (fail-safe) can be used for OTP configuration.&lt;/P&gt;
&lt;P&gt;Next, I would focus on the value of VDDI2C. By default, I2C is powered via LDO, but all regulators are turned off in debug mode, so it is necessary to solve the power supply of VDDI2C externally, as shown below.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="fs8x_vddi2c.png" style="width: 796px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/142647i5669593B2F654777/image-size/large?v=v2&amp;amp;px=999" role="button" title="fs8x_vddi2c.png" alt="fs8x_vddi2c.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Tomas&lt;/P&gt;</description>
      <pubDate>Mon, 19 Apr 2021 11:58:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/Configure-FS8530-using-NXP-Flex-GUI-and-I2C-interface/m-p/1264320#M1442</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2021-04-19T11:58:29Z</dc:date>
    </item>
  </channel>
</rss>