<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power Management中的主题 Re: NXQ1TXH5, breakage possible ?</title>
    <link>https://community.nxp.com/t5/Power-Management/NXQ1TXH5-breakage-possible/m-p/1222581#M1347</link>
    <description>&lt;P&gt;Hello, Jozef,&lt;/P&gt;&lt;P&gt;we use a different coil due to shape of the product where an A11 would be too big.&lt;/P&gt;&lt;P&gt;Furthermore we do not need Qi compliance/certificate and product will be precisely located by mechanical parts.&lt;/P&gt;&lt;P&gt;Coil is Wurth 760308102308.&lt;/P&gt;&lt;P&gt;It has 30mR resistance and 3µH impedance.&lt;/P&gt;&lt;P&gt;It is compensated by using 760nF capacitor to keep the frequency at ~100kHz.&lt;/P&gt;&lt;P&gt;The coil 760308111 has indeed a lower DCRes, 20-25mR.&lt;/P&gt;&lt;P&gt;can the 10mR extra DCRes be the cause of these constant "analog detection". Is there a way to compensate it with any resistor on the device ?&lt;/P&gt;</description>
    <pubDate>Thu, 28 Jan 2021 09:57:57 GMT</pubDate>
    <dc:creator>ysellin</dc:creator>
    <dc:date>2021-01-28T09:57:57Z</dc:date>
    <item>
      <title>NXQ1TXH5, breakage possible ?</title>
      <link>https://community.nxp.com/t5/Power-Management/NXQ1TXH5-breakage-possible/m-p/1211726#M1332</link>
      <description>&lt;P&gt;Hello NXP,&lt;/P&gt;&lt;P&gt;We have a non starting NXQ1TXH5 here and suspect a breakage that we try to understand.&lt;/P&gt;&lt;P&gt;In our schematics, a led in serie with a resistor, is supplied by 5V(from USB supply) and goes into LED_R pin.&lt;/P&gt;&lt;P&gt;The rest of the NXQ (VSYS) is supplied by a 5V, coming from a backuped supply.&lt;/P&gt;&lt;P&gt;The resistor , limiting led current limits to ~7mA , so does it in LED_R pin , at maximum.&lt;/P&gt;&lt;P&gt;Except this led input, the rest of the schematic is identical to UM10943 eval board.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Question:&lt;/P&gt;&lt;P&gt;Is it possible that : the 5VUSB coming up earlier than the backuped one breaks the component because datasheet says that voltage on inputs like LED_R should be &amp;lt;VDD , which is is =0 when VUSB comes up.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Isn't the internal transistor on LED_R blocked until VDD is up on the NXQ ? Clamping diodes here ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;Yann&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Jan 2021 11:03:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/NXQ1TXH5-breakage-possible/m-p/1211726#M1332</guid>
      <dc:creator>ysellin</dc:creator>
      <dc:date>2021-01-14T11:03:23Z</dc:date>
    </item>
    <item>
      <title>Re: NXQ1TXH5, breakage possible ?</title>
      <link>https://community.nxp.com/t5/Power-Management/NXQ1TXH5-breakage-possible/m-p/1212212#M1333</link>
      <description>&lt;P&gt;Hello Yann,&lt;/P&gt;
&lt;P&gt;please see a reply from an application engineer I have contacted.&lt;/P&gt;
&lt;P&gt;DESCRIPTION&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#3366FF"&gt;I don't think that the connection of he LED breaks down the NXQ1TXH5.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#3366FF"&gt;They should measure the voltage on OUT1 and OUT2 without a receiver placed and then they should&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#3366FF"&gt;see the ping signal there switching between 0V and 5V. Please see a scope attached.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#3366FF"&gt;If there is no signal at all or only on one of the two, then the internal mosfets are broken&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#3366FF"&gt;and&amp;nbsp; too high voltage is supplied.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#3366FF"&gt;Then they should investigate if there backupend supply is working correctly: the voltage&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#3366FF"&gt;should always remain below 5V.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#3366FF"&gt;They also should not submit the charger coil to a magnetic field.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Fri, 15 Jan 2021 07:49:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/NXQ1TXH5-breakage-possible/m-p/1212212#M1333</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2021-01-15T07:49:46Z</dc:date>
    </item>
    <item>
      <title>Re: NXQ1TXH5, breakage possible ?</title>
      <link>https://community.nxp.com/t5/Power-Management/NXQ1TXH5-breakage-possible/m-p/1212420#M1335</link>
      <description>&lt;P&gt;Thank you Jozef,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i have no activity on output 1&amp;amp;2.&lt;/P&gt;&lt;P&gt;Neither on the CNF_IN pin where I should see the measurement every ~3s.&lt;/P&gt;&lt;P&gt;But at the same time i have no activity on the quartz. In this case i believe that the chip is unable to do anything, right ?&lt;/P&gt;&lt;P&gt;I'm investigating this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In case we do not wire a coil: is the chip trying to ping as you mentionned ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 15 Jan 2021 14:31:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/NXQ1TXH5-breakage-possible/m-p/1212420#M1335</guid>
      <dc:creator>ysellin</dc:creator>
      <dc:date>2021-01-15T14:31:09Z</dc:date>
    </item>
    <item>
      <title>Re: NXQ1TXH5, breakage possible ?</title>
      <link>https://community.nxp.com/t5/Power-Management/NXQ1TXH5-breakage-possible/m-p/1212442#M1336</link>
      <description>&lt;P&gt;Thank you Jozef,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i have no activity on output 1&amp;amp;2.&lt;/P&gt;&lt;P&gt;Neither on the CNF_IN pin where I should see the measurement every ~3s.&lt;/P&gt;&lt;P&gt;But at the same time i have no activity on the quartz. In this case i believe that the chip is unable to do anything, right ?&lt;/P&gt;&lt;P&gt;I'm investigating this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In case we do not wire a coil: is the chip trying to ping as you mentionned ?&lt;/P&gt;</description>
      <pubDate>Fri, 15 Jan 2021 15:13:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/NXQ1TXH5-breakage-possible/m-p/1212442#M1336</guid>
      <dc:creator>ysellin</dc:creator>
      <dc:date>2021-01-15T15:13:02Z</dc:date>
    </item>
    <item>
      <title>Re: NXQ1TXH5, breakage possible ?</title>
      <link>https://community.nxp.com/t5/Power-Management/NXQ1TXH5-breakage-possible/m-p/1217092#M1339</link>
      <description>&lt;P&gt;The non starting was due to a pcb issue . Solved.&lt;/P&gt;&lt;P&gt;I have a question: the ping signal is different than the one you sent attached which is equal to the one I see with the eval board.&lt;/P&gt;&lt;P&gt;It appears with every small glitch (~0.529s) when I have the coil wired and every ~4s when the coil is not wired (like eval board).&lt;/P&gt;&lt;P&gt;Is it normal ? It makes me think that it detects something at every small glitch and tries to start. Which is not normal as there is nothing in front of the coil.&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 19 Jan 2021 19:41:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/NXQ1TXH5-breakage-possible/m-p/1217092#M1339</guid>
      <dc:creator>ysellin</dc:creator>
      <dc:date>2021-01-19T19:41:52Z</dc:date>
    </item>
    <item>
      <title>Re: NXQ1TXH5, breakage possible ?</title>
      <link>https://community.nxp.com/t5/Power-Management/NXQ1TXH5-breakage-possible/m-p/1218534#M1341</link>
      <description>&lt;P&gt;Hello Ysellin,&lt;/P&gt;
&lt;P&gt;please see below a reply from the application engineer.&lt;/P&gt;
&lt;P&gt;DESCRIPTION&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;When nothing is placed on the charger coil, then he signal on OUT1/OUT2 should look like this:&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;every 400msec there is an "analog ping" (small glitch) and every 4 seconds there is a "digital ping" (thick glitch).&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;analog-digital ping.jpg&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;During the analog ping the full bridge in the NXQ1TXH5 is switching a few times and then the current is monitored.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;When there is an object (coin, telephone, something from metal) on the charger coil then the current ringing is strongly damped.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;This is detected and the NXQ1TXH5 then starts a digital ping in order to find out if the "object" is sending messages back.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;object on the charger.png&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;In the picture below the NXQ1TXH5 is every analog ping detecting an "object" and starts a digital ping. However it does not get&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;any response and then goes to sleep again till the next analog ping.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;detecting an object.jpg&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;If the above picture is measured without an object on the charger coil (or other metal in the vicinity of the coil), then the resistance of the charger coil is too high.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Thu, 21 Jan 2021 06:17:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/NXQ1TXH5-breakage-possible/m-p/1218534#M1341</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2021-01-21T06:17:16Z</dc:date>
    </item>
    <item>
      <title>Re: NXQ1TXH5, breakage possible ?</title>
      <link>https://community.nxp.com/t5/Power-Management/NXQ1TXH5-breakage-possible/m-p/1221378#M1343</link>
      <description>&lt;P&gt;Thank you Jozef.&lt;/P&gt;&lt;P&gt;I have a constant detection of something that leads to digital ping every 0.5s .&lt;/P&gt;&lt;P&gt;What is the best way to find the cause ? I already have set FOD_E and R8 and R14 according to "NXQ1TXH5-FOD Configuration" document.&lt;/P&gt;&lt;P&gt;Remains FOD-T parameter which will be difficult to set because our mechanical stack leads certainly to a bit more loss in the path.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Snubber : seeing the attached curve "snubber..."&amp;nbsp; where black trace is original snubber (6.8nF) and bleu trace with 16nF,&amp;nbsp; do you think that we should add more capacitance ?&lt;/P&gt;</description>
      <pubDate>Tue, 26 Jan 2021 17:36:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/NXQ1TXH5-breakage-possible/m-p/1221378#M1343</guid>
      <dc:creator>ysellin</dc:creator>
      <dc:date>2021-01-26T17:36:11Z</dc:date>
    </item>
    <item>
      <title>Re: NXQ1TXH5, breakage possible ?</title>
      <link>https://community.nxp.com/t5/Power-Management/NXQ1TXH5-breakage-possible/m-p/1221735#M1344</link>
      <description>&lt;P&gt;Hello Ysellin,&lt;/P&gt;
&lt;P&gt;could you please reattach the "snubber" file you mentioned? It seems it didn't pass.&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Wed, 27 Jan 2021 07:16:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/NXQ1TXH5-breakage-possible/m-p/1221735#M1344</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2021-01-27T07:16:16Z</dc:date>
    </item>
    <item>
      <title>Re: NXQ1TXH5, breakage possible ?</title>
      <link>https://community.nxp.com/t5/Power-Management/NXQ1TXH5-breakage-possible/m-p/1221786#M1345</link>
      <description>&lt;P&gt;Oops.&lt;/P&gt;&lt;P&gt;here it is.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="snubberBefore_afterAdd10nF.png" style="width: 878px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/135891iCFB461F4E70F03A3/image-dimensions/878x476?v=v2" width="878" height="476" role="button" title="snubberBefore_afterAdd10nF.png" alt="snubberBefore_afterAdd10nF.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;</description>
      <pubDate>Wed, 27 Jan 2021 08:21:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/NXQ1TXH5-breakage-possible/m-p/1221786#M1345</guid>
      <dc:creator>ysellin</dc:creator>
      <dc:date>2021-01-27T08:21:06Z</dc:date>
    </item>
    <item>
      <title>Re: NXQ1TXH5, breakage possible ?</title>
      <link>https://community.nxp.com/t5/Power-Management/NXQ1TXH5-breakage-possible/m-p/1221923#M1346</link>
      <description>&lt;P&gt;Hello Ysellin,&lt;/P&gt;
&lt;P&gt;please see below an answer from the application engineer.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;DESCRIPTION&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#3366FF"&gt;The best way to find the rootcause is to remove all metal objects in the vicinity of the charger coil and see if the problem&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#3366FF"&gt;persists. If the problem persists, then the resistance in the LC tank is too high.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#3366FF"&gt;Which charger coil is the customer using? It should be a 6.3uH / Qi A11 coil.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#3366FF"&gt;They can connect one of the coils attached, and see if the problems is gone.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Wed, 27 Jan 2021 11:20:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/NXQ1TXH5-breakage-possible/m-p/1221923#M1346</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2021-01-27T11:20:04Z</dc:date>
    </item>
    <item>
      <title>Re: NXQ1TXH5, breakage possible ?</title>
      <link>https://community.nxp.com/t5/Power-Management/NXQ1TXH5-breakage-possible/m-p/1222581#M1347</link>
      <description>&lt;P&gt;Hello, Jozef,&lt;/P&gt;&lt;P&gt;we use a different coil due to shape of the product where an A11 would be too big.&lt;/P&gt;&lt;P&gt;Furthermore we do not need Qi compliance/certificate and product will be precisely located by mechanical parts.&lt;/P&gt;&lt;P&gt;Coil is Wurth 760308102308.&lt;/P&gt;&lt;P&gt;It has 30mR resistance and 3µH impedance.&lt;/P&gt;&lt;P&gt;It is compensated by using 760nF capacitor to keep the frequency at ~100kHz.&lt;/P&gt;&lt;P&gt;The coil 760308111 has indeed a lower DCRes, 20-25mR.&lt;/P&gt;&lt;P&gt;can the 10mR extra DCRes be the cause of these constant "analog detection". Is there a way to compensate it with any resistor on the device ?&lt;/P&gt;</description>
      <pubDate>Thu, 28 Jan 2021 09:57:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/NXQ1TXH5-breakage-possible/m-p/1222581#M1347</guid>
      <dc:creator>ysellin</dc:creator>
      <dc:date>2021-01-28T09:57:57Z</dc:date>
    </item>
    <item>
      <title>Re: NXQ1TXH5, breakage possible ?</title>
      <link>https://community.nxp.com/t5/Power-Management/NXQ1TXH5-breakage-possible/m-p/1222661#M1348</link>
      <description>&lt;P&gt;Hi Ysellin,&lt;/P&gt;
&lt;P&gt;please see an answer from the application engineer in a .pdf attached.&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 28 Jan 2021 13:39:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/NXQ1TXH5-breakage-possible/m-p/1222661#M1348</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2021-01-28T13:39:46Z</dc:date>
    </item>
    <item>
      <title>Re: NXQ1TXH5, breakage possible ?</title>
      <link>https://community.nxp.com/t5/Power-Management/NXQ1TXH5-breakage-possible/m-p/1223285#M1353</link>
      <description>&lt;P&gt;Thank you for that advice.&lt;/P&gt;&lt;P&gt;The A11 coils are way too big for our product.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If we use a coil with 6.8 µH but with 340mR it leads to R/L = 50000&lt;/P&gt;&lt;P&gt;This should fit , right ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;At the end of your message "...soon be another problem" =&amp;gt; what does he/she have in mind ?&lt;/P&gt;</description>
      <pubDate>Fri, 29 Jan 2021 13:03:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/NXQ1TXH5-breakage-possible/m-p/1223285#M1353</guid>
      <dc:creator>ysellin</dc:creator>
      <dc:date>2021-01-29T13:03:22Z</dc:date>
    </item>
    <item>
      <title>Re: NXQ1TXH5, breakage possible ?</title>
      <link>https://community.nxp.com/t5/Power-Management/NXQ1TXH5-breakage-possible/m-p/1224606#M1358</link>
      <description>&lt;P&gt;Hi Ysellin,&lt;/P&gt;
&lt;P&gt;please see an answer from the application engineer.&lt;/P&gt;
&lt;P&gt;DESCRIPTION&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;They can try and see if it solves the ping issue, but I stand by my previous statement:&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;&lt;EM&gt;The charger is not a standalone circuit with just a coil + capacitor: at the moment a receiver is &lt;/EM&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;&lt;EM&gt;placed the charger coil is the primary winding of a resonant converter. So also the number of turns&lt;/EM&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;&lt;EM&gt;from the charger coil is important as well as the size of the coil and coupling between charger coil&lt;/EM&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#0000FF"&gt;&lt;EM&gt;and receiver coil.&amp;nbsp;&amp;nbsp;&lt;/EM&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Tue, 02 Feb 2021 09:52:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/NXQ1TXH5-breakage-possible/m-p/1224606#M1358</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2021-02-02T09:52:40Z</dc:date>
    </item>
  </channel>
</rss>