<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックPF1550 supplied from an external source</title>
    <link>https://community.nxp.com/t5/Power-Management/PF1550-supplied-from-an-external-source/m-p/1133140#M1142</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;There is something I cannot understand from PF1550 datasheet: can the PMIC be supplied from an external source, even if the battery is present and being loaded?&lt;/P&gt;&lt;P&gt;How does the VSYS voltage interact with the battery charge? Is it possible to provide VSYS from an external source?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Davide&lt;/P&gt;</description>
    <pubDate>Tue, 01 Sep 2020 14:39:15 GMT</pubDate>
    <dc:creator>Davide91</dc:creator>
    <dc:date>2020-09-01T14:39:15Z</dc:date>
    <item>
      <title>PF1550 supplied from an external source</title>
      <link>https://community.nxp.com/t5/Power-Management/PF1550-supplied-from-an-external-source/m-p/1133140#M1142</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;There is something I cannot understand from PF1550 datasheet: can the PMIC be supplied from an external source, even if the battery is present and being loaded?&lt;/P&gt;&lt;P&gt;How does the VSYS voltage interact with the battery charge? Is it possible to provide VSYS from an external source?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Davide&lt;/P&gt;</description>
      <pubDate>Tue, 01 Sep 2020 14:39:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PF1550-supplied-from-an-external-source/m-p/1133140#M1142</guid>
      <dc:creator>Davide91</dc:creator>
      <dc:date>2020-09-01T14:39:15Z</dc:date>
    </item>
    <item>
      <title>Re: PF1550 supplied from an external source</title>
      <link>https://community.nxp.com/t5/Power-Management/PF1550-supplied-from-an-external-source/m-p/1133372#M1146</link>
      <description>&lt;P&gt;Hi Davide,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes, the PMIC be supplied from an external source, even if the battery is present and being loaded, use external 5.0V from USB on VBUSIN.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;VSYS voltage interact with the battery charge. VSYSMIN parameter sets the point where the VSYS loop starts taking control and regulates the output. 4.3 V is the recommended setting to ensure that there is enough headroom before reaching UVDET.&lt;/P&gt;
&lt;P&gt;Check Figure 17 of the datasheet that shows the charging profile for a better understanding of the relationship between VSYS and the battery charge.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Do not connect external source to VSYS.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jose&lt;/P&gt;</description>
      <pubDate>Tue, 01 Sep 2020 22:28:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PF1550-supplied-from-an-external-source/m-p/1133372#M1146</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2020-09-01T22:28:41Z</dc:date>
    </item>
  </channel>
</rss>