<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Power ManagementのトピックRe: PCA9685 with external drivers - Direct gate driving capability?</title>
    <link>https://community.nxp.com/t5/Power-Management/PCA9685-with-external-drivers-Direct-gate-driving-capability/m-p/1070619#M1021</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI&lt;/P&gt;&lt;P&gt;For example the 10mA source current limited by inside of IC.&lt;/P&gt;&lt;P&gt;You can test the drive waveform then decide to use the series resistor,if there is high over shoot on the waveform you can consider about 10Ω resistor in series.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Aug 2020 01:45:48 GMT</pubDate>
    <dc:creator>guoweisun</dc:creator>
    <dc:date>2020-08-27T01:45:48Z</dc:date>
    <item>
      <title>PCA9685 with external drivers - Direct gate driving capability?</title>
      <link>https://community.nxp.com/t5/Power-Management/PCA9685-with-external-drivers-Direct-gate-driving-capability/m-p/1070618#M1020</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working on a project where I would like to use PCA9685 to drive&lt;BR /&gt;power-mosfets (BUK9K25-40E or similar with ~800pF input capacitance).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However from the PCA9685 datasheet I cannot extract consistent information on&lt;BR /&gt;how to use the device with external drivers:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;On page 35 (Chapter 10. Application design-in information) an example&lt;BR /&gt; schematic is shown with driver mosfet Gates directly attached to the PCA9685&lt;/LI&gt;&lt;LI&gt;However on page 2 it is stated that totem-pole outputs are able to "sink 25&lt;BR /&gt; mA and source 10 mA at 5 V"&lt;/LI&gt;&lt;/UL&gt;&lt;UL&gt;&lt;LI&gt;I cannot find any details on how the 10mA source current is limited&lt;BR /&gt; (i.e. is this limited by the device internally, or do I have to add external&lt;BR /&gt; protection to prevent the PCA9685 from excessive gate charging current?)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;BR /&gt;This leads me to the design questions:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Do I need to add a Gate charge resistor between PCA9685 and the external&lt;BR /&gt;driver mosfet?&lt;/LI&gt;&lt;LI&gt;If yes which value should it have?&lt;/LI&gt;&lt;/UL&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Aug 2020 22:40:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PCA9685-with-external-drivers-Direct-gate-driving-capability/m-p/1070618#M1020</guid>
      <dc:creator>rainer-nxp</dc:creator>
      <dc:date>2020-08-26T22:40:02Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9685 with external drivers - Direct gate driving capability?</title>
      <link>https://community.nxp.com/t5/Power-Management/PCA9685-with-external-drivers-Direct-gate-driving-capability/m-p/1070619#M1021</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI&lt;/P&gt;&lt;P&gt;For example the 10mA source current limited by inside of IC.&lt;/P&gt;&lt;P&gt;You can test the drive waveform then decide to use the series resistor,if there is high over shoot on the waveform you can consider about 10Ω resistor in series.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Aug 2020 01:45:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Power-Management/PCA9685-with-external-drivers-Direct-gate-driving-capability/m-p/1070619#M1021</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2020-08-27T01:45:48Z</dc:date>
    </item>
  </channel>
</rss>