<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: UWB Secure Ranging (FIRALITE) in Other Connectivity</title>
    <link>https://community.nxp.com/t5/Other-Connectivity/UWB-Secure-Ranging-FIRALITE/m-p/1604098#M92</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/207753"&gt;@kuldeep&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Hope you are doing well. You will be contacted directly.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Wed, 22 Feb 2023 22:01:04 GMT</pubDate>
    <dc:creator>Ricardo_Zamora</dc:creator>
    <dc:date>2023-02-22T22:01:04Z</dc:date>
    <item>
      <title>UWB Secure Ranging (FIRALITE)</title>
      <link>https://community.nxp.com/t5/Other-Connectivity/UWB-Secure-Ranging-FIRALITE/m-p/1602947#M91</link>
      <description>&lt;P&gt;I need some help on secure ranging on SR150. I’m facing an issue when running Firalite secure ranging demo from UWBIOT_SR150_v04.02.01_MCUx. On debugging further I see a failure to select FIRALITE ADF,&lt;/P&gt;&lt;P&gt;The below call fails.&lt;/P&gt;&lt;P&gt;// initiator: select ADF LOG_I("initiator: select ADF");&lt;/P&gt;&lt;P&gt;se_status = Se_API_SelectADF(optsA, oid_entries, oid_entries_count, &amp;amp;selectAdfResponse);&lt;/P&gt;&lt;P&gt;ENSURE_OR_GO_EXIT(se_status == SE_STATUS_OK);&lt;/P&gt;&lt;P&gt;From readme for Firalite secure randing demo, below are the prerequisites&lt;/P&gt;&lt;P&gt;- SE051W should be connceted to host Refer :ref:`board-se051w`&lt;/P&gt;&lt;P&gt;- SR150 should be bound to SE051W. Refer :ref:`sr150-demo-binding`&lt;/P&gt;&lt;P&gt;- Perform the ADF provisioning Refer :ref:`firalite-adf-provisioning`&lt;/P&gt;&lt;P&gt;- Once ADF provisioning sucessful we can run the demo_fl_initator.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was able to do the binding successfully. I could not find any information on firalite-adf-provisioning in SDK or in NXP site documentation. I suspect, The failure to select ADF is because of not doing firalite-adf-provisioning. Can you please help share the steps/demo code for firalite-adf-provisioning?&lt;/P&gt;</description>
      <pubDate>Tue, 21 Feb 2023 13:51:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-Connectivity/UWB-Secure-Ranging-FIRALITE/m-p/1602947#M91</guid>
      <dc:creator>kuldeep</dc:creator>
      <dc:date>2023-02-21T13:51:27Z</dc:date>
    </item>
    <item>
      <title>Re: UWB Secure Ranging (FIRALITE)</title>
      <link>https://community.nxp.com/t5/Other-Connectivity/UWB-Secure-Ranging-FIRALITE/m-p/1604098#M92</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/207753"&gt;@kuldeep&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Hope you are doing well. You will be contacted directly.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 22 Feb 2023 22:01:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-Connectivity/UWB-Secure-Ranging-FIRALITE/m-p/1604098#M92</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2023-02-22T22:01:04Z</dc:date>
    </item>
    <item>
      <title>Re: UWB Secure Ranging (FIRALITE)</title>
      <link>https://community.nxp.com/t5/Other-Connectivity/UWB-Secure-Ranging-FIRALITE/m-p/2183004#M358</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have the same problem as Kuldeep; is there now a place where the information is accessible, or did we need to be contacted by NXP to solve this problem?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 09 Oct 2025 12:20:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-Connectivity/UWB-Secure-Ranging-FIRALITE/m-p/2183004#M358</guid>
      <dc:creator>Pierre0811</dc:creator>
      <dc:date>2025-10-09T12:20:00Z</dc:date>
    </item>
    <item>
      <title>Re: UWB Secure Ranging (FIRALITE)</title>
      <link>https://community.nxp.com/t5/Other-Connectivity/UWB-Secure-Ranging-FIRALITE/m-p/2344879#M396</link>
      <description>&lt;P&gt;When performing operations based on firalite-adf-provising, I have the following questions:&lt;BR /&gt;1. How can I burn the se_VCOM firmware? Is it through DK6Programmer.exe?&lt;BR /&gt;2. After running the JRCPProxyConsole.exe -c COM44 command, no feedback is displayed in PowerShell.&lt;/P&gt;&lt;P&gt;3. The JCShell tool is not available.&lt;/P&gt;</description>
      <pubDate>Fri, 03 Apr 2026 02:36:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-Connectivity/UWB-Secure-Ranging-FIRALITE/m-p/2344879#M396</guid>
      <dc:creator>two_cloud</dc:creator>
      <dc:date>2026-04-03T02:36:48Z</dc:date>
    </item>
  </channel>
</rss>