<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: OL2385 - 868 MHz data rate in Other Connectivity</title>
    <link>https://community.nxp.com/t5/Other-Connectivity/OL2385-868-MHz-data-rate/m-p/1686592#M226</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/195318"&gt;@JiaNa&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Yes, you are correct. According to the OL2385 datasheet, the maximum data rate for the 868 MHz frequency band is indeed up to 400 kbit/s. This is the maximum speed at which data can be transferred using this product under ideal conditions. However, please note that actual data rates can vary depending on a variety of factors, including the quality of the transmission medium, the distance between the transmitter and receiver, and the presence of any interference.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 12 Jul 2023 11:27:17 GMT</pubDate>
    <dc:creator>prakashram72</dc:creator>
    <dc:date>2023-07-12T11:27:17Z</dc:date>
    <item>
      <title>OL2385 - 868 MHz data rate</title>
      <link>https://community.nxp.com/t5/Other-Connectivity/OL2385-868-MHz-data-rate/m-p/1686228#M225</link>
      <description>&lt;P&gt;Hi, I would like to know what is the maximum data rate for 868 MHz in OL2385. In OL2385 datasheet, it mentioned that the maximum data rate up to 400 kbit/s.&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jul 2023 05:29:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-Connectivity/OL2385-868-MHz-data-rate/m-p/1686228#M225</guid>
      <dc:creator>JiaNa</dc:creator>
      <dc:date>2023-07-12T05:29:25Z</dc:date>
    </item>
    <item>
      <title>Re: OL2385 - 868 MHz data rate</title>
      <link>https://community.nxp.com/t5/Other-Connectivity/OL2385-868-MHz-data-rate/m-p/1686592#M226</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/195318"&gt;@JiaNa&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Yes, you are correct. According to the OL2385 datasheet, the maximum data rate for the 868 MHz frequency band is indeed up to 400 kbit/s. This is the maximum speed at which data can be transferred using this product under ideal conditions. However, please note that actual data rates can vary depending on a variety of factors, including the quality of the transmission medium, the distance between the transmitter and receiver, and the presence of any interference.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jul 2023 11:27:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-Connectivity/OL2385-868-MHz-data-rate/m-p/1686592#M226</guid>
      <dc:creator>prakashram72</dc:creator>
      <dc:date>2023-07-12T11:27:17Z</dc:date>
    </item>
  </channel>
</rss>