<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Motor control evaluation kit in Motor Control</title>
    <link>https://community.nxp.com/t5/Motor-Control/Motor-control-evaluation-kit/m-p/2408028#M39</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Yes, you can.&lt;/P&gt;
&lt;P&gt;The MCSPTR2AK396 kit is specifically intended for motor-control application development on the S32K396, and NXP provides the reference software as ANSI C source code for non-AUTOSAR applications, making it suitable for developing and replacing parts of the control algorithm with your own custom C code.&lt;/P&gt;
&lt;P&gt;Typical software toolchain:&lt;/P&gt;
&lt;P&gt;S32 Design Studio (S32DS) – IDE, compiler, debugger&lt;BR /&gt;RTD (Real-Time Drivers) – S32K3 peripheral drivers&lt;BR /&gt;S32 Configuration Tool (S32CT) – pin/clock/peripheral configuration&lt;BR /&gt;AMMCLib – motor-control algorithms library&lt;BR /&gt;FreeMASTER – runtime monitoring and debugging&lt;BR /&gt;MCAT – motor parameter identification and tuning&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
    <pubDate>Tue, 25 Aug 2026 05:53:45 GMT</pubDate>
    <dc:creator>petervlna</dc:creator>
    <dc:date>2026-08-25T05:53:45Z</dc:date>
    <item>
      <title>Motor control evaluation kit</title>
      <link>https://community.nxp.com/t5/Motor-Control/Motor-control-evaluation-kit/m-p/2407576#M37</link>
      <description>&lt;P&gt;Hello, i am new to NXP.&lt;/P&gt;&lt;P&gt;can i develop and write a custom motor control C based code for MCSPTR2AK396 development kit ?&lt;/P&gt;&lt;P&gt;If yes, would it be possible to list the SW tool chain that comes with this kit ?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Sat, 22 Aug 2026 21:00:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Motor-Control/Motor-control-evaluation-kit/m-p/2407576#M37</guid>
      <dc:creator>NRH</dc:creator>
      <dc:date>2026-08-22T21:00:11Z</dc:date>
    </item>
    <item>
      <title>Re: Motor control evaluation kit</title>
      <link>https://community.nxp.com/t5/Motor-Control/Motor-control-evaluation-kit/m-p/2408028#M39</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Yes, you can.&lt;/P&gt;
&lt;P&gt;The MCSPTR2AK396 kit is specifically intended for motor-control application development on the S32K396, and NXP provides the reference software as ANSI C source code for non-AUTOSAR applications, making it suitable for developing and replacing parts of the control algorithm with your own custom C code.&lt;/P&gt;
&lt;P&gt;Typical software toolchain:&lt;/P&gt;
&lt;P&gt;S32 Design Studio (S32DS) – IDE, compiler, debugger&lt;BR /&gt;RTD (Real-Time Drivers) – S32K3 peripheral drivers&lt;BR /&gt;S32 Configuration Tool (S32CT) – pin/clock/peripheral configuration&lt;BR /&gt;AMMCLib – motor-control algorithms library&lt;BR /&gt;FreeMASTER – runtime monitoring and debugging&lt;BR /&gt;MCAT – motor parameter identification and tuning&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Tue, 25 Aug 2026 05:53:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Motor-Control/Motor-control-evaluation-kit/m-p/2408028#M39</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2026-08-25T05:53:45Z</dc:date>
    </item>
  </channel>
</rss>