<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Position From 3-Hall sensors in FOC Motor Control in Motor Control</title>
    <link>https://community.nxp.com/t5/Motor-Control/Position-From-3-Hall-sensors-in-FOC-Motor-Control/m-p/2176939#M27</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Dear All,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am currently working on a 10 kW motor drive for controlling a PMSM in an automotive traction application, utilizing a Field-Oriented Control (FOC) algorithm. I am facing a challenge with position extraction from the motor’s Hall sensors.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The motor is equipped&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;   &lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;with three Hall sensors spaced 120 electrical degrees apart. However, due to sensor misalignment or misplacement, I am experiencing position jumps at N*60 electrical degrees. This issue appears to stem from the position extraction algorithm. Specifically, the Hall sensors' XOR logic determines position in 60-degree segments of the electrical cycle. To obtain a continuous angle, I interpolate between these segments using speed summation.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have tested various smoothing methods, including PLL and others, which work well up to around 3000 RPM. Beyond this speed, I observe current spikes leading to torque ripple and an audible buzzing noise from the motor.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I will attach plots of the extracted position and Hall sensor signals for reference.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If anyone has encountered similar issues or has experience with position extraction from Hall sensors in such conditions, I would greatly appreciate your insights or recommendations.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you in advance.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Sat, 27 Sep 2025 12:11:05 GMT</pubDate>
    <dc:creator>engeek</dc:creator>
    <dc:date>2025-09-27T12:11:05Z</dc:date>
    <item>
      <title>Position From 3-Hall sensors in FOC Motor Control</title>
      <link>https://community.nxp.com/t5/Motor-Control/Position-From-3-Hall-sensors-in-FOC-Motor-Control/m-p/2176939#M27</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Dear All,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am currently working on a 10 kW motor drive for controlling a PMSM in an automotive traction application, utilizing a Field-Oriented Control (FOC) algorithm. I am facing a challenge with position extraction from the motor’s Hall sensors.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The motor is equipped&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;   &lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;with three Hall sensors spaced 120 electrical degrees apart. However, due to sensor misalignment or misplacement, I am experiencing position jumps at N*60 electrical degrees. This issue appears to stem from the position extraction algorithm. Specifically, the Hall sensors' XOR logic determines position in 60-degree segments of the electrical cycle. To obtain a continuous angle, I interpolate between these segments using speed summation.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have tested various smoothing methods, including PLL and others, which work well up to around 3000 RPM. Beyond this speed, I observe current spikes leading to torque ripple and an audible buzzing noise from the motor.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I will attach plots of the extracted position and Hall sensor signals for reference.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If anyone has encountered similar issues or has experience with position extraction from Hall sensors in such conditions, I would greatly appreciate your insights or recommendations.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you in advance.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 27 Sep 2025 12:11:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Motor-Control/Position-From-3-Hall-sensors-in-FOC-Motor-Control/m-p/2176939#M27</guid>
      <dc:creator>engeek</dc:creator>
      <dc:date>2025-09-27T12:11:05Z</dc:date>
    </item>
    <item>
      <title>Re: Position From 3-Hall sensors in FOC Motor Control</title>
      <link>https://community.nxp.com/t5/Motor-Control/Position-From-3-Hall-sensors-in-FOC-Motor-Control/m-p/2176972#M28</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Please help to share the motor control system main processor/microcontroller part number.&lt;/P&gt;
&lt;P&gt;Or referred NXP motor control reference design name/link. Thanks.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Mike&lt;/P&gt;</description>
      <pubDate>Sun, 28 Sep 2025 00:49:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Motor-Control/Position-From-3-Hall-sensors-in-FOC-Motor-Control/m-p/2176972#M28</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2025-09-28T00:49:49Z</dc:date>
    </item>
  </channel>
</rss>