<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRe: Ethernet phy drivers</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Ethernet-phy-drivers/m-p/310047#M9971</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Umberto,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the driver is close enough to what would be required for the 8081, you can modify the definitions in the phy_ksz8041.h header to match the 8081. It is just a matther of register address modification and so on.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Garabo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 05 May 2014 13:32:39 GMT</pubDate>
    <dc:creator>Luis_Garabo</dc:creator>
    <dc:date>2014-05-05T13:32:39Z</dc:date>
    <item>
      <title>Ethernet phy drivers</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Ethernet-phy-drivers/m-p/310046#M9970</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are developing a&amp;nbsp; K60 board and we have to choose&lt;/P&gt;&lt;P&gt;a Ethernet phy Chip suitable. &lt;/P&gt;&lt;P&gt;The evaluation board uses KSZ8041NL (Micrel) that handles both mode MII RMII&lt;BR /&gt;but we wish to use one with only interface RMIII ex:&amp;nbsp; KSZ8081RNBIA&lt;/P&gt;&lt;P&gt;MQX drivers are compatible with this chip?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;BR /&gt;Umberto Simonato&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 May 2014 09:38:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Ethernet-phy-drivers/m-p/310046#M9970</guid>
      <dc:creator>simonatoumberto</dc:creator>
      <dc:date>2014-05-05T09:38:40Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet phy drivers</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Ethernet-phy-drivers/m-p/310047#M9971</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Umberto,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the driver is close enough to what would be required for the 8081, you can modify the definitions in the phy_ksz8041.h header to match the 8081. It is just a matther of register address modification and so on.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Garabo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 May 2014 13:32:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Ethernet-phy-drivers/m-p/310047#M9971</guid>
      <dc:creator>Luis_Garabo</dc:creator>
      <dc:date>2014-05-05T13:32:39Z</dc:date>
    </item>
  </channel>
</rss>