<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software Solutions中的主题 MQX usb Device stack Vbus ISR Configuration</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-usb-Device-stack-Vbus-ISR-Configuration/m-p/308870#M9916</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have used the mqx usb device stack for my usb application. I have used IRQ6 pin interrupt to detect vbus attached event , with the help of mqx gpio example code of mcf54418 stack.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is that,&lt;/P&gt;&lt;P&gt;When I am plugging In usb connector, the interrupt comes and control goes to ISR function but it continuously cal ISR after i have removed usb connector. I have set&amp;nbsp; EPFR resigister bit in ISR using till no effect.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where should i am wrong? Which register I have to configure in ISR so that ISR cal only one time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Panks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Apr 2014 11:55:29 GMT</pubDate>
    <dc:creator>panks</dc:creator>
    <dc:date>2014-04-02T11:55:29Z</dc:date>
    <item>
      <title>MQX usb Device stack Vbus ISR Configuration</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-usb-Device-stack-Vbus-ISR-Configuration/m-p/308870#M9916</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have used the mqx usb device stack for my usb application. I have used IRQ6 pin interrupt to detect vbus attached event , with the help of mqx gpio example code of mcf54418 stack.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is that,&lt;/P&gt;&lt;P&gt;When I am plugging In usb connector, the interrupt comes and control goes to ISR function but it continuously cal ISR after i have removed usb connector. I have set&amp;nbsp; EPFR resigister bit in ISR using till no effect.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Where should i am wrong? Which register I have to configure in ISR so that ISR cal only one time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Panks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Apr 2014 11:55:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-usb-Device-stack-Vbus-ISR-Configuration/m-p/308870#M9916</guid>
      <dc:creator>panks</dc:creator>
      <dc:date>2014-04-02T11:55:29Z</dc:date>
    </item>
  </channel>
</rss>