<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software Solutions中的主题 Re: MQX CAN Driver</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-CAN-Driver/m-p/304523#M9782</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The FlexCAN hardware module supports features like Rx FIFO or Rx Queue, but they are not enabled in MQX 3.8 and MQX 4.0 FlexCAN driver.&lt;/P&gt;&lt;P&gt;Now in&amp;nbsp; the latest MQX release is 4.1. we added RX FIFO support for twrk70120m board, please refer to driver code.&lt;/P&gt;&lt;P&gt;C:\Freescale\Freescale_MQX_4_1\mqx\source\io\can\flexcan\fsl_flexcan_driver.c&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding who occupied first, according to datasheet, The scan order for mailboxes and Rx FIFO is from the matching element with lowest number to the higher ones&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 29 Mar 2014 13:47:23 GMT</pubDate>
    <dc:creator>danielchen</dc:creator>
    <dc:date>2014-03-29T13:47:23Z</dc:date>
    <item>
      <title>MQX CAN Driver</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-CAN-Driver/m-p/304522#M9781</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am new to MQX. Currently i am using MQX 3.8 for the K20 processor. Looking into the CAN driver of MQX, i think it wont support Reception FIFO feature.&lt;/P&gt;&lt;P&gt;My question is suppose there is two active reception mail boxes, which of these two mailboxes are occupied first when a new CAN message is received? Is it depends on mailbox number or what else?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Mar 2014 12:04:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-CAN-Driver/m-p/304522#M9781</guid>
      <dc:creator>murugan_m</dc:creator>
      <dc:date>2014-03-26T12:04:12Z</dc:date>
    </item>
    <item>
      <title>Re: MQX CAN Driver</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-CAN-Driver/m-p/304523#M9782</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The FlexCAN hardware module supports features like Rx FIFO or Rx Queue, but they are not enabled in MQX 3.8 and MQX 4.0 FlexCAN driver.&lt;/P&gt;&lt;P&gt;Now in&amp;nbsp; the latest MQX release is 4.1. we added RX FIFO support for twrk70120m board, please refer to driver code.&lt;/P&gt;&lt;P&gt;C:\Freescale\Freescale_MQX_4_1\mqx\source\io\can\flexcan\fsl_flexcan_driver.c&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding who occupied first, according to datasheet, The scan order for mailboxes and Rx FIFO is from the matching element with lowest number to the higher ones&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Mar 2014 13:47:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-CAN-Driver/m-p/304523#M9782</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2014-03-29T13:47:23Z</dc:date>
    </item>
    <item>
      <title>Re: MQX CAN Driver</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-CAN-Driver/m-p/304524#M9783</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When will the Rx FIFO functionality be implemented for the Kinetis MCU's?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Shreyas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Oct 2014 22:49:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-CAN-Driver/m-p/304524#M9783</guid>
      <dc:creator>thegreendroid</dc:creator>
      <dc:date>2014-10-22T22:49:37Z</dc:date>
    </item>
  </channel>
</rss>