<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MQX USB Host MFS events in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-USB-Host-MFS-events/m-p/301951#M9703</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That's not extremely helpful...&amp;nbsp; The example there still relies on the BSP to be correct, fortunately I found what was causing my issue.&amp;nbsp; I was missing the initialization for the pull downs going to the MCU.&amp;nbsp; Interesting that it will work when the stack is initialized with that being incorrect&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 01 May 2014 14:40:08 GMT</pubDate>
    <dc:creator>Toe</dc:creator>
    <dc:date>2014-05-01T14:40:08Z</dc:date>
    <item>
      <title>MQX USB Host MFS events</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-USB-Host-MFS-events/m-p/301949#M9701</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a MQX 4.1 project built from the MFS USB example and I'm having a hard time finding out why attach/detach events do not seem to occur properly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Right now the project will mount a usb storage device ONLY if the device is present when the usb stack is initialized.&amp;nbsp; If the stack is initialized and then a USB stick is inserted the mass device event is never triggered.&amp;nbsp; The event never triggers on the removal of the device either.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there something I can look at that may be missing?&amp;nbsp; &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;I assume there's an initialization step I missed either in one of the mqx libraries or in the usb stack.&amp;nbsp; &lt;/SPAN&gt;When debugging I can see the host task is running and not starving or running out of stack space.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MCU is 52252 clocked at 60MHz.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Apr 2014 15:18:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-USB-Host-MFS-events/m-p/301949#M9701</guid>
      <dc:creator>Toe</dc:creator>
      <dc:date>2014-04-23T15:18:47Z</dc:date>
    </item>
    <item>
      <title>Re: MQX USB Host MFS events</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-USB-Host-MFS-events/m-p/301950#M9702</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Are you using a Freescale board?&lt;/P&gt;&lt;P&gt;Could you please try using the example located at the next path:&lt;/P&gt;&lt;P&gt;C:\Freescale\Freescale_MQX_4_1\usb\host\examples\msd\msd_commands&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know if this helps :smileywink: &lt;BR /&gt;Have a great day,&lt;BR /&gt; Regards &lt;BR /&gt; Sol&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Apr 2014 22:28:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-USB-Host-MFS-events/m-p/301950#M9702</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2014-04-29T22:28:48Z</dc:date>
    </item>
    <item>
      <title>Re: MQX USB Host MFS events</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-USB-Host-MFS-events/m-p/301951#M9703</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That's not extremely helpful...&amp;nbsp; The example there still relies on the BSP to be correct, fortunately I found what was causing my issue.&amp;nbsp; I was missing the initialization for the pull downs going to the MCU.&amp;nbsp; Interesting that it will work when the stack is initialized with that being incorrect&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 May 2014 14:40:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-USB-Host-MFS-events/m-p/301951#M9703</guid>
      <dc:creator>Toe</dc:creator>
      <dc:date>2014-05-01T14:40:08Z</dc:date>
    </item>
  </channel>
</rss>