<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Flexbus read and write issue in MQX in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Flexbus-read-and-write-issue-in-MQX/m-p/297331#M9550</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I follow Flexbus demo case in MQX to write CAN application,&lt;/P&gt;&lt;P&gt;compared with original demo, I use mulitple mailbox for read/write.&lt;/P&gt;&lt;P&gt;But this application only can TX or RX, for example: one node run TX task, another run RX task, which is OK.&lt;/P&gt;&lt;P&gt;But the node run RX and TX togrther, which couldn't run well, it couldn't receive corrent data from another node, even can't enter into ISR.&lt;/P&gt;&lt;P&gt;the code run two nodes is same, only node ID is different.&lt;/P&gt;&lt;P&gt;So please help check attached file, thx!&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338939"&gt;test.h.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338939"&gt;fc.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 May 2014 08:30:17 GMT</pubDate>
    <dc:creator>daweiyou</dc:creator>
    <dc:date>2014-05-14T08:30:17Z</dc:date>
    <item>
      <title>Flexbus read and write issue in MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Flexbus-read-and-write-issue-in-MQX/m-p/297331#M9550</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I follow Flexbus demo case in MQX to write CAN application,&lt;/P&gt;&lt;P&gt;compared with original demo, I use mulitple mailbox for read/write.&lt;/P&gt;&lt;P&gt;But this application only can TX or RX, for example: one node run TX task, another run RX task, which is OK.&lt;/P&gt;&lt;P&gt;But the node run RX and TX togrther, which couldn't run well, it couldn't receive corrent data from another node, even can't enter into ISR.&lt;/P&gt;&lt;P&gt;the code run two nodes is same, only node ID is different.&lt;/P&gt;&lt;P&gt;So please help check attached file, thx!&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338939"&gt;test.h.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338939"&gt;fc.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 May 2014 08:30:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Flexbus-read-and-write-issue-in-MQX/m-p/297331#M9550</guid>
      <dc:creator>daweiyou</dc:creator>
      <dc:date>2014-05-14T08:30:17Z</dc:date>
    </item>
    <item>
      <title>Re: Flexbus read and write issue in MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Flexbus-read-and-write-issue-in-MQX/m-p/297332#M9551</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dawei:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;which board you are using, K60F120 or K70F120 ?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Daniel &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 May 2014 23:31:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Flexbus-read-and-write-issue-in-MQX/m-p/297332#M9551</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2014-05-22T23:31:20Z</dc:date>
    </item>
  </channel>
</rss>