<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software Solutions中的主题 [FNET/RTCS] MAC&amp;lt;-&amp;gt;PHY ===&amp;gt; MAC&amp;lt;-&amp;gt;MAC</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/FNET-RTCS-MAC-lt-gt-PHY-gt-MAC-lt-gt-MAC/m-p/158206#M942</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using FNET bootloader and MQX with RTCS on K60 tower and ethernet works fine.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need to change PHY device (ksz8041nl on tower board) to switch device (KSZ8863RLL) so it means change MAC(K60)&amp;lt;-&amp;gt;PHY to MAC(K60)&amp;lt;-&amp;gt;MAC connection, I think.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I wonder if is it difficult to change firmware of FNET and RTCS to work properly with this hardware change?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Apr 2012 13:24:58 GMT</pubDate>
    <dc:creator>master_szumi</dc:creator>
    <dc:date>2012-04-27T13:24:58Z</dc:date>
    <item>
      <title>[FNET/RTCS] MAC&lt;-&gt;PHY ===&gt; MAC&lt;-&gt;MAC</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/FNET-RTCS-MAC-lt-gt-PHY-gt-MAC-lt-gt-MAC/m-p/158206#M942</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using FNET bootloader and MQX with RTCS on K60 tower and ethernet works fine.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need to change PHY device (ksz8041nl on tower board) to switch device (KSZ8863RLL) so it means change MAC(K60)&amp;lt;-&amp;gt;PHY to MAC(K60)&amp;lt;-&amp;gt;MAC connection, I think.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I wonder if is it difficult to change firmware of FNET and RTCS to work properly with this hardware change?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Apr 2012 13:24:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/FNET-RTCS-MAC-lt-gt-PHY-gt-MAC-lt-gt-MAC/m-p/158206#M942</guid>
      <dc:creator>master_szumi</dc:creator>
      <dc:date>2012-04-27T13:24:58Z</dc:date>
    </item>
    <item>
      <title>Re: [FNET/RTCS] MAC&lt;-&gt;PHY ===&gt; MAC&lt;-&gt;MAC</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/FNET-RTCS-MAC-lt-gt-PHY-gt-MAC-lt-gt-MAC/m-p/158207#M943</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using both KSZ8041 and KSZ8873 and they both work with the same firmware.&lt;/P&gt;&lt;P&gt;I am using a MCF52259 and I modified the BSP by using the DEMO board example on the EVB platform.&lt;/P&gt;&lt;P&gt;There is no files for the KSZ8873 but it is very similar to the KSZ8041 so it works.&lt;/P&gt;&lt;P&gt;In the future I would like to add the additional features of the switch.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 May 2012 21:44:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/FNET-RTCS-MAC-lt-gt-PHY-gt-MAC-lt-gt-MAC/m-p/158207#M943</guid>
      <dc:creator>drummer</dc:creator>
      <dc:date>2012-05-03T21:44:16Z</dc:date>
    </item>
  </channel>
</rss>