<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Where is MQX TWR-WIFI-AR4100 Code ? in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Where-is-MQX-TWR-WIFI-AR4100-Code/m-p/289233#M9251</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;check&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/318565#318565"&gt;https://community.freescale.com/message/318565#318565&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In short, download and install the patch for MQX 3.7. There you will get the files that don't install with MQX 4.0 by default.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 Apr 2013 12:14:57 GMT</pubDate>
    <dc:creator>Martin_</dc:creator>
    <dc:date>2013-04-29T12:14:57Z</dc:date>
    <item>
      <title>Where is MQX TWR-WIFI-AR4100 Code ?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Where-is-MQX-TWR-WIFI-AR4100-Code/m-p/289232#M9250</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;I have MQX 4.0 and I've read the posts on this subject that identifies the \source\io\enet directory as containing AR4100 code.&amp;nbsp; My download of MQX 4.0 does not have that code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does MQX 4.0 support TWR-WIFI-AR4100 or must I move back to an older version that has support?&amp;nbsp; If support was dropped in the current release, can you share the reason why?&amp;nbsp; I was hoping to design in the AR4100 part but if it is not longer "recommended for new designs", I'd like to know that quickly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are other community members using the AR4100 part or has the community moved to other WiFi parts?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm not planning to use MQX.&amp;nbsp; I just need to get to the MQX driver source code so I can have a working example of SPI and API code that interfaces with the AR4100 chip and I will build upon that code to develop my end system.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, Chris&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Apr 2013 12:09:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Where-is-MQX-TWR-WIFI-AR4100-Code/m-p/289232#M9250</guid>
      <dc:creator>ChrisNielsen</dc:creator>
      <dc:date>2013-04-29T12:09:56Z</dc:date>
    </item>
    <item>
      <title>Re: Where is MQX TWR-WIFI-AR4100 Code ?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Where-is-MQX-TWR-WIFI-AR4100-Code/m-p/289233#M9251</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;check&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/318565#318565"&gt;https://community.freescale.com/message/318565#318565&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In short, download and install the patch for MQX 3.7. There you will get the files that don't install with MQX 4.0 by default.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Apr 2013 12:14:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Where-is-MQX-TWR-WIFI-AR4100-Code/m-p/289233#M9251</guid>
      <dc:creator>Martin_</dc:creator>
      <dc:date>2013-04-29T12:14:57Z</dc:date>
    </item>
  </channel>
</rss>