<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックCan someone point me out where K60 wakes up from VLLS3 in MQX, which function it will run first?</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Can-someone-point-me-out-where-K60-wakes-up-from-VLLS3-in-MQX/m-p/286141#M9061</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on the K60 on MQX4..0.1,CW10.4.&lt;/P&gt;&lt;P&gt;I am trying to implement VLLS3 mode in MQX. I can put the MCU into VLLS3 mode and wake it up using PTD0.&lt;/P&gt;&lt;P&gt;It said that when the MCU wakes up, it will go to reset vector. But in MQX4.0.1, how does it work? Is there any reset interrupt handler in MQX BSP code?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please advice.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Oct 2013 23:12:53 GMT</pubDate>
    <dc:creator>danielchai</dc:creator>
    <dc:date>2013-10-17T23:12:53Z</dc:date>
    <item>
      <title>Can someone point me out where K60 wakes up from VLLS3 in MQX, which function it will run first?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Can-someone-point-me-out-where-K60-wakes-up-from-VLLS3-in-MQX/m-p/286141#M9061</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on the K60 on MQX4..0.1,CW10.4.&lt;/P&gt;&lt;P&gt;I am trying to implement VLLS3 mode in MQX. I can put the MCU into VLLS3 mode and wake it up using PTD0.&lt;/P&gt;&lt;P&gt;It said that when the MCU wakes up, it will go to reset vector. But in MQX4.0.1, how does it work? Is there any reset interrupt handler in MQX BSP code?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please advice.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Oct 2013 23:12:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Can-someone-point-me-out-where-K60-wakes-up-from-VLLS3-in-MQX/m-p/286141#M9061</guid>
      <dc:creator>danielchai</dc:creator>
      <dc:date>2013-10-17T23:12:53Z</dc:date>
    </item>
    <item>
      <title>Re: Can someone point me out where K60 wakes up from VLLS3 in MQX, which function it will run first?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Can-someone-point-me-out-where-K60-wakes-up-from-VLLS3-in-MQX/m-p/286142#M9062</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;MQX is not currently setup to support low power modes below LLS mode.&lt;/P&gt;&lt;P&gt;If you go into VLLSx mode, a wake up event will simple cause a reset of the device and the MQX application will simple start and run as if a Power On Reset occurred.&lt;/P&gt;&lt;P&gt;You may add your own code into the initialization sequence to do whatever you want based on the wake-up mode.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Oct 2013 18:19:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Can-someone-point-me-out-where-K60-wakes-up-from-VLLS3-in-MQX/m-p/286142#M9062</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2013-10-18T18:19:47Z</dc:date>
    </item>
  </channel>
</rss>