<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Unable to change from dhcp bind to static ip when no dhcp server - device busy in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Unable-to-change-from-dhcp-bind-to-static-ip-when-no-dhcp-server/m-p/283795#M8951</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm experiencing problems when trying to apply a static ip. The device is configured from start up to poll an ip from a DHCP server (by &lt;EM&gt;ipcfg_bind_dhcp&lt;/EM&gt;). Changing to a fixed IP (using &lt;EM&gt;ipcfg_unbind &lt;/EM&gt;and &lt;EM&gt;ipcfg_bind_staticip&lt;/EM&gt;) is no problem if a server exists in the network however otherwise both functions return IPCFG_BUSY.&lt;/P&gt;&lt;P&gt;When going deeper into the code it looks like that the request_semaphore is not freed and polling for it fails.&lt;/P&gt;&lt;P&gt;What am I doing wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks in advance&lt;/P&gt;&lt;P&gt;Ren&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 Nov 2013 08:43:17 GMT</pubDate>
    <dc:creator>admin</dc:creator>
    <dc:date>2013-11-18T08:43:17Z</dc:date>
    <item>
      <title>Unable to change from dhcp bind to static ip when no dhcp server - device busy</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Unable-to-change-from-dhcp-bind-to-static-ip-when-no-dhcp-server/m-p/283795#M8951</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm experiencing problems when trying to apply a static ip. The device is configured from start up to poll an ip from a DHCP server (by &lt;EM&gt;ipcfg_bind_dhcp&lt;/EM&gt;). Changing to a fixed IP (using &lt;EM&gt;ipcfg_unbind &lt;/EM&gt;and &lt;EM&gt;ipcfg_bind_staticip&lt;/EM&gt;) is no problem if a server exists in the network however otherwise both functions return IPCFG_BUSY.&lt;/P&gt;&lt;P&gt;When going deeper into the code it looks like that the request_semaphore is not freed and polling for it fails.&lt;/P&gt;&lt;P&gt;What am I doing wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks in advance&lt;/P&gt;&lt;P&gt;Ren&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Nov 2013 08:43:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Unable-to-change-from-dhcp-bind-to-static-ip-when-no-dhcp-server/m-p/283795#M8951</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2013-11-18T08:43:17Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to change from dhcp bind to static ip when no dhcp server - device busy</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Unable-to-change-from-dhcp-bind-to-static-ip-when-no-dhcp-server/m-p/283796#M8952</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ren,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you tried to use ipcfg_bind_dhcp_wait() instead? Make sure that the second parameter is TRUE. This will cause to try auto-ip in case the DHCP request fails.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Garabo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jan 2014 22:08:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Unable-to-change-from-dhcp-bind-to-static-ip-when-no-dhcp-server/m-p/283796#M8952</guid>
      <dc:creator>Luis_Garabo</dc:creator>
      <dc:date>2014-01-07T22:08:00Z</dc:date>
    </item>
  </channel>
</rss>