<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRe: MQX4.0 and TWR-WIFI-AR4100 patch?</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282796#M8879</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks again for your quick reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, I disabled the preprocessor error, and enabled GPIODEV in user_config.h.&lt;/P&gt;&lt;P&gt;I also removed TWR-SER from the setup, now I only have AR4100 on top and K60F120M in the second position.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SDCARD problem appears when the J12 from the AR4100 is set to 2-3 (Tower System GPIO3 will control reset/power down of AR4100), because GPIO3 is connected to PTE28, which is also the SD Card Detect pin. But I don't have a card inserted. I also changed the &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define BSP_ATHEROS_WIFI_GPIO_INT_PIN&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (GPIO_PORT_A|GPIO_PIN_IRQ_FALLING|GPIO_PIN27)&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in your example to &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define BSP_ATHEROS_WIFI_GPIO_INT_PIN&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (GPIO_PORT_B|GPIO_PIN_IRQ_FALLING|GPIO_PIN7) &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Because on K60F120M the IRQ_A is PTB7, and the J16 is set on the AR4100 (Tower System IRQ_A will connect to AR4100 SPI_INT).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried with baudrates 10000000 and 20000000 and I got the same result: error 0xA4FF. There must be something I'm missing, but I can't figure out what.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Sebastian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 May 2013 14:30:56 GMT</pubDate>
    <dc:creator>aisebastian</dc:creator>
    <dc:date>2013-05-07T14:30:56Z</dc:date>
    <item>
      <title>MQX4.0 and TWR-WIFI-AR4100 patch?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282787#M8870</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i just obtained a TWR-WIFI-AR4100 and instructions says to install an "enablement patch for MQX" but there are only versions for MQX 3.6.2 and 3.7 listed in downloads (&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-WIFI-AR4100&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-WIFI-AR4100&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-WIFI-AR4100&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;) &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;does this mean that it is already enabled in MQX4.0 or that no patch exists?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Mar 2013 16:22:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282787#M8870</guid>
      <dc:creator>fireblade</dc:creator>
      <dc:date>2013-03-04T16:22:43Z</dc:date>
    </item>
    <item>
      <title>Re: MQX4.0 and TWR-WIFI-AR4100 patch?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282788#M8871</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually, patch exists only for MQX 3.6.2 and MQX 3.7, No official patch for MQX 4.0 at the moment.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What can be done is to take MQX 3.7 patch for TWR-WIFI-AR4100 and integrate the source code files into MQX 4.0. This solution uses the MQX 4.0 I/O SPI driver to communicate with the Wi-fi chip. Some time ago I did this work for TWR-K60D100M, I describe my steps here. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1)&lt;BR /&gt;Download and install TWR-WIFI-AR100 patch for MQX 3.7. This doesn't require to have MQX 3.7 installed and I would recommend to use an empty directory for the installation path, as the source code files of the patch would be isolated from MQX 3.7 source code files.&lt;/P&gt;&lt;P&gt;If MQX 3.7 is installed, no problem, the patch can be installed to this folder too; the patch source files are listed then in the text file "atheros_manifest.txt". &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2)&lt;BR /&gt;copy all files and subfolders from:&lt;BR /&gt;C:\Freescale\Freescale MQX 3.7\Mqx\source\io\enet\atheros_wifi\*.*&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;copy to:&lt;BR /&gt;C:\Freescale\Freescale MQX 4.0\Mqx\source\io\enet\atheros_wifi\*.*&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3)&lt;BR /&gt;overwrite file. from:&lt;BR /&gt;c:\Freescale\Freescale MQX 3.7\mqx\source\io\enet\enet_wifi.h&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;to:&lt;BR /&gt;c:\Freescale\Freescale_MQX_4_0\mqx\source\io\enet\enet_wifi.h&lt;BR /&gt;(we need &lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="_jivemacro_uid_13626625786065921 jive_text_macro jive_macro_code" jivemacro_uid="_13626625786065921"&gt;
&lt;P&gt;#define ENET_MEDIACTL_VENDOR_SPECIFIC&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; _IO(IO_TYPE_MEDIACTL_WIFI,0x81)&lt;/P&gt;
&lt;/PRE&gt;&lt;P&gt;4)&lt;BR /&gt;copy from:&lt;BR /&gt;c:\Freescale\Freescale MQX 3.7\mqx\source\io\enet\phy\atheros_phy.c&lt;BR /&gt;c:\Freescale\Freescale MQX 3.7\mqx\source\io\enet\phy\atheros_phy.h&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;copy to:&lt;BR /&gt;c:\Freescale\Freescale_MQX_4_0\mqx\source\io\enet\phy\atheros_phy.c&lt;BR /&gt;c:\Freescale\Freescale_MQX_4_0\mqx\source\io\enet\phy\atheros_phy.h&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;5)&lt;BR /&gt;clone BSP of your board. for example I use MQX 4.0 bsp clone tool to clone twrk60d100m BSP into twrk60d100m_atheros.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;6)&lt;BR /&gt;CW 10.3 (or 10.2 if you wish), drag &amp;amp; drop the .wsd file of the new BSP to the CW 10.x Projects window.&lt;BR /&gt;c:\Freescale\Freescale_MQX_4_0\config\twrk60d100m_atheros\cw10\twrk60d100m_atheros.wsd&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;7)&lt;BR /&gt;Add the new folder files (from steps 1) to 4) above) to the bsp build project.&lt;BR /&gt;(in CW 10.3, we can just drag atheros_wifi folder and drop into bsp-&amp;gt;Peripheral IO Drivers-&amp;gt;enet. I choose the option to "Link to files and recreate folder structure with virtual folders" relative to MQX_ROOT_DIR.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="lia-unicode-emoji" title=":smiling_face_with_sunglasses:"&gt;&lt;LI-EMOJI id="lia_smiling-face-with-sunglasses" title=":smiling_face_with_sunglasses:"&gt;&lt;/LI-EMOJI&gt;&lt;/SPAN&gt;&lt;BR /&gt;Add the following C compiler include search paths into the C compiler properties:&lt;/P&gt;&lt;P&gt;"${MQX_ROOT_DIR}/mqx/source/io/enet/atheros_wifi"&lt;BR /&gt;"${MQX_ROOT_DIR}/mqx/source/io/enet/atheros_wifi/include"&lt;BR /&gt;"${MQX_ROOT_DIR}/mqx/source/io/enet/atheros_wifi/include/AR6002"&lt;BR /&gt;"${MQX_ROOT_DIR}/mqx/source/io/enet/atheros_wifi/custom_src/include"&lt;BR /&gt;"${MQX_ROOT_DIR}/mqx/source/io/enet/atheros_wifi/custom_src/stack_custom"&lt;BR /&gt;"${MQX_ROOT_DIR}/mqx/source/io/enet/atheros_wifi/common_src/include"&lt;BR /&gt;"${MQX_ROOT_DIR}/mqx/source/io/enet/atheros_wifi/common_src/stack_common"&lt;BR /&gt;"${MQX_ROOT_DIR}/mqx/source/io/enet/atheros_wifi/common_src/wmi"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;9)&lt;BR /&gt;in user_config.h for the new BSP, &lt;BR /&gt;c:\Freescale\Freescale_MQX_4_0\config\twrk60d100m_atheros\user_config.h&lt;/P&gt;&lt;P&gt;define the following definitions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_text_macro jive_macro_code _jivemacro_uid_13626625959076969" jivemacro_uid="_13626625959076969"&gt;
&lt;P&gt;#define BSPCFG_ENABLE_GPIODEV 1
 #define BSPCFG_ENABLE_SPI2&amp;nbsp;&amp;nbsp;&amp;nbsp; 1
 #define BSPCFG_ENABLE_ATHEROS_WIFI 1
 #define RTCSCFG_ENABLE_IP_REASSEMBLY 1
 #define RTCSCFG_ENABLE_IGMP&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1&lt;/P&gt;
&lt;/PRE&gt;&lt;P&gt;&lt;BR /&gt;10)&lt;BR /&gt;in BSP init_enet.c we need to add 2nd enet device:&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="_jivemacro_uid_1362662751673651 jive_text_macro jive_macro_code" jivemacro_uid="_1362662751673651" modifiedtitle="true"&gt;
&lt;P&gt;#if BSPCFG_ENABLE_ATHEROS_WIFI
#include &amp;lt;atheros_wifi.h&amp;gt;&amp;nbsp; 
#include &amp;lt;atheros_phy.h&amp;gt;
#endif /* BSPCFG_ENABLE_ATHEROS_WIFI */&lt;/P&gt;
&lt;P&gt;#if BSPCFG_ENABLE_ATHEROS_WIFI &lt;/P&gt;
&lt;P&gt;const ENET_IF_STRUCT ENET_1 = {
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;amp;ATHEROS_WIFI_IF,
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;amp;ATHEROS_PHY_IF,
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1,
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1,
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0,
};&lt;/P&gt;
&lt;P&gt;ATHEROS_PARAM_WIFI_STRUCT atheros_wifi_param = {
 BSP_ATHEROS_WIFI_SPI_DEVICE,
&amp;nbsp;&amp;nbsp;&amp;nbsp; BSP_ATHEROS_WIFI_GPIO_INT_DEVICE,
&amp;nbsp;&amp;nbsp;&amp;nbsp; BSP_ATHEROS_WIFI_GPIO_INT_PIN,
&amp;nbsp;&amp;nbsp;&amp;nbsp; BSP_ATHEROS_WIFI_GPIO_PWD_DEVICE,
&amp;nbsp;&amp;nbsp;&amp;nbsp; BSP_ATHEROS_WIFI_GPIO_PWD_PIN
};
#endif /* BSPCFG_ENABLE_ATHEROS_WIFI */
 &lt;/P&gt;
&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;additions to the ENET_PARAM_STRUCT struct:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_text_macro jive_macro_code _jivemacro_uid_13626628346774405" jivemacro_uid="_13626628346774405"&gt;
&lt;P&gt;#if BSPCFG_ENABLE_ATHEROS_WIFI 
&amp;nbsp;&amp;nbsp;&amp;nbsp; {
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;amp;ENET_1,
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // # Default WiFi Device parameter
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Auto_Negotiate,
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BSPCFG_TX_RING_LEN,&amp;nbsp;&amp;nbsp; //&amp;nbsp; # NOT USED IN ATHEROS WIFI
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BSPCFG_TX_RING_LEN,&amp;nbsp;&amp;nbsp; //&amp;nbsp; # NOT USED IN ATHEROS WIFI
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ENET_FRAMESIZE,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //&amp;nbsp; # NOT USED IN ATHEROS WIFI
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BSPCFG_RX_RING_LEN,&amp;nbsp;&amp;nbsp; //&amp;nbsp; # NOT USED IN ATHEROS WIFI
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BSPCFG_RX_RING_LEN,&amp;nbsp;&amp;nbsp; //&amp;nbsp; # NOT USED IN ATHEROS WIFI
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ENET_FRAMESIZE,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //&amp;nbsp; # NOT USED IN ATHEROS WIFI
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BSP_CONFIG_ATHEROS_PCB,&amp;nbsp;&amp;nbsp; //&amp;nbsp; # rx PCBs 
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0,&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 ,
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (pointer)&amp;amp;atheros_wifi_param&amp;nbsp;&amp;nbsp;&amp;nbsp; 
&amp;nbsp;&amp;nbsp; },
#endif&amp;nbsp; /* BSPCFG_ENABLE_ATHEROS_WIFI */&lt;/P&gt;
&lt;/PRE&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt; &lt;/P&gt;&lt;P&gt;11)&lt;BR /&gt;in BSP init_spi.c&lt;BR /&gt;-----------------------------------&lt;BR /&gt;change _bsp_spi2_init structure Baudrate from 10000000 to 20000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;12)&lt;BR /&gt;in BSP twrk60d100m_atheros.h&lt;BR /&gt;-----------------------------------&lt;BR /&gt;change BSP_ENET_DEVICE_COUNT to&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_text_macro jive_macro_code _jivemacro_uid_13626628508905801" jivemacro_uid="_13626628508905801"&gt;
&lt;P&gt;#define BSP_ENET_DEVICE_COUNT&amp;nbsp;&amp;nbsp;&amp;nbsp; (MACNET_DEVICE_COUNT +(BSPCFG_ENABLE_ATHEROS_WIFI?1:0))&lt;/P&gt;
&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;add:&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_text_macro jive_macro_code _jivemacro_uid_136266286499139" jivemacro_uid="_136266286499139"&gt;
&lt;P&gt;#define ATHEROS_WIFI_DEFAULT_ENET_DEVICE&amp;nbsp;&amp;nbsp;&amp;nbsp; 1&lt;/P&gt;
&lt;P&gt;#if BSPCFG_ENABLE_SPI2
/* in file name, number after : is the mask for chip select. chip select 0 in this case. */
#define BSP_ATHEROS_WIFI_SPI_DEVICE&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "spi2:1"
#else
#error "SPI2 must be defined in user_config.h"
#endif
#define BSP_ATHEROS_WIFI_GPIO_INT_DEVICE&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "gpio:input"
#define BSP_ATHEROS_WIFI_GPIO_INT_PIN&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (GPIO_PORT_A|GPIO_PIN_IRQ_FALLING|GPIO_PIN27) 
#define BSP_ATHEROS_WIFI_GPIO_PWD_DEVICE&amp;nbsp;&amp;nbsp;&amp;nbsp; "gpio:write"
// corresponds to B23 on elevator
#define BSP_ATHEROS_WIFI_GPIO_PWD_PIN&amp;nbsp;&amp;nbsp;&amp;nbsp; (GPIO_PORT_E|GPIO_PIN28)&lt;/P&gt;
&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;13)&lt;BR /&gt;in atheros low level, we need to add couple of minor modifications:&lt;BR /&gt;c:\Freescale\Freescale_MQX_4_0\mqx\source\io\enet\atheros_wifi\custom_src\hw_interface\cust_hw_api.c&lt;/P&gt;&lt;P&gt;on lines 112 adn 157 add the source code line:&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_text_macro jive_macro_code _jivemacro_uid_13626628839067316" jivemacro_uid="_13626628839067316"&gt;
&lt;P&gt; fflush(GET_DRIVER_CXT(pCxt)-&amp;gt;spi_cxt);&lt;/P&gt;
&lt;/PRE&gt;&lt;P&gt;remove lines 265-268 ioctl(SPI_SET_CS). it is not needed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;14)&lt;BR /&gt;in file:&lt;BR /&gt;C:\Freescale\Freescale_MQX_4_0\mqx\source\io\enet\atheros_wifi\custom_src\driver\cust_driver_netbuf.c&lt;/P&gt;&lt;P&gt;on line 52&lt;BR /&gt;change from:&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="_jivemacro_uid_13626628965372705 jive_text_macro jive_macro_code" jivemacro_uid="_13626628965372705"&gt;
&lt;P&gt;a_netbuf_ptr-&amp;gt;native.FREE = (_pcb_free_fn)freefn;&lt;/P&gt;
&lt;/PRE&gt;&lt;P&gt;change to:&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_text_macro _jivemacro_uid_13626629070478577 jive_macro_code" jivemacro_uid="_13626629070478577"&gt;
&lt;P&gt;a_netbuf_ptr-&amp;gt;native.FREE = (PCB_FREE_FPTR)freefn;&lt;/P&gt;
&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;15)&lt;BR /&gt;Ready to build BSP and other MQX libs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;16)&lt;BR /&gt;After build, copy two header files&lt;/P&gt;&lt;P&gt;copy from:&lt;BR /&gt;"c:\Freescale\Freescale_MQX_4_0\mqx\source\io\enet\atheros_wifi\custom_src\include\a_types.h"&lt;BR /&gt;c:\Freescale\Freescale_MQX_4_0\mqx\source\io\enet\atheros_wifi\atheros_wifi_api.h&lt;/P&gt;&lt;P&gt;copy to:&lt;BR /&gt;"c:\Freescale\Freescale_MQX_4_0\lib\twrk60d100m_atheros.cw10\debug\bsp\a_types.h"&lt;BR /&gt;"c:\Freescale\Freescale_MQX_4_0\lib\twrk60d100m_atheros.cw10\debug\bsp\atheros_wifi_api.h"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At this point we should be fine to make a Wi-fi application. For this we can use c:\Freescale\Freescale_MQX_4_0\rtcs\examples\httpsrv\&lt;/P&gt;&lt;P&gt;Import this project into your workspace.&lt;BR /&gt;c:\Freescale\Freescale_MQX_4_0\rtcs\examples\httpsrv\cw10\httpsrv_twrk60d100m_atheros\&lt;BR /&gt;after import, set its build configuration to Int_Flash_Debug.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Attached are the httpsrv example demo files with Atheros Wifi.&lt;BR /&gt;It runs two http servers.&lt;BR /&gt; One over Ethernet on 192.168.1.200&lt;BR /&gt; Second over Wi-fi on 192.168.1.201&lt;BR /&gt; Wi-fi access point name is "atheros_demo"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tried on TWR-K60D100M, TWR-SER, TWR-WIFI-AR4100, with CW 10.3 IDE to build MQX 4.0 and twrk60d100m_atheros BSP. "ttyd:" = RS232 on TWR-SER used as default MQX IO channel (BSP_DEFAULT_IO_CHANNEL).&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Mar 2013 13:30:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282788#M8871</guid>
      <dc:creator>Martin_</dc:creator>
      <dc:date>2013-03-07T13:30:47Z</dc:date>
    </item>
    <item>
      <title>Re: MQX4.0 and TWR-WIFI-AR4100 patch?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282789#M8872</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;ive done that and all seams to compile correctly&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but when run it seems to get stuck somewhere inside ipcfg_init_device for the atheros device,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Mar 2013 13:51:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282789#M8872</guid>
      <dc:creator>fireblade</dc:creator>
      <dc:date>2013-03-08T13:51:59Z</dc:date>
    </item>
    <item>
      <title>Re: MQX4.0 and TWR-WIFI-AR4100 patch?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282790#M8873</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Which TWR processor board do you use ? When I was debugging the spi communication, I found the first spi transaction occurs in Hcd_Init() in the source file:&lt;BR /&gt;c:\Freescale\Freescale_MQX_4_0\mqx\source\io\enet\atheros_wifi\common_src\hcd\spi_hcd.c&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;There is a call to DoPioWriteInternal(), which is the first spi communication with the Wi-fi chip out of reset. Shortly after that there is&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_text_macro jive_macro_code _jivemacro_uid_13629827268263051" jivemacro_uid="_13629827268263051"&gt;
&lt;P&gt;status = DoPioReadInternal(pCxt, ATH_SPI_WRBUF_SPC_AVA_REG, &amp;amp;pDCxt-&amp;gt;hcd.WriteBufferSpace);&lt;/P&gt;
&lt;/PRE&gt;&lt;P&gt;&lt;BR /&gt;Debug this code to make sure the SPI communication is working, WriteBufferSpace should read EXPECTED_MAX_WRITE_BUFFER_SPACE. If it doesn't, the spi communication is not functioning. Put oscilloscope probes to spi bus signals and see if there is everything as it should be.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;In the source code, double check if you have modified all steps for spi chip select:&lt;/P&gt;&lt;P&gt;- the chip select 0 is in the spi file name: "spi2:1" &lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_text_macro jive_macro_code _jivemacro_uid_13629827576163137" jivemacro_uid="_13629827576163137"&gt;
&lt;P&gt;#define BSP_ATHEROS_WIFI_SPI_DEVICE&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "spi2:1"&lt;/P&gt;
&lt;/PRE&gt;&lt;P&gt;- completely remove a call to&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_text_macro jive_macro_code _jivemacro_uid_1362982779826346" jivemacro_uid="_1362982779826346"&gt;
&lt;P&gt;ioctl (pCustCxt-&amp;gt;spi_cxt, IO_IOCTL_SPI_SET_CS, &amp;amp;input))&lt;/P&gt;
&lt;/PRE&gt;&lt;P&gt;from Custom_HW_Init()&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Mar 2013 06:20:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282790#M8873</guid>
      <dc:creator>Martin_</dc:creator>
      <dc:date>2013-03-11T06:20:53Z</dc:date>
    </item>
    <item>
      <title>Re: MQX4.0 and TWR-WIFI-AR4100 patch?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282791#M8874</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Christopher, have you had any breakthroughs?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Keep us posted! :smileywink:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Mar 2013 23:27:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282791#M8874</guid>
      <dc:creator>Monica</dc:creator>
      <dc:date>2013-03-19T23:27:50Z</dc:date>
    </item>
    <item>
      <title>Re: MQX4.0 and TWR-WIFI-AR4100 patch?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282792#M8875</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am running mqx 3.8 and k60f120m. I went through the above steps to be able to use the AR4100, except &lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;change from:&lt;/P&gt;&lt;P class="dp-highlighter"&gt;&lt;/P&gt;&lt;DIV class="bar" style="font-style: inherit; font-family: inherit;"&gt;&lt;P&gt;&lt;/P&gt;&lt;OL class="dp-cpp" start="1" style="font-style: inherit; font-family: inherit;"&gt;&lt;LI&gt;&lt;SPAN style="font-style: inherit;"&gt;a_netbuf_ptr-&amp;gt;native.FREE = (_pcb_free_fn)freefn;&amp;nbsp; &lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;/DIV&gt;&lt;P&gt;&lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;change to:&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="bar" style="font-style: inherit; font-family: inherit;"&gt;&lt;/P&gt;&lt;DIV style="font-style: inherit; font-family: inherit;"&gt;&lt;P&gt;&lt;/P&gt;&lt;OL class="dp-cpp" start="1" style="font-style: inherit; font-family: inherit;"&gt;&lt;LI&gt;&lt;SPAN style="font-style: inherit;"&gt;a_netbuf_ptr-&amp;gt;native.FREE = (PCB_FREE_FPTR)freefn;&amp;nbsp; &lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;which seems to be MQX 4.0 specific. Everything compiles fine, but ipcfg_init_device returns error 0xA4FF (ENET_ERROR). I checked if &lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;WriteBufferSpace reads EXPECTED_MAX_WRITE_BUFFER_SPACE, and it does, and I removed the &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-size: 12px; background-color: #ffffff; font-family: helvetica, arial;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-size: 12px; background-color: #ffffff; font-family: helvetica, arial;"&gt;ioctl (pCustCxt-&amp;gt;spi_cxt, IO_IOCTL_SPI_SET_CS, &amp;amp;input))&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;line from custom_hw_init().&lt;/P&gt;&lt;P&gt;Do you have any idea as to what I could do next to make it work? Or perhaps where to search for info?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Sebastian&lt;/P&gt;&lt;/DIV&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 21 Apr 2013 12:39:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282792#M8875</guid>
      <dc:creator>aisebastian</dc:creator>
      <dc:date>2013-04-21T12:39:53Z</dc:date>
    </item>
    <item>
      <title>Re: MQX4.0 and TWR-WIFI-AR4100 patch?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282793#M8876</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sebastian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this was specific to MQX 4.0 spi driver. MQX 4.0 has different SPI driver than MQX 3.8 / 3.8.1. As far as I know Atheros have their own port for MQX 3.8, so try contacting them. With MQX 3.8 you would need that SET_CS ioctl. You code stops exactly at the place where it checks if spi communication with the wi-fi chip is working. If you connect oscilloscope on spi signals you will see problems (no chip select asserted I guess).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Apr 2013 08:50:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282793#M8876</guid>
      <dc:creator>Martin_</dc:creator>
      <dc:date>2013-04-22T08:50:37Z</dc:date>
    </item>
    <item>
      <title>Re: MQX4.0 and TWR-WIFI-AR4100 patch?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282794#M8877</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello again, Martin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for late reply and thank's for your prompt response; I switched everything to MQX4.0 to be on par with these instructions and followed them exactly. the &lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;ipcfg_init_device&lt;/SPAN&gt; still returns A4FF. Is there any jumper setting that I need to change, or anything else? I tried with the httpd demo with your modified files.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have yet to inspect the signals with an osciloscope. Do you have any further hints as to what might go wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;P.S. The ENABLE_GPIODEV generates a preprocessor error, instructing me to use the LWGPIO driver instead. I tried commenting out the preprocessor error and removing the GPIODEV_ENABLE and neither worked.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Sebastian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 May 2013 09:38:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282794#M8877</guid>
      <dc:creator>aisebastian</dc:creator>
      <dc:date>2013-05-07T09:38:08Z</dc:date>
    </item>
    <item>
      <title>Re: MQX4.0 and TWR-WIFI-AR4100 patch?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282795#M8878</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sebastian, comment out the preprocessor error. Because you have to enable BSPCFG_ENABLE_GPIODEV in user_config.h, because the wi-fi stack uses this driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;on the thread below, another user gives feedback that he has the code working. he had to remove SD card from the slot on his hardware. also suggested to test at 10 MBits first, then 20 MBits.&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/327111#327111"&gt;https://community.freescale.com/message/327111#327111&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 May 2013 10:16:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282795#M8878</guid>
      <dc:creator>Martin_</dc:creator>
      <dc:date>2013-05-07T10:16:01Z</dc:date>
    </item>
    <item>
      <title>Re: MQX4.0 and TWR-WIFI-AR4100 patch?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282796#M8879</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks again for your quick reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, I disabled the preprocessor error, and enabled GPIODEV in user_config.h.&lt;/P&gt;&lt;P&gt;I also removed TWR-SER from the setup, now I only have AR4100 on top and K60F120M in the second position.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SDCARD problem appears when the J12 from the AR4100 is set to 2-3 (Tower System GPIO3 will control reset/power down of AR4100), because GPIO3 is connected to PTE28, which is also the SD Card Detect pin. But I don't have a card inserted. I also changed the &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define BSP_ATHEROS_WIFI_GPIO_INT_PIN&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (GPIO_PORT_A|GPIO_PIN_IRQ_FALLING|GPIO_PIN27)&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in your example to &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define BSP_ATHEROS_WIFI_GPIO_INT_PIN&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (GPIO_PORT_B|GPIO_PIN_IRQ_FALLING|GPIO_PIN7) &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Because on K60F120M the IRQ_A is PTB7, and the J16 is set on the AR4100 (Tower System IRQ_A will connect to AR4100 SPI_INT).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried with baudrates 10000000 and 20000000 and I got the same result: error 0xA4FF. There must be something I'm missing, but I can't figure out what.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Sebastian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 May 2013 14:30:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282796#M8879</guid>
      <dc:creator>aisebastian</dc:creator>
      <dc:date>2013-05-07T14:30:56Z</dc:date>
    </item>
    <item>
      <title>Re: MQX4.0 and TWR-WIFI-AR4100 patch?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282797#M8880</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sebastian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the TWR-K60N512 board with the same application and it's working, but only,when I make a power up reset. If I just push the reset button with power left attached, I'm getting the same error massage as you get. I have no idea, why, but may be, that information helps!?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 May 2013 15:26:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282797#M8880</guid>
      <dc:creator>ThomNet</dc:creator>
      <dc:date>2013-05-10T15:26:19Z</dc:date>
    </item>
    <item>
      <title>Re: MQX4.0 and TWR-WIFI-AR4100 patch?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282798#M8881</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I redid all the steps and it seems to work now. I must have broke something while tinkering with the bsp and demo app. Now it works perfectly. Thank you all for your help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 12 May 2013 01:15:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282798#M8881</guid>
      <dc:creator>aisebastian</dc:creator>
      <dc:date>2013-05-12T01:15:10Z</dc:date>
    </item>
    <item>
      <title>Re: MQX4.0 and TWR-WIFI-AR4100 patch?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282799#M8882</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sebastian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;are you using a DHCP server with your application?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 May 2013 20:59:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282799#M8882</guid>
      <dc:creator>ThomNet</dc:creator>
      <dc:date>2013-05-13T20:59:28Z</dc:date>
    </item>
    <item>
      <title>Re: MQX4.0 and TWR-WIFI-AR4100 patch?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282800#M8883</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Thomas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, and it works. I am also using wpa2/tkip, no issues. It works on both button reset and power cycle&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sebastian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 May 2013 09:50:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282800#M8883</guid>
      <dc:creator>aisebastian</dc:creator>
      <dc:date>2013-05-14T09:50:53Z</dc:date>
    </item>
    <item>
      <title>Re: MQX4.0 and TWR-WIFI-AR4100 patch?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282801#M8884</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sebastian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;are you using your WiFi application in "adhoc" or in "managed" mode?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 May 2013 12:03:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282801#M8884</guid>
      <dc:creator>ThomNet</dc:creator>
      <dc:date>2013-05-14T12:03:17Z</dc:date>
    </item>
    <item>
      <title>Re: MQX4.0 and TWR-WIFI-AR4100 patch?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282802#M8885</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Thomas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried only managed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sebastian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 May 2013 12:12:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282802#M8885</guid>
      <dc:creator>aisebastian</dc:creator>
      <dc:date>2013-05-14T12:12:25Z</dc:date>
    </item>
    <item>
      <title>Re: MQX4.0 and TWR-WIFI-AR4100 patch?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282803#M8886</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Martin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have done all the steps with : MQX4.0 and Atheros patch.We have executed all the steps given , but when reached to step no. 15 , we have build error. May i know what is the cause and not able to see the error too. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For your reference image is attached.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Nilesh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 01 Jun 2013 07:40:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282803#M8886</guid>
      <dc:creator>sNilesh</dc:creator>
      <dc:date>2013-06-01T07:40:12Z</dc:date>
    </item>
    <item>
      <title>Re: MQX4.0 and TWR-WIFI-AR4100 patch?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282804#M8887</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;At the Downloads page (&lt;A class="jive-link-external-small" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-WIFI-AR4100&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-WIFI-AR4100&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;), for some reason, I do not see any TWR-WIFI-AR4100 patches for the MQX at all.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Guys, can you confirm the files are removed? Or, do I do anything stupid?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Jul 2013 07:02:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282804#M8887</guid>
      <dc:creator>denisnechitailo</dc:creator>
      <dc:date>2013-07-01T07:02:10Z</dc:date>
    </item>
    <item>
      <title>Re: MQX4.0 and TWR-WIFI-AR4100 patch?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282805#M8888</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Denis,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have all the patches and MQX versions with us. Let me know if oyu required it,&lt;/P&gt;&lt;P&gt;we can share with Drop-box.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have AR4100P or AR4100 only ? Kindly confirm.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Nilesh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Jul 2013 07:51:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282805#M8888</guid>
      <dc:creator>sNilesh</dc:creator>
      <dc:date>2013-07-01T07:51:07Z</dc:date>
    </item>
    <item>
      <title>Re: MQX4.0 and TWR-WIFI-AR4100 patch?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282806#M8889</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks! It would be really nice if you could share the code. I have no chips on hand yet, but think that they will be AR4100/6302 (i.e. without the integrated stack). &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just do not have too much info about these chips (will have to sign the NDA with Qualcomm), but hope for a better result than we got with the SIPs from TI and Nanoradio.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Jul 2013 08:17:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX4-0-and-TWR-WIFI-AR4100-patch/m-p/282806#M8889</guid>
      <dc:creator>denisnechitailo</dc:creator>
      <dc:date>2013-07-01T08:17:05Z</dc:date>
    </item>
  </channel>
</rss>