<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Unknown USB Device connected? in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Unknown-USB-Device-connected/m-p/157473#M868</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When it happens to me ( Coldfire MCF51 and K60), one of two things is usually occuring.&lt;/P&gt;&lt;P&gt;1. I don't have the driver installed, which can be found in &amp;lt;your MQX path&amp;gt;usb\device\examples\cdc\virtual_com\inf&lt;/P&gt;&lt;P&gt;-or-&lt;/P&gt;&lt;P&gt;2. The device is booting up in BAM mode, which is a hardware driver that resides on some chips to allow firmware upgrading. I think the driver install can be found on this website somewhere, but I have never used it.&lt;/P&gt;&lt;P&gt;(This is usually the result of the hardware registers not being set correctly ).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 May 2012 06:17:07 GMT</pubDate>
    <dc:creator>timias</dc:creator>
    <dc:date>2012-05-02T06:17:07Z</dc:date>
    <item>
      <title>Unknown USB Device connected?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Unknown-USB-Device-connected/m-p/157472#M867</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Im using the MQX USB Device library with a 52259. With most Windows computers, it enumerates correctly and Windows recognizes it as a CDC device and it works. However, on some computers, Windows reports "Unknown USB Device connected", and there is nothing I can do to get it to enumerate or work at all.&lt;BR /&gt;&lt;BR /&gt;This happens on WinXP, Win2000, and Win7 computers. Some work, some dont.&lt;BR /&gt;&lt;BR /&gt;Ive tried upgrading from MQX 3.6 to MQX 3.8 to no avail.&lt;BR /&gt;&lt;BR /&gt;Has anyone else seen this and figured out how to fix it?&lt;BR /&gt;&lt;BR /&gt;Thanks for your help,&lt;BR /&gt;&lt;BR /&gt;Byra&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Apr 2012 00:20:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Unknown-USB-Device-connected/m-p/157472#M867</guid>
      <dc:creator>Byra</dc:creator>
      <dc:date>2012-04-26T00:20:10Z</dc:date>
    </item>
    <item>
      <title>Re: Unknown USB Device connected?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Unknown-USB-Device-connected/m-p/157473#M868</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When it happens to me ( Coldfire MCF51 and K60), one of two things is usually occuring.&lt;/P&gt;&lt;P&gt;1. I don't have the driver installed, which can be found in &amp;lt;your MQX path&amp;gt;usb\device\examples\cdc\virtual_com\inf&lt;/P&gt;&lt;P&gt;-or-&lt;/P&gt;&lt;P&gt;2. The device is booting up in BAM mode, which is a hardware driver that resides on some chips to allow firmware upgrading. I think the driver install can be found on this website somewhere, but I have never used it.&lt;/P&gt;&lt;P&gt;(This is usually the result of the hardware registers not being set correctly ).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 May 2012 06:17:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Unknown-USB-Device-connected/m-p/157473#M868</guid>
      <dc:creator>timias</dc:creator>
      <dc:date>2012-05-02T06:17:07Z</dc:date>
    </item>
  </channel>
</rss>