<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Is possible to do a MQX USB general purpose communication without virtual COM? in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Is-possible-to-do-a-MQX-USB-general-purpose-communication/m-p/275523#M8512</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Freescale team and community.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to do a general purpose USB communication between Kinetis (TWR-K60 using MQX) and PC. The PC side is solved thanks to example from Freescale ("How to make a graphical user interface (GUI) for USB communication") and the extensive host drivers examples for PC. But in the microcontroller side, I am not able to do this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I started using the good example of USB CDC Virtual COM and worked perfectly, but now, I need to do the communication without virtual COM port.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried to do a new class driver using the manual "Freescale MQX USB Device User’s Guide" specifically the chapter "Chapter 4 Developing new Class Drivers", but it has a very short explanation and there are not any examples for to do a complete new class driver. Also I have tried to move the micro side code from Freescale example (How to make a graphical user interface (GUI) for USB communication) and neither I have been able.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need some help with this theme and if somebody has an example, I would be greatful. Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Oct 2013 10:37:15 GMT</pubDate>
    <dc:creator>raulnorthstar</dc:creator>
    <dc:date>2013-10-11T10:37:15Z</dc:date>
    <item>
      <title>Is possible to do a MQX USB general purpose communication without virtual COM?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Is-possible-to-do-a-MQX-USB-general-purpose-communication/m-p/275523#M8512</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Freescale team and community.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to do a general purpose USB communication between Kinetis (TWR-K60 using MQX) and PC. The PC side is solved thanks to example from Freescale ("How to make a graphical user interface (GUI) for USB communication") and the extensive host drivers examples for PC. But in the microcontroller side, I am not able to do this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I started using the good example of USB CDC Virtual COM and worked perfectly, but now, I need to do the communication without virtual COM port.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried to do a new class driver using the manual "Freescale MQX USB Device User’s Guide" specifically the chapter "Chapter 4 Developing new Class Drivers", but it has a very short explanation and there are not any examples for to do a complete new class driver. Also I have tried to move the micro side code from Freescale example (How to make a graphical user interface (GUI) for USB communication) and neither I have been able.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need some help with this theme and if somebody has an example, I would be greatful. Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Oct 2013 10:37:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Is-possible-to-do-a-MQX-USB-general-purpose-communication/m-p/275523#M8512</guid>
      <dc:creator>raulnorthstar</dc:creator>
      <dc:date>2013-10-11T10:37:15Z</dc:date>
    </item>
  </channel>
</rss>